Ming
November 6, 2023, 9:11am
1
Hello,
I am using the zed-ros2-wrapper for the ZED2i camera in ROS2 Foxy on a Jetson AGX Xavier. When I attempt to call the /zed2i/zed_node/set_pose service, I encounter the error message “Service call not valid: GNSS fusion is enabled,” even though I am certain that GNSS fusion is disabled.
Testing as shown in the figure below:
I would appreciate a response as this issue is causing me significant inconvenience.
Thank you.
Myzhar
November 6, 2023, 9:43am
2
Hi @Ming
I just tested and validated the bug.
A fix will be provided as soon as possible
Ming
November 6, 2023, 10:38am
4
Thank you. Looking forward to your response!
Myzhar
November 6, 2023, 11:08am
5
The bug has been fixed. The fix will be automatically merged into the master branch as soon as the CI pipeline is completed.
Ming
November 8, 2023, 9:47am
7
Hi @Myzhar Please excuse me for making another inquiry here.
I often receive the following warning during launch:
“[zed_wrapper-2] [2023-03-27 18:56:18 UTC][ZED][WARNING] [Init] Requested depth_minimum_distance: 0.3 meters is too close, clamped to 1.5000001 meters.”
This results in my depth minimum being set to 1.5 meters, which is not what I desire. This occurs frequently.
I look forward to your response and appreciate your help.
Myzhar
November 8, 2023, 10:02am
8
This seems a ZED SDK bug. I report it to the team.
What SDK version are you using?
Ming
November 8, 2023, 10:37am
9
The SDK version I am using is 4.0.7 on Jetson AGX Xavier.
Ming
November 9, 2023, 6:00am
10
Hi @Myzhar
Where can I track whether this issue has been resolved?
thanks
Myzhar
November 9, 2023, 10:25am
11
The issue was solved a few hours after your report: Fix `set_pose` service call and Github deploy · stereolabs/zed-ros2-wrapper@b3ab2dd · GitHub
I recommend you subscribe to the GitHub repository to obtain notifications as soon as a new version is available by clicking on Watch and Star
Ming
November 10, 2023, 11:13am
12
@Myzhar Oh, sorry about the set_pose problem. I have solved it from the latest repository of github. Thank you very much.
What I am referring to here is the problem that depth_minimum_distance cannot be set normally during startup.
I want to know as soon as possible if there is any solution.
thanks
Myzhar
November 10, 2023, 11:18am
13
This is an SDK problem. Can you install the ZED SDK v4.0.8 released yesterday and verify if the problem persists?
Ming
November 13, 2023, 7:15am
14
OK I will try, I just need to download v4.0.8 and execute the installer, It will be updated directly from v4.0.7, right?
Will it affect the original things?
thanks
Myzhar
November 13, 2023, 9:00am
15
@Ming you can simply run the installer, it will handle everything with no issues.
Ming
November 14, 2023, 9:40am
16
Hi @Myzhar ,
Why does my ros_wrapper still show 4.0.7 after I installed v4.0.8?
[zed_wrapper-2] [INFO] [1699954564.681889117] [zed2i.zed_node]: ZED SDK Version: 4.0.7 - Build 78516_cbe54973
It is conceivable that depth_minimum_distance is not resolved
I use ZED_explorer and the lower right corner shows v4.0.8
thanks
Myzhar
November 14, 2023, 9:54am
17
Hi @Ming
did you clean the ROS workspace cache after installing the SDK?
Ming
November 14, 2023, 11:10am
18
okay, it can read v4.0.8!
Unfortunately, the depth_minimum_distance problem still exists.
Myzhar
November 14, 2023, 11:12am
19
OK, I issued a bug report for the SDK team
Ming
November 17, 2023, 8:38am
20
Thanks, Where can I track whether this depth_minimum_distance issue has been resolved?
This problem bothers me so much that I can’t use it normally
Grateful!
Myzhar
November 17, 2023, 8:51am
21
We have no public bug trackers. You can find the fix in the next SDK release, so follow the SDK download page for updates.