Hi,
I’m developing an outdoor application using Zed2i camera.
Today I experieced, for the first time, a thermal instability of the camera.
The camera stopped comunicates over usb3 or communicates same values for pose/twist data (stucked pose/twist data).
After some investigation I realized that temperature of both cameras was very close to datasheet limit: around 50/51 °C .
The air temperature was 31/34°C . With camera off (or nearly off) the temperature read by the Sensors tools application is around 48°C. After a while, with the camera on, the temperature went up to 51/52°C, stable.
If self-heating is 3/4°C I suppose that the main source of heat sould be irradiation from direct sunlight.
Do you have any advise to work under direct sunlight. The Zed2i is painted black that is not helping.
I read in the forum about a box to extend the temperature range from the standard values to -30° - + 60°C but I didn’t find any details about that box.
Any advice about active cooling? Heatsink or even Peltier cooler along with heatsink?
Thank you