Zed2i Operating Temperature mismatch spec sheet vs webpage

Hi,
The webpage lists the operating temperature as -10°C to +50°C (14°F to 122°F) here ZED 2i - Industrial AI Stereo Camera | Stereolabs whie the spec sheet lists the operating temperature as -10°C to +45° (14°F to 113°F) here https://www.stereolabs.com/assets/datasheets/ZED%202i%20Datasheet%20Jan2023.pdf.

Which upper bound is correct, 45C or 50C?

Additionally, what do we expect will happen when this sensor reaches temperatures above the operating range? Will elaborations get slow or will the sensor stop working entirely?

Hi @bradyasheehan
the website is correct, the datasheet will be fixed soon

Hi @Myzhar thank you for following up.

Could you comment on the second question?

Additionally, what do we expect will happen when this sensor reaches temperatures above the operating range? Will elaborations get slow or will the sensor stop working entirely?

When the temperature raises the camera can have unpredictable behaviors, the USB3 connection can become unstable and the camera calibration can be invalidated.