ZED 2i - How to generate 2D Map?

how can i generated a 2D map using Zed with ROS2? I can only see 3D Map when mapping mode is enabled. Because I will use this 2dmap for Nav2

Hi @AddyPete
we are working on a ZED SDK module to provide this feature that will be released in the next few months.

Meanwhile, you can use STVL layer, Voxel Layer, Obstacle layer to convert point cloud messages into local and global cost maps.
Here’s a full list of available plugins that you can use: Navigation Plugins — Navigation 2 1.0.0 documentation

okay thanks, so I don’t need to use SLAM toolbox for mapping right? If yes, does it publish map->odom transformation?

Hello I just installed STVL Nav2 plugin. But I got error when running nav2.

1st Step. I did ros2 launch zed_wrapper zed2i.launch.py

Config file: common.yaml

# config/common_yaml
# Common parameters to Stereolabs ZED and ZED mini cameras
#
# Note: the parameter svo_file is passed as exe argumet
---
/**:
    ros__parameters:

        general:
            svo_file: "" # usually overwritten by launch file
            svo_loop: false # Enable loop mode when using an SVO as input source
            svo_realtime: true # if true the SVO will be played trying to respect the original framerate eventually skipping frames, otherwise every frame will be processed respecting the `pub_frame_rate` setting
            camera_timeout_sec: 5
            camera_max_reconnect: 5
            camera_flip: false
            zed_id: 0 # IMPORTANT: to be used in simulation to distinguish individual cameras im multi-camera configurations - usually overwritten by launch file
            serial_number: 0 # usually overwritten by launch file
            pub_resolution: 'MEDIUM' # The resolution used for output. 'HD2K', 'HD1080', 'HD1200', 'HD720', 'MEDIUM', 'SVGA', 'VGA', 'LOW'
            pub_frame_rate: 15.0 # [DYNAMIC] - frequency of publishing of visual images and depth images
            gpu_id: -1
            region_of_interest: '[]' # A polygon defining the ROI where the ZED SDK perform the processing ignoring the rest. Coordinates must be normalized to '1.0' to be resolution independent.
            #region_of_interest: '[[0.25,0.33],[0.75,0.33],[0.75,0.5],[0.5,0.75],[0.25,0.5]]' # A polygon defining the ROI where the ZED SDK perform the processing ignoring the rest. Coordinates must be normalized to '1.0' to be resolution independent.
            #region_of_interest: '[[0.25,0.25],[0.75,0.25],[0.75,0.75],[0.25,0.75]]' # A polygon defining the ROI where the ZED SDK perform the processing ignoring the rest. Coordinates must be normalized to '1.0' to be resolution independent.
            #region_of_interest: '[[0.5,0.25],[0.75,0.5],[0.5,0.75],[0.25,0.5]]' # A polygon defining the ROI where the ZED SDK perform the processing ignoring the rest. Coordinates must be normalized to '1.0' to be resolution independent.
            sdk_verbose: 1

        video:
            brightness: 4 # [DYNAMIC] Not available for ZED X/ZED X Mini
            contrast: 4 # [DYNAMIC] Not available for ZED X/ZED X Mini
            hue: 0 # [DYNAMIC] Not available for ZED X/ZED X Mini
            saturation: 4 # [DYNAMIC]
            sharpness: 4 # [DYNAMIC]
            gamma: 8 # [DYNAMIC]
            auto_exposure_gain: true # [DYNAMIC]
            exposure: 80 # [DYNAMIC]
            gain: 80 # [DYNAMIC]
            auto_whitebalance: true # [DYNAMIC]
            whitebalance_temperature: 42 # [DYNAMIC] - [28,65] works only if `auto_whitebalance` is false
            qos_history: 1 # '1': KEEP_LAST - '2': KEEP_ALL
            qos_depth: 1 # Queue size if using KEEP_LAST
            qos_reliability: 1 # '1': RELIABLE - '2': BEST_EFFORT -
            qos_durability: 2 # '1': TRANSIENT_LOCAL - '2': VOLATILE

        depth:
            depth_mode: 'NEURAL' # Matches the ZED SDK setting: 'NONE', 'PERFORMANCE', 'QUALITY', 'ULTRA', 'NEURAL' - Note: if 'NONE' all the modules that requires depth extraction are disabled by default (Pos. Tracking, Obj. Detection, Mapping, ...)
            depth_stabilization: 1 # Forces positional tracking to start if major than 0 - Range: [0,100]
            openni_depth_mode: false # 'false': 32bit float [meters], 'true': 16bit unsigned int [millimeters]
            point_cloud_freq: 10.0 # [DYNAMIC] - frequency of the pointcloud publishing (equal or less to `grab_frame_rate` value)
            depth_confidence: 50 # [DYNAMIC]
            depth_texture_conf: 100 # [DYNAMIC]
            remove_saturated_areas: true # [DYNAMIC]
            qos_history: 1 # '1': KEEP_LAST - '2': KEEP_ALL
            qos_depth: 1 # Queue size if using KEEP_LAST
            qos_reliability: 1 # '1': RELIABLE - '2': BEST_EFFORT -
            qos_durability: 2 # '1': TRANSIENT_LOCAL - '2': VOLATILE 

        pos_tracking:
            pos_tracking_enabled: true # True to enable positional tracking from start            
            imu_fusion: true # enable/disable IMU fusion. When set to false, only the optical odometry will be used.
            publish_tf: true # [usually overwritten by launch file] publish `odom -> base_link` TF
            publish_map_tf: true # [usually overwritten by launch file] publish `map -> odom` TF
            publish_imu_tf: true # [usually overwritten by launch file] enable/disable the IMU TF broadcasting
            base_frame: "base_link" # usually overwritten by launch file
            map_frame: "map"
            odometry_frame: "odom"
            area_memory_db_path: ""
            area_memory: true # Enable to detect loop closure
            depth_min_range: 0.0 # Set this value for removing fixed zones of the robot in the FoV of the camerafrom the visual odometry evaluation
            set_as_static: false # If 'true' the camera will be static and not move in the environment
            set_gravity_as_origin: true # If 'true' align the positional tracking world to imu gravity measurement. Keep the yaw from the user initial pose.
            floor_alignment: false # Enable to automatically calculate camera/floor offset
            initial_base_pose: [0.0, 0.0, 0.0, 0.0, 0.0, 0.0] # Initial position of the `base_frame` in the map -> [X, Y, Z, R, P, Y]
            init_odom_with_first_valid_pose: true # Enable to initialize the odometry with the first valid pose
            path_pub_rate: 2.0 # [DYNAMIC] - Camera trajectory publishing frequency
            path_max_count: -1 # use '-1' for unlimited path size
            two_d_mode: false # Force navigation on a plane. If true the Z value will be fixed to "fixed_z_value", roll and pitch to zero
            fixed_z_value: 0.00 # Value to be used for Z coordinate if `two_d_mode` is true
            transform_time_offset: 0.0 # The value added to the timestamp of `map->odom` and `odom->base_link`` transform being generated
            qos_history: 1 # '1': KEEP_LAST - '2': KEEP_ALL
            qos_depth: 1 # Queue size if using KEEP_LAST
            qos_reliability: 1 # '1': RELIABLE - '2': BEST_EFFORT
            qos_durability: 2 # '1': TRANSIENT_LOCAL - '2': VOLATILE

        gnss_fusion:
            gnss_fusion_enabled: false # fuse 'sensor_msg/NavSatFix' message information into pose data
            gnss_fix_topic: "/gps/fix" # Name of the GNSS topic of type NavSatFix to subscribe [Default: "/gps/fix"]
            gnss_init_distance: 5.0 # The minimum distance traveled by the robot required to initilize the GNSS fusion
            gnss_zero_altitude: false # Set to `true` to ignore GNSS altitude information
            gnss_frame: "gnss_link" # [usually overwritten by launch file] The TF frame of the GNSS sensor
            publish_utm_tf: true # Publish `utm` -> `map` TF
            broadcast_utm_transform_as_parent_frame: false # if 'true' publish `utm` -> `map` TF, otherwise `map` -> `utm`

        mapping:
            mapping_enabled: true # True to enable mapping and fused point cloud pubblication
            resolution: 0.05 # maps resolution in meters [min: 0.01f - max: 0.2f]
            max_mapping_range: 5.0 # maximum depth range while mapping in meters (-1 for automatic calculation) [2.0, 20.0]
            fused_pointcloud_freq: 1.0 # frequency of the publishing of the fused colored point cloud
            clicked_point_topic: "/clicked_point" # Topic published by Rviz when a point of the cloud is clicked. Used for plane detection
            qos_history: 1 # '1': KEEP_LAST - '2': KEEP_ALL
            qos_depth: 1 # Queue size if using KEEP_LAST
            qos_reliability: 1 # '1': RELIABLE - '2': BEST_EFFORT -
            qos_durability: 2 # '1': TRANSIENT_LOCAL - '2': VOLATILE

        sensors:
            sensors_image_sync: false # Synchronize Sensors messages with latest published video/depth message
            sensors_pub_rate: 200. # frequency of publishing of sensors data. MAX: 400. - MIN: grab rate
            qos_history: 1 # '1': KEEP_LAST - '2': KEEP_ALL
            qos_depth: 1 # Queue size if using KEEP_LAST
            qos_reliability: 1 # '1': RELIABLE - '2': BEST_EFFORT -
            qos_durability: 2 # '1': TRANSIENT_LOCAL - '2': VOLATILE

        object_detection:
            od_enabled: false # True to enable Object Detection
            model: 'MULTI_CLASS_BOX_MEDIUM' # 'MULTI_CLASS_BOX_FAST', 'MULTI_CLASS_BOX_MEDIUM', 'MULTI_CLASS_BOX_ACCURATE', 'PERSON_HEAD_BOX_FAST', 'PERSON_HEAD_BOX_ACCURATE'
            allow_reduced_precision_inference: true # Allow inference to run at a lower precision to improve runtime and memory usage
            max_range: 20.0 # [m] Defines a upper depth range for detections
            confidence_threshold: 50.0 # [DYNAMIC] - Minimum value of the detection confidence of an object [0,99]
            prediction_timeout: 0.5 # During this time [sec], the object will have OK state even if it is not detected. Set this parameter to 0 to disable SDK predictions            
            filtering_mode: 1 # '0': NONE - '1': NMS3D - '2': NMS3D_PER_CLASS
            mc_people: false # [DYNAMIC] - Enable/disable the detection of persons for 'MULTI_CLASS_X' models
            mc_vehicle: true # [DYNAMIC] - Enable/disable the detection of vehicles for 'MULTI_CLASS_X' models
            mc_bag: true # [DYNAMIC] - Enable/disable the detection of bags for 'MULTI_CLASS_X' models
            mc_animal: true # [DYNAMIC] - Enable/disable the detection of animals for 'MULTI_CLASS_X' models
            mc_electronics: true # [DYNAMIC] - Enable/disable the detection of electronic devices for 'MULTI_CLASS_X' models
            mc_fruit_vegetable: true # [DYNAMIC] - Enable/disable the detection of fruits and vegetables for 'MULTI_CLASS_X' models
            mc_sport: true # [DYNAMIC] - Enable/disable the detection of sport-related objects for 'MULTI_CLASS_X' models            
            qos_history: 1 # '1': KEEP_LAST - '2': KEEP_ALL
            qos_depth: 1 # Queue size if using KEEP_LAST
            qos_reliability: 1 # '1': RELIABLE - '2': BEST_EFFORT
            qos_durability: 2 # '1': TRANSIENT_LOCAL - '2': VOLATILE
        
        body_tracking:
            bt_enabled: false # True to enable Body Tracking
            model: 'HUMAN_BODY_MEDIUM' # 'HUMAN_BODY_FAST', 'HUMAN_BODY_MEDIUM', 'HUMAN_BODY_ACCURATE'
            body_format: 'BODY_38' # 'BODY_18','BODY_34','BODY_38','BODY_70'
            allow_reduced_precision_inference: false # Allow inference to run at a lower precision to improve runtime and memory usage
            max_range: 20.0 # [m] Defines a upper depth range for detections
            body_kp_selection: 'FULL' # 'FULL', 'UPPER_BODY'
            enable_body_fitting: false # Defines if the body fitting will be applied
            enable_tracking: true # Defines if the object detection will track objects across images flow
            prediction_timeout_s: 0.5 # During this time [sec], the skeleton will have OK state even if it is not detected. Set this parameter to 0 to disable SDK predictions
            confidence_threshold: 50.0 # [DYNAMIC] - Minimum value of the detection confidence of skeleton key points [0,99]
            minimum_keypoints_threshold: 5 # [DYNAMIC] - Minimum number of skeleton key points to be detected for a valid skeleton
            qos_history: 1 # '1': KEEP_LAST - '2': KEEP_ALL
            qos_depth: 1 # Queue size if using KEEP_LAST
            qos_reliability: 1 # '1': RELIABLE - '2': BEST_EFFORT
            qos_durability: 2 # '1': TRANSIENT_LOCAL - '2': VOLATILE

        use_sim_time: false # EXPERIMENTAL (only for development) - Set to true to enable SIMULATION mode # 
        sim_address: '192.168.1.90' # EXPERIMENTAL (only for development) - The local address of the machine running the simulator

        debug:
            debug_common: false
            debug_video_depth: false
            debug_camera_controls: false
            debug_point_cloud: false
            debug_positional_tracking: false
            debug_gnss: false
            debug_sensors: false
            debug_mapping : false
            debug_terrain_mapping : false
            debug_object_detection : false
            debug_body_tracking : false

Config file: zed2i.yaml

# config/zed2i_yaml
# Parameters for Stereolabs zed2i camera
---
/**:
    ros__parameters:
        general:
            camera_model: "zed2i"
            camera_name: "zed2i" # usually overwritten by launch file
            grab_resolution: 'HD720' # The native camera grab resolution. 'HD2K', 'HD1080', 'HD720', 'VGA', 'AUTO'
            grab_frame_rate: 30 # ZED SDK internal grabbing rate

        depth:
            min_depth: 0.2 # Min: 0.2, Max: 3.0
            max_depth: 10.0 # Max: 40.0

2nd Step: I ran nav2 with:
ros2 launch nav2_bringup navigation_launch.py params_file:=//home/myfileloc/Desktop/myfilelocdesk/nav2_params.yaml

This is my params file: nav2_params.yaml

amcl:
  ros__parameters:
    use_sim_time: True
    alpha1: 0.2
    alpha2: 0.2
    alpha3: 0.2
    alpha4: 0.2
    alpha5: 0.2
    base_frame_id: "base_link"
    beam_skip_distance: 0.5
    beam_skip_error_threshold: 0.9
    beam_skip_threshold: 0.3
    do_beamskip: false
    global_frame_id: "map"
    lambda_short: 0.1
    laser_likelihood_max_dist: 2.0
    laser_max_range: 100.0
    laser_min_range: -1.0
    laser_model_type: "likelihood_field"
    max_beams: 60
    max_particles: 2000
    min_particles: 500
    odom_frame_id: "odom"
    pf_err: 0.05
    pf_z: 0.99
    recovery_alpha_fast: 0.0
    recovery_alpha_slow: 0.0
    resample_interval: 1
    robot_model_type: "nav2_amcl::DifferentialMotionModel"
    save_pose_rate: 0.5
    sigma_hit: 0.2
    tf_broadcast: true
    transform_tolerance: 1.0
    update_min_a: 0.2
    update_min_d: 0.25
    z_hit: 0.5
    z_max: 0.05
    z_rand: 0.5
    z_short: 0.05
    scan_topic: scan

bt_navigator:
  ros__parameters:
    use_sim_time: True
    global_frame: map
    robot_base_frame: base_link
    odom_topic: /odom
    bt_loop_duration: 10
    default_server_timeout: 20
    # 'default_nav_through_poses_bt_xml' and 'default_nav_to_pose_bt_xml' are use defaults:
    # nav2_bt_navigator/navigate_to_pose_w_replanning_and_recovery.xml
    # nav2_bt_navigator/navigate_through_poses_w_replanning_and_recovery.xml
    # They can be set here or via a RewrittenYaml remap from a parent launch file to Nav2.
    plugin_lib_names:
    - nav2_compute_path_to_pose_action_bt_node
    - nav2_compute_path_through_poses_action_bt_node
    - nav2_smooth_path_action_bt_node
    - nav2_follow_path_action_bt_node
    - nav2_spin_action_bt_node
    - nav2_wait_action_bt_node
    - nav2_assisted_teleop_action_bt_node
    - nav2_back_up_action_bt_node
    - nav2_drive_on_heading_bt_node
    - nav2_clear_costmap_service_bt_node
    - nav2_is_stuck_condition_bt_node
    - nav2_goal_reached_condition_bt_node
    - nav2_goal_updated_condition_bt_node
    - nav2_globally_updated_goal_condition_bt_node
    - nav2_is_path_valid_condition_bt_node
    - nav2_initial_pose_received_condition_bt_node
    - nav2_reinitialize_global_localization_service_bt_node
    - nav2_rate_controller_bt_node
    - nav2_distance_controller_bt_node
    - nav2_speed_controller_bt_node
    - nav2_truncate_path_action_bt_node
    - nav2_truncate_path_local_action_bt_node
    - nav2_goal_updater_node_bt_node
    - nav2_recovery_node_bt_node
    - nav2_pipeline_sequence_bt_node
    - nav2_round_robin_node_bt_node
    - nav2_transform_available_condition_bt_node
    - nav2_time_expired_condition_bt_node
    - nav2_path_expiring_timer_condition
    - nav2_distance_traveled_condition_bt_node
    - nav2_single_trigger_bt_node
    - nav2_goal_updated_controller_bt_node
    - nav2_is_battery_low_condition_bt_node
    - nav2_navigate_through_poses_action_bt_node
    - nav2_navigate_to_pose_action_bt_node
    - nav2_remove_passed_goals_action_bt_node
    - nav2_planner_selector_bt_node
    - nav2_controller_selector_bt_node
    - nav2_goal_checker_selector_bt_node
    - nav2_controller_cancel_bt_node
    - nav2_path_longer_on_approach_bt_node
    - nav2_wait_cancel_bt_node
    - nav2_spin_cancel_bt_node
    - nav2_back_up_cancel_bt_node
    - nav2_assisted_teleop_cancel_bt_node
    - nav2_drive_on_heading_cancel_bt_node

bt_navigator_navigate_through_poses_rclcpp_node:
  ros__parameters:
    use_sim_time: True

bt_navigator_navigate_to_pose_rclcpp_node:
  ros__parameters:
    use_sim_time: True

controller_server:
  ros__parameters:
    use_sim_time: True
    controller_frequency: 20.0
    min_x_velocity_threshold: 0.001
    min_y_velocity_threshold: 0.5
    min_theta_velocity_threshold: 0.001
    failure_tolerance: 0.3
    progress_checker_plugin: "progress_checker"
    goal_checker_plugins: ["general_goal_checker"] # "precise_goal_checker"
    controller_plugins: ["FollowPath"]

    # Progress checker parameters
    progress_checker:
      plugin: "nav2_controller::SimpleProgressChecker"
      required_movement_radius: 0.5
      movement_time_allowance: 10.0
    # Goal checker parameters
    #precise_goal_checker:
    #  plugin: "nav2_controller::SimpleGoalChecker"
    #  xy_goal_tolerance: 0.25
    #  yaw_goal_tolerance: 0.25
    #  stateful: True
    general_goal_checker:
      stateful: True
      plugin: "nav2_controller::SimpleGoalChecker"
      xy_goal_tolerance: 0.25
      yaw_goal_tolerance: 0.25
    # DWB parameters
    FollowPath:
      plugin: "dwb_core::DWBLocalPlanner"
      debug_trajectory_details: True
      min_vel_x: 0.0
      min_vel_y: 0.0
      max_vel_x: 0.26
      max_vel_y: 0.0
      max_vel_theta: 1.0
      min_speed_xy: 0.0
      max_speed_xy: 0.26
      min_speed_theta: 0.0
      # Add high threshold velocity for turtlebot 3 issue.
      # https://github.com/ROBOTIS-GIT/turtlebot3_simulations/issues/75
      acc_lim_x: 2.5
      acc_lim_y: 0.0
      acc_lim_theta: 3.2
      decel_lim_x: -2.5
      decel_lim_y: 0.0
      decel_lim_theta: -3.2
      vx_samples: 20
      vy_samples: 5
      vtheta_samples: 20
      sim_time: 1.7
      linear_granularity: 0.05
      angular_granularity: 0.025
      transform_tolerance: 0.2
      xy_goal_tolerance: 0.25
      trans_stopped_velocity: 0.25
      short_circuit_trajectory_evaluation: True
      stateful: True
      critics: ["RotateToGoal", "Oscillation", "BaseObstacle", "GoalAlign", "PathAlign", "PathDist", "GoalDist"]
      BaseObstacle.scale: 0.02
      PathAlign.scale: 32.0
      PathAlign.forward_point_distance: 0.1
      GoalAlign.scale: 24.0
      GoalAlign.forward_point_distance: 0.1
      PathDist.scale: 32.0
      GoalDist.scale: 24.0
      RotateToGoal.scale: 32.0
      RotateToGoal.slowing_factor: 5.0
      RotateToGoal.lookahead_time: -1.0

local_costmap:
  local_costmap:
    ros__parameters:
      update_frequency: 5.0
      publish_frequency: 2.0
      global_frame: odom
      robot_base_frame: base_link
      use_sim_time: True
      rolling_window: true
      width: 3
      height: 3
      resolution: 0.05
      robot_radius: 0.22
      plugins: ["static_layer", "stvl_layer"]
      stvl_layer:
        plugin: "nav2_costmap_2d::spatio_temporal_voxel_layer/SpatioTemporalVoxelLayer"
        enabled: true
        voxel_decay: 15.
        decay_model: 0
        voxel_size: 0.05
        track_unknown_space: true
        unknown_threshold: 15
        mark_threshold: 0
        update_footprint_enabled: true
        combination_method: 1
        origin_z: 0.0
        publish_voxel_map: true
        transform_tolerance: 0.2
        mapping_mode: false
        map_save_duration: 60.0
        observation_sources: pointcloud
        pointcloud:
          data_type: PointCloud2
          topic: /zed2i/zed_node/point_cloud/cloud_registered
          marking: true
          clearing: true
          obstacle_range: 3.0
          min_obstacle_height: 0.0
          max_obstacle_height: 2.0
          expected_update_rate: 0.0
          observation_persistence: 0.0
          inf_is_valid: false
          filter: "voxel"
          voxel_min_points: 0
          clear_after_reading: true
          max_z: 7.0
          min_z: 0.1
          vertical_fov_angle: 0.8745
          horizontal_fov_angle: 1.048
          decay_acceleration: 15.0
          model_type: 0
      inflation_layer:
        plugin: "nav2_costmap_2d::InflationLayer"
        cost_scaling_factor: 3.0
        inflation_radius: 0.55
      voxel_layer:
        plugin: "nav2_costmap_2d::VoxelLayer"
        enabled: True
        publish_voxel_map: True
        origin_z: 0.0
        z_resolution: 0.05
        z_voxels: 16
        max_obstacle_height: 2.0
        mark_threshold: 0
        observation_sources: scan
        scan:
          topic: /scan
          max_obstacle_height: 2.0
          clearing: True
          marking: True
          data_type: "LaserScan"
          raytrace_max_range: 3.0
          raytrace_min_range: 0.0
          obstacle_max_range: 2.5
          obstacle_min_range: 0.0
      static_layer:
        plugin: "nav2_costmap_2d::StaticLayer"
        map_subscribe_transient_local: True
      always_send_full_costmap: True

global_costmap:
  global_costmap:
    ros__parameters:
      update_frequency: 1.0
      publish_frequency: 1.0
      global_frame: map
      robot_base_frame: base_link
      use_sim_time: True
      robot_radius: 0.22
      resolution: 0.05
      track_unknown_space: true
      plugins: ["static_layer", "stvl_layer"]
      stvl_layer:
        plugin: "nav2_costmap_2d::spatio_temporal_voxel_layer/SpatioTemporalVoxelLayer"
        enabled: true
        voxel_decay: 15.
        decay_model: 0
        voxel_size: 0.05
        track_unknown_space: true
        unknown_threshold: 15
        mark_threshold: 0
        update_footprint_enabled: true
        combination_method: 1
        origin_z: 0.0
        publish_voxel_map: true
        transform_tolerance: 0.2
        mapping_mode: false
        map_save_duration: 60.0
        observation_sources: pointcloud
        pointcloud:
          data_type: PointCloud2
          topic: /zed2i/zed_node/point_cloud/cloud_registered
          marking: true
          clearing: true
          obstacle_range: 3.0
          min_obstacle_height: 0.0
          max_obstacle_height: 2.0
          expected_update_rate: 0.0
          observation_persistence: 0.0
          inf_is_valid: false
          filter: "voxel"
          voxel_min_points: 0
          clear_after_reading: true
          max_z: 7.0
          min_z: 0.1
          vertical_fov_angle: 0.8745
          horizontal_fov_angle: 1.048
          decay_acceleration: 15.0
          model_type: 0
      obstacle_layer:
        plugin: "nav2_costmap_2d::ObstacleLayer"
        enabled: True
        observation_sources: scan
        scan:
          topic: /scan
          max_obstacle_height: 2.0
          clearing: True
          marking: True
          data_type: "LaserScan"
          raytrace_max_range: 3.0
          raytrace_min_range: 0.0
          obstacle_max_range: 2.5
          obstacle_min_range: 0.0
      static_layer:
        plugin: "nav2_costmap_2d::StaticLayer"
        map_subscribe_transient_local: True
      inflation_layer:
        plugin: "nav2_costmap_2d::InflationLayer"
        cost_scaling_factor: 3.0
        inflation_radius: 0.55
      always_send_full_costmap: True

map_server:
  ros__parameters:
    use_sim_time: True
    # Overridden in launch by the "map" launch configuration or provided default value.
    # To use in yaml, remove the default "map" value in the tb3_simulation_launch.py file & provide full path to map below.
    yaml_filename: ""

map_saver:
  ros__parameters:
    use_sim_time: True
    save_map_timeout: 5.0
    free_thresh_default: 0.25
    occupied_thresh_default: 0.65
    map_subscribe_transient_local: True

planner_server:
  ros__parameters:
    expected_planner_frequency: 20.0
    use_sim_time: True
    planner_plugins: ["GridBased"]
    GridBased:
      plugin: "nav2_navfn_planner/NavfnPlanner"
      tolerance: 0.5
      use_astar: false
      allow_unknown: true

smoother_server:
  ros__parameters:
    use_sim_time: True
    smoother_plugins: ["simple_smoother"]
    simple_smoother:
      plugin: "nav2_smoother::SimpleSmoother"
      tolerance: 1.0e-10
      max_its: 1000
      do_refinement: True

behavior_server:
  ros__parameters:
    costmap_topic: local_costmap/costmap_raw
    footprint_topic: local_costmap/published_footprint
    cycle_frequency: 10.0
    behavior_plugins: ["spin", "backup", "drive_on_heading", "assisted_teleop", "wait"]
    spin:
      plugin: "nav2_behaviors/Spin"
    backup:
      plugin: "nav2_behaviors/BackUp"
    drive_on_heading:
      plugin: "nav2_behaviors/DriveOnHeading"
    wait:
      plugin: "nav2_behaviors/Wait"
    assisted_teleop:
      plugin: "nav2_behaviors/AssistedTeleop"
    global_frame: odom
    robot_base_frame: base_link
    transform_tolerance: 0.1
    use_sim_time: true
    simulate_ahead_time: 2.0
    max_rotational_vel: 1.0
    min_rotational_vel: 0.4
    rotational_acc_lim: 3.2

robot_state_publisher:
  ros__parameters:
    use_sim_time: True

waypoint_follower:
  ros__parameters:
    use_sim_time: True
    loop_rate: 20
    stop_on_failure: false
    waypoint_task_executor_plugin: "wait_at_waypoint"
    wait_at_waypoint:
      plugin: "nav2_waypoint_follower::WaitAtWaypoint"
      enabled: True
      waypoint_pause_duration: 200

velocity_smoother:
  ros__parameters:
    use_sim_time: True
    smoothing_frequency: 20.0
    scale_velocities: False
    feedback: "OPEN_LOOP"
    max_velocity: [0.26, 0.0, 1.0]
    min_velocity: [-0.26, 0.0, -1.0]
    max_accel: [2.5, 0.0, 3.2]
    max_decel: [-2.5, 0.0, -3.2]
    odom_topic: "odom"
    odom_duration: 0.1
    deadband_velocity: [0.0, 0.0, 0.0]
    velocity_timeout: 1.0

The nav2 nodes succesfully launched but it has error in this part:

[bt_navigator-5] [ERROR] [1688958789.844996049] [bt_navigator]: Exception when loading BT: basic_string::_M_create
[bt_navigator-5] [ERROR] [1688958789.845054066] [bt_navigator]: Error loading XML file: /opt/ros/humble/share/nav2_bt_navigator/behavior_trees/navigate_through_poses_w_replanning_and_recovery.xml
[lifecycle_manager-8] [ERROR] [1688958789.845386197] [lifecycle_manager_navigation]: Failed to change state for node: bt_navigator
[lifecycle_manager-8] [ERROR] [1688958789.845442491] [lifecycle_manager_navigation]: Failed to bring up all requested nodes. Aborting bringup.

What is wrong with my configurations?

This is an issue with Nav2 configuration. I suggest you ask on ROS forums:

@Myzhar Following up on your comment that ZED was working on a module for 2D map generation. Has that been implemented?