Hi,
We’re connecting a Linux computer to a KUKA robot (ethernet cable) and a ZED2i camera (c-type cable). However, we are facing an issue - both devices can’t be tethered within the same ROS2 domain.
Find more details here: UDP communication interference between ZED2i and Robot arm via ROS2 · Issue #190 · stereolabs/zed-ros2-wrapper · GitHub
UDP communication interferece between ZED2i and Robot arm via ROS2 · Issue #190 · stereolabs/zed-ros2-wrapper
Preliminary Checks This issue is not a duplicate. Before opening a new issue, please search existing issues. This issue is not a question, feature request, or anything other than a bug report direc…
Everything runs smoothly when connected solely to the robot; robot simulation control is seamless. On the other hand, without a robot connection, all the ZED tools are working flawlessly. But, when the ZED2i camera comes into play with robot connection, all active terminals start spitting out the following:
[control_node-1] 1698357420.879862 [0] tev: ddsi_udp_conn_write to udp/239.255.0.1:7400 failed with retcode -1
1698357420.902612 [0] tev: ddsi_udp_conn_write to udp/239.255.0.1:7400 failed with retcode -1
[robot_manager_node-2] 1698357420.979563 [0] tev: ddsi_udp_conn_write to udp/239.255.0.1:7400 failed with retcode -1
[robot_manager_node-2] 1698357420.979697 [0] tev: ddsi_udp_conn_write to udp/239.255.0.1:7400 failed with retcode -1
[control_node-1] 1698357420.979805 [0] tev: ddsi_udp_conn_write to udp/239.255.0.1:7400 failed with retcode -1
[control_node-1] 1698357420.979821 [0] tev: ddsi_udp_conn_write to udp/239.255.0.1:7400 failed with retcode -1
1698357421.002722 [0] tev: ddsi_udp_conn_write to udp/239.255.0.1:7400 failed with retcode -1
[robot_manager_node-2] 1698357421.079865 [0] tev: ddsi_udp_conn_write to udp/239.255.0.1:7400 failed with retcode -1
[control_node-1] 1698357421.079892 [0] tev: ddsi_udp_conn_write to udp/239.255.0.1:7400 failed with retcode -1
1698357421.102879 [0] tev: ddsi_udp_conn_write to udp/239.255.0.1:7400 failed with retcode -1
[control_node-1] 1698357421.179963 [0] tev: ddsi_udp_conn_write to udp/239.255.0.1:7400 failed with retcode -1
[robot_manager_node-2] 1698357421.180049 [0] tev: ddsi_udp_conn_write to udp/239.255.0.1:7400 failed with retcode -1
1698357421.202999 [0] tev: ddsi_udp_conn_write to udp/239.255.0.1:7400 failed with retcode -1
We attempted a workaround by utilizing ROS DOMAIN_ID. DOMAIN_ID = 1 for Kuka and DOMAIN_ID = 2 for the ZED 2i camera, but it proved ineffective. If you’ve successfully linked a robot with any sensors before, could you share your approach to setting IPs or interface configuration for each machine? Alternatively, if you’re familiar with the error mentioned above, any guidance would be highly appreciated. Thank you!