[ROS2 Wrapper] 4 ZED2i cameras same device in docker container

The ZED 2i when connected to the USB port creates two devices:

  • 2b03:f880 → UVC video module (USB3)
  • 2b03:f881 → HID sensors data module (USB2)

The fact that when you connect one camera another one stops to work make me think that this is also a power issue.

@adujardin already suggested to be sure that the expansion cards are correctly powered. Is the power configuration correct?