Ros2 rviz2 example not working on Jetson AGX Orin Dev Kit with ZED 2i

hi,

I’m trying to follow the tutorial here to config ROS2 on Jetson AGX Orin Dev Kit

Installation of ROS2 and ZED ROS2 wrapper were successful.

When I try to run the rviz example on new ZED 2i camera using following cli

ros2 launch zed_display_rviz2 display_zed2i.launch.py

Rviz launched with error, see screen grab

Error in the terminal:

[zed_wrapper-3] 1685969951.245337512 [zed2.zed_node] [INFO] ***** STARTING CAMERA *****
[zed_wrapper-3] 1685969951.245352808 [zed2.zed_node] [INFO] ZED SDK Version: 4.0.3 - Build 72471_a14c21bc
[zed_wrapper-3] 1685969951.248521215 [zed2.zed_node] [INFO] *** CAMERA OPENING ***
[rviz2-1] 1685969952.056706918 [rviz2] [INFO] Stereo is NOT SUPPORTED
[rviz2-1] 1685969952.057105481 [rviz2] [INFO] OpenGl version: 4.6 (GLSL 4.6)
[rviz2-1] 1685969952.110045326 [rviz2] [INFO] Stereo is NOT SUPPORTED
[rviz2-1] 1685969952.196258118 [rviz2] [ERROR] PluginlibFactory: The plugin for class 'grid_map_rviz_plugin/GridMap' failed to load. Error: According to the loaded plugin descriptions the class grid_map_rviz_plugin/GridMap with base class type rviz_common::Display does not exist. Declared types are  rviz_default_plugins/Axes rviz_default_plugins/Camera rviz_default_plugins/FluidPressure rviz_default_plugins/Grid rviz_default_plugins/GridCells rviz_default_plugins/Illuminance rviz_default_plugins/Image rviz_default_plugins/InteractiveMarkers rviz_default_plugins/LaserScan rviz_default_plugins/Map rviz_default_plugins/Marker rviz_default_plugins/MarkerArray rviz_default_plugins/Odometry rviz_default_plugins/Path rviz_default_plugins/PointCloud rviz_default_plugins/PointCloud2 rviz_default_plugins/PointStamped rviz_default_plugins/Polygon rviz_default_plugins/Pose rviz_default_plugins/PoseArray rviz_default_plugins/PoseWithCovariance rviz_default_plugins/Range rviz_default_plugins/RelativeHumidity rviz_default_plugins/RobotModel rviz_default_plugins/TF rviz_default_plugins/Temperature rviz_default_plugins/Wrench rviz_plugin_zed_od/ZedOdDisplay
[rviz2-1] Warning: Invalid frame ID "map" passed to canTransform argument target_frame - frame does not exist

Did I miss some configuration?

Hi @Jian
you must install the ros-humble-grid-map-rviz-plugin package:
sudo apt install ros-humble-grid-map-rviz-plugin

Hi,

Thank you for the prompt reply.

I am using ros2 foxy, will try foxy equivalent plugin amd let you know.

However, the plugin is not required. You can remove the Local Grid Map object and save to not see that warning anymore:
image
I suppose the problem that you are facing is something different.
Does the command
ros2 launch zed_wrapper zed2i.launch.py
work correctly?

hi, just tested above command

ros2 launch zed_wrapper zed2i.launch.py

It works. It downloaded the model and optimized it. After it, the rviz2 command starts to work as well.

I couldn’t find a way to install grid-map-rviz-plugin on ros foxy. local grid map is unchecked.