Hey I’m trying to install the examples in the same workspace as the Wrapper but it says it cant locate the “grid_map_msgs”.
Here the build output :
CMake Error at CMakeLists.txt:61 (find_package):
By not providing “Findgrid_map_msgs.cmake” in CMAKE_MODULE_PATH this
project has asked CMake to find a package configuration file provided by
“grid_map_msgs”, but CMake did not find one.
Could not find a package configuration file provided by “grid_map_msgs”
with any of the following names:
grid_map_msgsConfig.cmake
grid_map_msgs-config.cmake
Add the installation prefix of “grid_map_msgs” to CMAKE_PREFIX_PATH or set
“grid_map_msgs_DIR” to a directory containing one of the above files. If
“grid_map_msgs” provides a separate development package or SDK, be sure it
has been installed.
Failed <<< zed_nav2 [12.1s, exited with code 1]
Aborted <<< zed_topic_benchmark_component [3.72s]
Aborted <<< zed_tutorial_video [10.6s]
Aborted <<< zed_components [10.3s]
Aborted <<< zed_tutorial_depth [36.2s]
Aborted <<< zed_tutorial_pos_tracking [46.3s]
Summary: 6 packages finished [51.5s]
1 package failed: zed_nav2
5 packages aborted: zed_components zed_topic_benchmark_component zed_tutorial_depth zed_tutorial_pos_tracking zed_tutorial_video
2 packages had stderr output: zed_nav2 zed_topic_benchmark_component
8 packages not processed
bart@ubuntu:~/ros2_ws$