ZED360 multi-cam calibration improvement

Hello Stereolabs team,

I have started to work with your SDK and its pretty awesome what we can we do with it. The amount of functionality and control we have in most modules is super handy.

I’m setting up a multi-camera setup, with two ZED2i cameras facing each other, angled downwards and approximately 3.6m apart, with pretty good lighting. Additionally, they share a pretty good FOV (> 40%).

They are also both locally connected to a Jetson ORIN NX and their purpose is inspecting static objects to create accurate pointclouds.

My issue is that I have been trying the past few days to get a good extrinsic calibration with ZED360 and even at those pretty-good conditions, I get a mismatch particularly in the XY plane, of around ±15cm. This unfortunately is not acceptable for my application and I was wondering if you have any suggestions to improve the accuracy. I have fiddled around with the room settings and played with both NEURAL and ULTRA models, while moving very slowly everywhere in the scene, for more than 1 minute. No matter what settings I use I get a very similar calibration output, which is not correct.

Any ideas what I can do to improve the ZED360 calibration? Is there any way I can increase the camera resolution from the default HD720? I would expect calibration inaccuracy to be below the cm level at these conditions.

Sample output from the Fusion API:

Im using the stereolabs/zed:5.0-tools-devel-l4t-r36.4 docker image for the ZED360 tool.

Thanks a lot!

Hi,

In that case, when both cameras are facing each other, you might get a more accurate calibration by using a classic calibration method based on aruco detection.
You can use this sample: zed-aruco/multi-camera at master · stereolabs/zed-aruco · GitHub
to perform the calibration.

Hi Benjamin, thanks for the quick reply. I was not aware of this, will definitely give it a try and post the results :slight_smile: !

I’ll push internally to add this option in ZED360 so you can directly choose between both methods.

Thanks for the feedback.

Stereolabs Support

Hi again Benjamin. Having managed to run the zed-aruco sample with a 655mm ARUCO marker in the same setup, I am facing the same issue as this thread: Zed-aruco not calibrating correctly for multi-camera

Im wondering, if this is something you would be looking to fix?

Best