Zed2i ros2 wrapper launch "pos tracking required" messages filling logs

Hi, I’m seeing the following messages fill the log output after launching the camera and I am wondering if this is expected or if the configuration is wrong.

[zed_wrapper-1] [DEBUG] [1675960517.167128887] [rail_right_zed2i.zed_node]: POS. TRACKING required: enabled by param.
[zed_wrapper-1] [DEBUG] [1675960517.167143493] [rail_right_zed2i.zed_node]: Depth extraction enabled
[zed_wrapper-1] [DEBUG] [1675960517.167152301] [rail_right_zed2i.zed_node]: POS. TRACKING required: enabled by param.

the following is my configuration yaml:

# config/common_yaml
# Common parameters to Stereolabs ZED and ZED mini cameras
#
# Note: the parameter svo_file is passed as exe argumet
---
/**:
    ros__parameters:
        general:
            svo_file: "" # usually overwritten by launch file
            svo_loop: false # Enable loop mode when using an SVO as input source
            svo_realtime: false # if true SVO will be played trying to respect the original framerate eventually skipping frames, otherwise every frame will be processed respecting the `pub_frame_rate` setting
            camera_timeout_sec: 10
            camera_max_reconnect: 10
            camera_flip: false
            zed_id: 0
            serial_number: 32972525
            resolution: 0 # '0': HD2K, '1': HD1080, '2': HD720, '3': VGA
            sdk_verbose: 1
            grab_frame_rate: 15 # ZED SDK internal grabbing rate
            pub_frame_rate: 10.0 # [DYNAMIC] - frequency of publishing of visual images and depth images
            gpu_id: -1
            region_of_interest: "" # A polygon defining the ROI where the ZED SDK perform the processing ignoring the rest. Coordinates must be normalized to '1.0' to be resolution independent.
        
        video:
            extrinsic_in_camera_frame: false # if `false` extrinsic parameter in `camera_info` will use ROS native frame (X FORWARD, Z UP) instead of the camera frame (Z FORWARD, Y DOWN) [`true` use old behavior as for version < v3.1]
            img_downsample_factor: 1.0 # Resample factor for image data matrices [0.01,1.0] The SDK works with native data sizes, but publishes rescaled matrices
            brightness: 4 # [DYNAMIC]
            contrast: 4 # [DYNAMIC]
            hue: 0 # [DYNAMIC]
            saturation: 4 # [DYNAMIC]
            sharpness: 4 # [DYNAMIC]
            gamma: 8 # [DYNAMIC] - Requires SDK >=v3.1
            auto_exposure_gain: true # [DYNAMIC]
            exposure: 80 # [DYNAMIC]
            gain: 80 # [DYNAMIC]
            auto_whitebalance: true # [DYNAMIC]
            whitebalance_temperature: 42 # [DYNAMIC] - [28,65] works only if `auto_whitebalance` is false
            qos_history: 1 # '1': KEEP_LAST - '2': KEEP_ALL
            qos_depth: 1 # Queue size if using KEEP_LAST
            qos_reliability: 2 # '1': RELIABLE - '2': BEST_EFFORT -
            qos_durability: 2 # '1': TRANSIENT_LOCAL - '2': VOLATILE

        depth:
            quality: 3 # '0': NONE, '1': PERFORMANCE, '2': QUALITY, '3': ULTRA - '4': NEURAL - Note: if '0' all the modules that requires depth extraction are disabled by default (Pos. Tracking, Obj. Detection, Mapping, ...)
            sensing_mode: 1 # '0': STANDARD, '1': FILL
            depth_stabilization: true # Forces positional tracking to start if 'true'
            openni_depth_mode: false # 'false': 32bit float [meters], 'true': 16bit unsigned int [millimeters]
            depth_downsample_factor: 1.0 # Resample factor for depth data matrices [0.01,1.0] The SDK works with native data sizes, but publishes rescaled matrices (depth map, point cloud, ...)
            # I suspect we can lower the poin cloud frequency because we are not using point clouds right now.
            point_cloud_freq: 1.0 # [DYNAMIC] - frequency of the pointcloud publishing (equal or less to `grab_frame_rate` value) 
            depth_confidence: 100 # [DYNAMIC]
            depth_texture_conf: 100 # [DYNAMIC]
            remove_saturated_areas: true # [DYNAMIC]
            qos_history: 1 # '1': KEEP_LAST - '2': KEEP_ALL
            qos_depth: 1 # Queue size if using KEEP_LAST
            qos_reliability: 2 # '1': RELIABLE - '2': BEST_EFFORT -
            qos_durability: 2 # '1': TRANSIENT_LOCAL only applies to Datawriters and datareaders - '2': VOLATILE means that no attempt is made to persist samples

        pos_tracking:
            pos_tracking_enabled: true # True to enable positional tracking from start
            imu_fusion: true # enable/disable IMU fusion. When set to false, only the optical odometry will be used.
            publish_tf: false # publish `odom -> base_link` TF
            publish_map_tf: false # publish `map -> odom` TF
            publish_imu_tf: true # enable/disable the IMU TF broadcasting
            base_frame: "base_link" # use the same name as in the URDF file
            map_frame: "map"
            odometry_frame: "odom"
            area_memory_db_path: ""
            area_memory: true # Enable to detect loop closure
            depth_min_range: 0.0 # Set this value for removing fixed zones of the robot in the FoV of the camerafrom the visual odometry evaluation
            set_gravity_as_origin: false # If 'true' align the positional tracking world to imu gravity measurement. Keep the yaw from the user initial pose.
            floor_alignment: false # Enable to automatically calculate camera/floor offset
            initial_base_pose: [0.0, 0.0, 0.0, 0.0, 0.0, 0.0] # Initial position of the `base_frame` -> [X, Y, Z, R, P, Y]
            init_odom_with_first_valid_pose: true # Enable to initialize the odometry with the first valid pose
            path_pub_rate: 2.0 # [DYNAMIC] - Camera trajectory publishing frequency
            path_max_count: 10 # use '-1' for unlimited path size
            two_d_mode: false # Force navigation on a plane. If true the Z value will be fixed to "fixed_z_value", roll and pitch to zero
            fixed_z_value: 0.00 # Value to be used for Z coordinate if `two_d_mode` is true
            qos_history: 1 # '1': KEEP_LAST - '2': KEEP_ALL
            qos_depth: 1 # Queue size if using KEEP_LAST
            qos_reliability: 2 # '1': RELIABLE - '2': BEST_EFFORT -
            qos_durability: 2 # '1': TRANSIENT_LOCAL - '2': VOLATILE
            transform_time_offset: 0.0 # The value added to the timestamp of `map->odom` and `odom->base_link`` transform being generated

        mapping:
            mapping_enabled: false # True to enable mapping and fused point cloud pubblication
            resolution: 0.1 # maps resolution in meters [0.01f, 0.2f]
            max_mapping_range: 20.0 # maximum depth range while mapping in meters (-1 for automatic calculation) [2.0, 20.0]
            fused_pointcloud_freq: 0.5 # frequency of the publishing of the fused colored point cloud
            clicked_point_topic: "/clicked_point" # Topic published by Rviz when a point of the cloud is clicked. Used for plane detection
            qos_history: 1 # '1': KEEP_LAST - '2': KEEP_ALL
            qos_depth: 1 # Queue size if using KEEP_LAST
            qos_reliability: 2 # '1': RELIABLE - '2': BEST_EFFORT -
            qos_durability: 2 # '1': TRANSIENT_LOCAL - '2': VOLATILE

        sensors:
            sensors_image_sync: false # Synchronize Sensors messages with latest published video/depth message
            sensors_pub_rate: 200. # frequency of publishing of sensors data. MAX: 400. - MIN: grab rate
            qos_history: 1 # '1': KEEP_LAST - '2': KEEP_ALL
            qos_depth: 1 # Queue size if using KEEP_LAST
            qos_reliability: 2 # '1': RELIABLE - '2': BEST_EFFORT -
            qos_durability: 2 # '1': TRANSIENT_LOCAL - '2': VOLATILE

        object_detection:
            od_enabled: false # True to enable Object Detection [only ZED 2]
            confidence_threshold: 50.0 # [DYNAMIC] - Minimum value of the detection confidence of an object [0,100]
            prediction_timeout: 0.5 # During this time [sec], the object will have OK state even if it is not detected. Set this parameter to 0 to disable SDK predictions
            model: 0 # '0': MULTI_CLASS_BOX - '1': MULTI_CLASS_BOX_ACCURATE - '2': HUMAN_BODY_FAST - '3': HUMAN_BODY_ACCURATE - '4': MULTI_CLASS_BOX_MEDIUM - '5': HUMAN_BODY_MEDIUM - '6': PERSON_HEAD_BOX
            filtering_mode: 1 # '0': NONE - '1': NMS3D - '2': NMS3D_PER_CLASS
            mc_people: true # [DYNAMIC] - Enable/disable the detection of persons for 'MULTI_CLASS_X' models
            mc_vehicle: true # [DYNAMIC] - Enable/disable the detection of vehicles for 'MULTI_CLASS_X' models
            mc_bag: true # [DYNAMIC] - Enable/disable the detection of bags for 'MULTI_CLASS_X' models
            mc_animal: true # [DYNAMIC] - Enable/disable the detection of animals for 'MULTI_CLASS_X' models
            mc_electronics: true # [DYNAMIC] - Enable/disable the detection of electronic devices for 'MULTI_CLASS_X' models
            mc_fruit_vegetable: true # [DYNAMIC] - Enable/disable the detection of fruits and vegetables for 'MULTI_CLASS_X' models
            mc_sport: true # [DYNAMIC] - Enable/disable the detection of sport-related objects for 'MULTI_CLASS_X' models
            body_fitting: true # Enable/disable body fitting for 'HUMAN_BODY_FAST' and 'HUMAN_BODY_ACCURATE' models
            body_format: 1 # '0': POSE_18 - '1': POSE_34 [Only if `HUMAN_BODY_*` model is selected]
            qos_history: 1 # '1': KEEP_LAST - '2': KEEP_ALL
            qos_depth: 1 # Queue size if using KEEP_LAST
            qos_reliability: 2 # '1': RELIABLE - '2': BEST_EFFORT
            qos_durability: 2 # '1': TRANSIENT_LOCAL - '2': VOLATILE

        debug:
            debug_mode: True # we may want to consider having two copies of this file. one for debug and one for operation.
            debug_sensors: false

Please set debug_mode to false