Hi, we are running some tests with Zed X on Orin Zed Box but in some cases the camera fails the Diagnostic Test…It seems that on the outside it fails and on the insider it runs
The outside temperature is around 8 degrees. Here is the Diagnostic file.
Hi, I have Orin and I wrote: ‘apt-cache show nvidia-l4t-core | grep Version’ and I get 36.4.3-20250107174145 so I install ZED SDK for JetPack 6.1 and 6.2 (L4T 36.4) 5.2 (Jetson Orin, CUDA 12.6)?
I have a ZED x mini, Zed capture card duo and a Jetson orin nano dev kit and I’m experiencing the exact same issue with the temperature.
With 22 degrees inside it works, then when I go outside with 10 degrees and I get the stream fail error ([2026-05-14 15:18:57 UTC][ZED][ERROR] CAMERA STREAM FAILED TO START in sl::ERROR_CODE sl::open(sl::InitParameters)).
Any idea on how to solve this? The camera is sold with an operating range of -20 to 55 degrees and I would expect it to work easily at 10 degrees…