Hi all,
I have a SeeedStudio j4012 recomputer witha Orin NX 16GB mounted on their j401 carrier board. It came with Jetpack 5.1.1, the Zed SDK and Driver installed fine on that and my Zed X + Mono capture card combo worked fine.
However, there were OpenGL freeglut errors and viewer issues on some of the demos (namely birds_eye_viewer). So I decided to upgrade to Jetpack 6.
Jetpack 6 is installed, but it looks like there’s a driver issue, on boot I see that there is a failed to open /boot/tegra234-j401-camera-zedlink-mono-sl-overlay.dtbo file error, so I think driver installation is going wrong?
dmesg diagnostic output below:
Created: Mon Aug 19 2024
###########################################
############ DMESG [ZEDX] LOG #############
###########################################
[ 15.234512] sl_zedx: disagrees about version of symbol tegracam_v4l2subdev_unregister
[ 15.234521] sl_zedx: Unknown symbol tegracam_v4l2subdev_unregister (err -22)
[ 15.234562] sl_zedx: disagrees about version of symbol tegracam_v4l2subdev_register
[ 15.234563] sl_zedx: Unknown symbol tegracam_v4l2subdev_register (err -22)
[ 15.234573] sl_zedx: disagrees about version of symbol tegracam_device_unregister
[ 15.234574] sl_zedx: Unknown symbol tegracam_device_unregister (err -22)
[ 15.234602] sl_zedx: disagrees about version of symbol tegracam_get_privdata
[ 15.234603] sl_zedx: Unknown symbol tegracam_get_privdata (err -22)
[ 15.234617] sl_zedx: disagrees about version of symbol camera_common_mclk_enable
[ 15.234618] sl_zedx: Unknown symbol camera_common_mclk_enable (err -22)
[ 15.234626] sl_zedx: disagrees about version of symbol tegracam_set_privdata
[ 15.234627] sl_zedx: Unknown symbol tegracam_set_privdata (err -22)
[ 15.234633] sl_zedx: disagrees about version of symbol tegracam_device_register
[ 15.234633] sl_zedx: Unknown symbol tegracam_device_register (err -22)
[ 15.268552] sl_zedxone_uhd: disagrees about version of symbol tegracam_v4l2subdev_unregister
[ 15.268562] sl_zedxone_uhd: Unknown symbol tegracam_v4l2subdev_unregister (err -22)
[ 15.268603] sl_zedxone_uhd: disagrees about version of symbol camera_common_g_ctrl
[ 15.268604] sl_zedxone_uhd: Unknown symbol camera_common_g_ctrl (err -22)
[ 15.268620] sl_zedxone_uhd: disagrees about version of symbol tegracam_v4l2subdev_register
[ 15.268621] sl_zedxone_uhd: Unknown symbol tegracam_v4l2subdev_register (err -22)
[ 15.268629] sl_zedxone_uhd: disagrees about version of symbol tegracam_device_unregister
[ 15.268630] sl_zedxone_uhd: Unknown symbol tegracam_device_unregister (err -22)
[ 15.268715] sl_zedxone_uhd: disagrees about version of symbol tegracam_get_privdata
[ 15.268717] sl_zedxone_uhd: Unknown symbol tegracam_get_privdata (err -22)
[ 15.268735] sl_zedxone_uhd: disagrees about version of symbol camera_common_mclk_enable
[ 15.268735] sl_zedxone_uhd: Unknown symbol camera_common_mclk_enable (err -22)
[ 15.268743] sl_zedxone_uhd: disagrees about version of symbol camera_common_mclk_disable
[ 15.268744] sl_zedxone_uhd: Unknown symbol camera_common_mclk_disable (err -22)
[ 15.268749] sl_zedxone_uhd: disagrees about version of symbol tegracam_set_privdata
[ 15.268750] sl_zedxone_uhd: Unknown symbol tegracam_set_privdata (err -22)
[ 15.268756] sl_zedxone_uhd: disagrees about version of symbol tegracam_device_register
[ 15.268757] sl_zedxone_uhd: Unknown symbol tegracam_device_register (err -22)
###########################################
############ DMESG [MAX9x] LOG #############
###########################################
###########################################
############ DMESG [PCA] LOG #############
###########################################
###########################################
############ DMESG [DTS] LOG #############
###########################################
###########################################
############ DTB list original ###########
###########################################
/boot/dtb/kernel_tegra234-j401-p3768-0000+p3767-0000-recomputer.dtb
###########################################
############ DTB list SLabs ###########
###########################################
board.py
extlinux.py
fio.py
Headers
Jetson
Linux
__pycache__
Utils
zlconfig
###########################################
############ EXTlinux file ###########
###########################################
TIMEOUT 30
DEFAULT Stereolabs
MENU TITLE L4T boot options
LABEL primary
MENU LABEL primary kernel
LINUX /boot/Image
INITRD /boot/initrd
APPEND ${cbootargs} root=PARTUUID=4b8a73c4-da72-45a0-bf8e-233d1240f538 rw rootwait rootfstype=ext4 mminit_loglevel=4 console=ttyTCU0,115200 firmware_class.path=/etc/firmware fbcon=map:0 net.ifnames=0 nospectre_bhb video=efifb:off console=tty0
# When testing a custom kernel, it is recommended that you create a backup of
# the original kernel and add a new entry to this file so that the device can
# fallback to the original kernel. To do this:
#
# 1, Make a backup of the original kernel
# sudo cp /boot/Image /boot/Image.backup
#
# 2, Copy your custom kernel into /boot/Image
#
# 3, Uncomment below menu setting lines for the original kernel
#
# 4, Reboot
# LABEL backup
# MENU LABEL backup kernel
# LINUX /boot/Image.backup
# INITRD /boot/initrd
# APPEND ${cbootargs}
LABEL Stereolabs
MENU LABEL Stereolabs kernel
LINUX /boot/Image
FDT /boot/dtb/kernel_tegra234-j401-p3768-0000+p3767-0000-recomputer.dtb
INITRD /boot/initrd
APPEND ${cbootargs} root=PARTUUID=4b8a73c4-da72-45a0-bf8e-233d1240f538 rw rootwait rootfstype=ext4 mminit_loglevel=4 console=ttyTCU0,115200 firmware_class.path=/etc/firmware fbcon=map:0 net.ifnames=0 nospectre_bhb video=efifb:off console=tty0
OVERLAYS /boot/tegra234-j401-camera-zedlink-mono-sl-overlay.dtbo
###########################################
############ Jetpack ###########
###########################################
# R36 (release), REVISION: 3.0, GCID: 36191598, BOARD: generic, EABI: aarch64, DATE: Mon May 6 17:34:21 UTC 2024
# KERNEL_VARIANT: oot
TARGET_USERSPACE_LIB_DIR=nvidia
TARGET_USERSPACE_LIB_DIR_PATH=usr/lib/aarch64-linux-gnu/nvidia
###########################################
############ Dpkg list ###########
###########################################
####################################
############ Driver list ###########
####################################
/usr/lib/modules/5.15.136-tegra/kernel/drivers/stereolabs/max9296/sl_max9296.ko==> exists
/usr/lib/modules/5.15.136-tegra/kernel/drivers/stereolabs/zedx/sl_zedx.ko ==> exists
/usr/lib/modules/5.15.136-tegra/kernel/drivers/stereolabs/zedone4k/sl_zedxone_uhd.ko ==> exists
################################################
############ ZEDX Daemon Status LS #############
################################################
● zed_x_daemon.service - ZED-X Daemon service
Loaded: loaded (/etc/systemd/system/zed_x_daemon.service; enabled; vendor preset: enabled)
Active: active (running) since Mon 2024-08-19 17:43:09 IST; 2min 38s ago
Main PID: 1055 (ZEDX_Daemon)
Tasks: 5 (limit: 18458)
Memory: 12.0M
CPU: 289ms
CGroup: /system.slice/zed_x_daemon.service
└─1055 /usr/sbin/ZEDX_Daemon
Aug 19 17:43:09 orin ZEDX_Daemon[1055]: Tegra release : 9
Aug 19 17:43:09 orin ZEDX_Daemon[1055]: [ "Mon Aug 19 17:43:09 2024" ] ** Searching for Preload file "/etc/systemd/system/zed_x_daemon.preload" : false
Aug 19 17:43:09 orin ZEDX_Daemon[1055]: [ "Mon Aug 19 17:43:09 2024" ] Process "rmmod sl_zedxone_uhd" outputs "rmmod: ERROR: Module sl_zedxone_uhd is not currently loaded\n"
Aug 19 17:43:09 orin ZEDX_Daemon[1055]: [ "Mon Aug 19 17:43:09 2024" ] Process "rmmod sl_zedx" outputs "rmmod: ERROR: Module sl_zedx is not currently loaded\n"
Aug 19 17:43:09 orin ZEDX_Daemon[1055]: [ "Mon Aug 19 17:43:09 2024" ] Process "rmmod sl_max9296" outputs "rmmod: ERROR: Module sl_max9296 is not currently loaded\n"
Aug 19 17:43:09 orin ZEDX_Daemon[1055]: [ "Mon Aug 19 17:43:09 2024" ] Process "insmod /usr/lib/modules/5.15.136-tegra/kernel/drivers/stereolabs/zedx/sl_zedx.ko" outputs "insmod: ERROR: could not insert module /usr/lib/modules/5.15.136-tegra/kernel/drivers/stereolabs/zedx/sl_zedx.ko: Invalid parameters\n"
Aug 19 17:43:09 orin ZEDX_Daemon[1055]: [ "Mon Aug 19 17:43:09 2024" ] Process "insmod /usr/lib/modules/5.15.136-tegra/kernel/drivers/stereolabs/zedone4k/sl_zedxone_uhd.ko" outputs "insmod: ERROR: could not insert module /usr/lib/modules/5.15.136-tegra/kernel/drivers/stereolabs/zedone4k/sl_zedxone_uhd.ko: Invalid parameters\n"
Aug 19 17:43:09 orin ZEDX_Daemon[1055]: ** ZED-X Driver loaded
Aug 19 17:43:09 orin ZEDX_Daemon[1055]: [ "Mon Aug 19 17:43:09 2024" ] ** Searching for Postload file "/etc/systemd/system/zed_x_daemon.postload" : false
Aug 19 17:43:09 orin ZEDX_Daemon[1055]: [ "Mon Aug 19 17:43:09 2024" ] ** Created Endpoint "tcp://127.0.0.1:20026"
################################################
############ I2C Trace [-l] #############
################################################
i2c-0 i2c 3160000.i2c I2C adapter
i2c-1 i2c c240000.i2c I2C adapter
i2c-2 i2c 3180000.i2c I2C adapter
i2c-4 i2c Tegra BPMP I2C adapter I2C adapter
i2c-5 i2c 31b0000.i2c I2C adapter
i2c-7 i2c c250000.i2c I2C adapter
i2c-9 i2c i2c-2-mux (chan_id 1) I2C adapter
i2c-10 i2c i2c-2-mux (chan_id 0) I2C adapter
################################################
############ I2C Trace /dev/i2C-0 #############
################################################
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
50: UU -- -- -- -- -- -- UU -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --
################################################
############ I2C Trace /dev/i2C-1 #############
################################################
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
40: UU -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --
################################################
############ I2C Trace /dev/i2C-2 #############
################################################
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --
################################################
############ I2C Trace /dev/i2C-3 #############
################################################
Error: Could not open file `/dev/i2c-3' or `/dev/i2c/3': No such file or directory
################################################
############ I2C Trace /dev/i2C-4 #############
################################################
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- UU -- -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --
################################################
############ I2C Trace /dev/i2C-5 #############
################################################
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --
################################################
############ I2C Trace /dev/i2C-6 #############
################################################
Error: Could not open file `/dev/i2c-6' or `/dev/i2c/6': No such file or directory
################################################
############ I2C Trace /dev/i2C-7 #############
################################################
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --
################################################
############ I2C Trace /dev/i2C-8 #############
################################################
Error: Could not open file `/dev/i2c-8' or `/dev/i2c/8': No such file or directory
################################################
############ I2C Trace /dev/i2C-9 #############
################################################
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --
################################################
############ I2C Trace /dev/i2C-10 #############
################################################
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --
################################################
############ I2C Trace /dev/i2C-30 #############
################################################
Error: Could not open file `/dev/i2c-30' or `/dev/i2c/30': No such file or directory
################################################
############ I2C Trace /dev/i2C-31 #############
################################################
Error: Could not open file `/dev/i2c-31' or `/dev/i2c/31': No such file or directory
################################################
############ I2C Trace /dev/i2C-32 #############
################################################
Error: Could not open file `/dev/i2c-32' or `/dev/i2c/32': No such file or directory
################################################
############ I2C Trace /dev/i2C-33 #############
################################################
Error: Could not open file `/dev/i2c-33' or `/dev/i2c/33': No such file or directory
#########################
Additionally, I went into the boot folder, found a file from the driver called /boot/tegra234-3738-camera-zedlink-mono-sl-overlay.dtbo, and renamed it to /boot/tegra234-j401-camera-zedlink-mono-sl-overlay.dtbo - then doing sudo dmesg | grep zedx I saw a camera connected message for a new sl_max9296… line - however still behaviour did not change and I cannot run any examples etc.