ZED X Connection/Argus issues

Hello.
I’m trying to work with my setup of Zed X with a GMSL board (ZED Link Capture Card Mono) connected to a Jetson Orin Nano Devkit. I’m facing the dreaded Argus Timeout error, but it does not seem consistent. Sometimes, the tools included with the SDK work fine, sometimes they stop working after some time passes, and sometimes they immediately crash with:

(Argus) Error Timeout:  (propagating from src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 137)
(Argus) Error Timeout:  (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 91)

or

[2025-11-18 12:42:50 UTC][ZED][INFO] Logging level INFO
[2025-11-18 12:42:51 UTC][ZED][INFO] Using GMSL input... Switched to default resolution HD1200
[2025-11-18 12:42:52 UTC][ZED][INFO] [Init]  Camera FW version: 2001
[2025-11-18 12:42:52 UTC][ZED][INFO] [Init]  Video mode: HD1200@30
[2025-11-18 12:42:52 UTC][ZED][INFO] [Init]  Serial Number: S/N 41165475
[2025-11-18 12:42:52 UTC][ZED][INFO] [Init]  Depth mode: NEURAL LIGHT
(Argus) Error Timeout:  (propagating from src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 137)
(Argus) Error Timeout:  (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 92)
(Argus) Error Timeout:  (propagating from src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 137)
(Argus) Error Timeout:  (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 92)
[2025-11-18 12:43:22 UTC][ZED][ERROR] [Init]  Corrupted frames detected. Check that your camera is connected properly.
[2025-11-18 12:43:26 UTC][ZED][ERROR] FAILURE in sl::ERROR_CODE sl::Camera::open(sl::InitParameters)

The same goes for the diagnostic tool - the diagnostic sometimes passes saying that everything should be working fine, when the camera is clearly not initialized, or right as Argus is throwing socket reading errors:

So far I have tried downgrading JetPack and L4T, different versions of SDK and driver, but this behavior remains consistently inconsistent.

At one point I managed to get far enough by restarting nvargus and zed_x daemons, but when I actually tried to do something with the output itself - by running the ros2 wrapper, it seemed to work, before hanging on ‘CAMERA REBOOTING’ (it didn’t). I was following this tutorial: Setting up Isaac™ ROS to work with ZED Cameras in ROS 2 - Stereolabs

My general assumptions/questions are:

  • Can this be caused by software incompatibilities? Something like a patch version difference in L4T and SDK requirements? Incorrectly installed drivers? The checks pass both during installation and diagnostics though.
  • Can this be a hardware issue? I’m not very experienced at tinkering with Jetson hardware, but I did follow the tutorials provided by NVIDIA. Jetson is set to MAXN SUPER mode and should be configured correctly.

I’m also including a diagnostics report:
https://drive.google.com/file/d/1waM2qc8j8K1lbXiv93SyQI65FKdkqUkC/view?usp=sharing

Any idea what could I be doing wrong? Thanks.

Hi @TSB17
Please verify that the ribbon cable of the ZED Link Mono capture card is stably connected to the carrier board and to the capture card.

Are you using the original cable or a longer cable?

Furthermore, what settings are you using with the Jetson Orin Nano?
It’s not a powerful board, if you overload it the stability of the connection can be compromised.

I’ve just noticed this… try to lower the resolution.

Hello @Myzhar, thank you for your quick response.

I’m sorry if this is answered elsewhere, but I cannot seem to understand how to change the default parameters such as resolution, as I don’t see them referenced in the config files as they are referenced in the terminal readout.
Previously, I could edit the camera parameters using the GUI tools, but they only allow you to change anything when the camera is fully initialized, which currently doesn’t happen.

Regarding the rest:

  • I am using the original cable, and as far as I am concerned, it is properly connected to both the board and the host device. Now whether everything is ok with this cable itself, is something I currently cannot verify, as at the moment I don’t have a spare that would fit.

  • I am using all default settings, I did not change anything. I’m following the guides word for word, and settings were not yet touched on in the article I linked.

I recommend you read the ROS 2 documentation: ROS 2 - ZED Stereo Node - Stereolabs

You find the resolution parameter in each specific camera file; in your case, zedx.yaml:

Hello.
I’m very sorry I failed to explain myself properly, that’s not what I meant. What I did mean was that the linked instruction prompts you to try to interact with the connected camera from your host device - something I cannot do.

I though you wanted me to change the startup parameters of the camera so that I could check if it is working at all, after all, these parameters are being read from somewhere:

[2025-11-18 12:42:50 UTC][ZED][INFO] Logging level INFO
[2025-11-18 12:42:51 UTC][ZED][INFO] Using GMSL input... Switched to default resolution HD1200
[2025-11-18 12:42:52 UTC][ZED][INFO] [Init]  Camera FW version: 2001
[2025-11-18 12:42:52 UTC][ZED][INFO] [Init]  Video mode: HD1200@30
[2025-11-18 12:42:52 UTC][ZED][INFO] [Init]  Serial Number: S/N 41165475
[2025-11-18 12:42:52 UTC][ZED][INFO] [Init]  Depth mode: NEURAL LIGHT

For this misunderstanding I apologize.

Regarding what you added, I am familiar with running and tuning the ros2 wrapper, as I said, I made it all the way to it throwing the ‘CAMERA IS REBOOTING’ error. I tried running the wrapper again, trying different quality presets:

ros2 launch zed_wrapper zed_camera.launch.py camera_model:=zedx enable_ipc:=false
[INFO] [launch]: All log files can be found below /home/admin/.ros/log/2025-11-18-17-31-44-808281-thjytson-6173
[INFO] [launch]: Default logging verbosity is set to INFO
[INFO] [launch.user]: Using common configuration file: /workspaces/isaac_ros-dev/install/zed_wrapper/share/zed_wrapper/config/common_stereo.yaml
[INFO] [launch.user]: Using camera configuration file: /workspaces/isaac_ros-dev/install/zed_wrapper/share/zed_wrapper/config/zedx.yaml
[INFO] [launch.user]: Using Object Detection configuration file: /workspaces/isaac_ros-dev/install/zed_wrapper/share/zed_wrapper/config/object_detection.yaml
[INFO] [launch.user]: Using Custom Object Detection configuration file: /workspaces/isaac_ros-dev/install/zed_wrapper/share/zed_wrapper/config/custom_object_detection.yaml
[INFO] [launch.user]: Loading ZED node `zed_node` in container `/zed/zed_container`
[INFO] [robot_state_publisher-1]: process started with pid [6186]
[INFO] [component_container_isolated-2]: process started with pid [6188]
[robot_state_publisher-1] [INFO] [1763479906.013561606] [zed.zed_state_publisher]: got segment zed_camera_center
[robot_state_publisher-1] [INFO] [1763479906.013764879] [zed.zed_state_publisher]: got segment zed_camera_link
[robot_state_publisher-1] [INFO] [1763479906.013785040] [zed.zed_state_publisher]: got segment zed_left_camera_frame
[robot_state_publisher-1] [INFO] [1763479906.013796145] [zed.zed_state_publisher]: got segment zed_left_camera_optical_frame
[robot_state_publisher-1] [INFO] [1763479906.013804593] [zed.zed_state_publisher]: got segment zed_right_camera_frame
[robot_state_publisher-1] [INFO] [1763479906.013812305] [zed.zed_state_publisher]: got segment zed_right_camera_optical_frame
[component_container_isolated-2] [INFO] [1763479906.250390129] [zed.zed_container]: Load Library: /workspaces/isaac_ros-dev/install/zed_components/lib/libzed_camera_component.so
[component_container_isolated-2] [INFO] [1763479908.318868445] [zed.zed_container]: Found class: rclcpp_components::NodeFactoryTemplate<stereolabs::ZedCamera>
[component_container_isolated-2] [INFO] [1763479908.319433557] [zed.zed_container]: Instantiate class: rclcpp_components::NodeFactoryTemplate<stereolabs::ZedCamera>
[component_container_isolated-2] [INFO] [1763479908.689406641] [zed.zed_node]: ================================
[INFO] [launch_ros.actions.load_composable_nodes]: Loaded node '/zed/zed_node' in container '/zed/zed_container'
[component_container_isolated-2] [INFO] [1763479908.689541463] [zed.zed_node]:       ZED Camera Component 
[component_container_isolated-2] [INFO] [1763479908.689573272] [zed.zed_node]: ================================
[component_container_isolated-2] [INFO] [1763479908.689598905] [zed.zed_node]:  * namespace: /zed
[component_container_isolated-2] [INFO] [1763479908.689620506] [zed.zed_node]:  * node name: zed_node
[component_container_isolated-2] [INFO] [1763479908.689640603] [zed.zed_node]:  * IPC: disabled
[component_container_isolated-2] [INFO] [1763479908.689654876] [zed.zed_node]: ================================
[component_container_isolated-2] [INFO] [1763479908.740212302] [zed.zed_node]: === DEBUG parameters ===
[component_container_isolated-2] [INFO] [1763479908.740945518] [zed.zed_node]:  * SDK Verbose: 1
[component_container_isolated-2] [INFO] [1763479908.741249851] [zed.zed_node]:  * Use Pub Timestamps: FALSE
[component_container_isolated-2] [INFO] [1763479908.741410178] [zed.zed_node]:  * SDK Verbose File: 
[component_container_isolated-2] [INFO] [1763479908.741580330] [zed.zed_node]:  * Debug Common: FALSE
[component_container_isolated-2] [INFO] [1763479908.741702191] [zed.zed_node]:  * Debug Simulation: FALSE
[component_container_isolated-2] [INFO] [1763479908.741887063] [zed.zed_node]:  * Debug Video/Depth: FALSE
[component_container_isolated-2] [INFO] [1763479908.742153794] [zed.zed_node]:  * Debug Control settings: FALSE
[component_container_isolated-2] [INFO] [1763479908.742289224] [zed.zed_node]:  * Debug Point Cloud: FALSE
[component_container_isolated-2] [INFO] [1763479908.742399149] [zed.zed_node]:  * Debug GNSS: FALSE
[component_container_isolated-2] [INFO] [1763479908.742844736] [zed.zed_node]:  * Debug Positional Tracking: FALSE
[component_container_isolated-2] [INFO] [1763479908.743035593] [zed.zed_node]:  * Debug sensors: FALSE
[component_container_isolated-2] [INFO] [1763479908.743276275] [zed.zed_node]:  * Debug Mapping: FALSE
[component_container_isolated-2] [INFO] [1763479908.743599457] [zed.zed_node]:  * Debug Object Detection: FALSE
[component_container_isolated-2] [INFO] [1763479908.743779017] [zed.zed_node]:  * Debug Body Tracking: FALSE
[component_container_isolated-2] [INFO] [1763479908.743891438] [zed.zed_node]:  * Debug Streaming: FALSE
[component_container_isolated-2] [INFO] [1763479908.744457798] [zed.zed_node]:  * Debug ROI: FALSE
[component_container_isolated-2] [INFO] [1763479908.744762420] [zed.zed_node]:  * Debug Nitros: FALSE
[component_container_isolated-2] [INFO] [1763479908.744910778] [zed.zed_node]:  * Debug Advanced: FALSE
[component_container_isolated-2] [INFO] [1763479908.745262313] [zed.zed_node]: === TOPIC selection parameters ===
[component_container_isolated-2] [INFO] [1763479908.745687772] [zed.zed_node]:  * Publish Status: TRUE
[component_container_isolated-2] [INFO] [1763479908.745867364] [zed.zed_node]:  * Publish Left/Right images: FALSE
[component_container_isolated-2] [INFO] [1763479908.745989225] [zed.zed_node]:  * Publish Raw images: FALSE
[component_container_isolated-2] [INFO] [1763479908.746100974] [zed.zed_node]:  * Publish Gray images: FALSE
[component_container_isolated-2] [INFO] [1763479908.746245300] [zed.zed_node]:  * Publish RGB image: TRUE
[component_container_isolated-2] [INFO] [1763479908.746359609] [zed.zed_node]:  * Publish Stereo image: FALSE
[component_container_isolated-2] [INFO] [1763479908.746473438] [zed.zed_node]:  * Publish ROI Mask image: FALSE
[component_container_isolated-2] [INFO] [1763479908.746603908] [zed.zed_node]:  * Publish Depth Map: TRUE
[component_container_isolated-2] [INFO] [1763479908.746702792] [zed.zed_node]:  * Publish Depth Info: FALSE
[component_container_isolated-2] [INFO] [1763479908.746797772] [zed.zed_node]:  * Publish Point Cloud: TRUE
[component_container_isolated-2] [INFO] [1763479908.747182525] [zed.zed_node]:  * Publish Depth Confidence: FALSE
[component_container_isolated-2] [INFO] [1763479908.747392934] [zed.zed_node]:  * Publish Disparity: FALSE
[component_container_isolated-2] [INFO] [1763479908.747535564] [zed.zed_node]:  * Publish IMU: TRUE
[component_container_isolated-2] [INFO] [1763479908.747664018] [zed.zed_node]:  * Publish IMU Raw: FALSE
[component_container_isolated-2] [INFO] [1763479908.747812376] [zed.zed_node]:  * Publish LeftCam/IMU Transf.: FALSE
[component_container_isolated-2] [INFO] [1763479908.748070275] [zed.zed_node]:  * Publish Magnetometer: FALSE
[component_container_isolated-2] [INFO] [1763479908.748476149] [zed.zed_node]:  * Publish Barometer: FALSE
[component_container_isolated-2] [INFO] [1763479908.748812804] [zed.zed_node]:  * Publish Temperature: FALSE
[component_container_isolated-2] [INFO] [1763479908.749102224] [zed.zed_node]:  * Publish Odometry/Pose: TRUE
[component_container_isolated-2] [INFO] [1763479908.749249910] [zed.zed_node]:  * Publish Pose with Covariance: FALSE
[component_container_isolated-2] [INFO] [1763479908.749394621] [zed.zed_node]:  * Publish Camera Path: FALSE
[component_container_isolated-2] [INFO] [1763479908.749614438] [zed.zed_node]:  * Publish Detection Plane: FALSE
[component_container_isolated-2] [INFO] [1763479908.749829104] [zed.zed_node]: === SVO INPUT parameters ===
[component_container_isolated-2] [INFO] [1763479908.750250178] [zed.zed_node]: === LOCAL STREAMING parameters ===
[component_container_isolated-2] [INFO] [1763479908.750522766] [zed.zed_node]: === GENERAL parameters ===
[component_container_isolated-2] [INFO] [1763479908.750952192] [zed.zed_node]:  * Camera model: zedx - ZED X
[component_container_isolated-2] [INFO] [1763479908.751185963] [zed.zed_node]:  * Camera name: zed
[component_container_isolated-2] [INFO] [1763479908.751340113] [zed.zed_node]:  * Camera SN: 0
[component_container_isolated-2] [INFO] [1763479908.751482391] [zed.zed_node]:  * Camera ID: -1
[component_container_isolated-2] [INFO] [1763479908.751590044] [zed.zed_node]:  * Camera timeout [sec]: 5
[component_container_isolated-2] [INFO] [1763479908.751698337] [zed.zed_node]:  * Camera reconnection temptatives: 5
[component_container_isolated-2] [INFO] [1763479908.752046224] [zed.zed_node]:  * Camera framerate: 30
[component_container_isolated-2] [INFO] [1763479908.752416544] [zed.zed_node]:  * GPU ID: -1
[component_container_isolated-2] [INFO] [1763479908.752595176] [zed.zed_node]:  * Asynchronous image retrieval: FALSE
[component_container_isolated-2] [INFO] [1763479908.752739662] [zed.zed_node]:  * Image Validity Check: 1
[component_container_isolated-2] [INFO] [1763479908.753006426] [zed.zed_node]:  * Camera resolution: SVGA
[component_container_isolated-2] [INFO] [1763479908.753261029] [zed.zed_node]:  * Publishing resolution: CUSTOM
[component_container_isolated-2] [INFO] [1763479908.753686935] [zed.zed_node]:  * Publishing downscale factor: 2
[component_container_isolated-2] [INFO] [1763479908.753850270] [zed.zed_node]:  * OpenCV custom calibration: 
[component_container_isolated-2] [INFO] [1763479908.753995588] [zed.zed_node]:  * Camera self calibration: TRUE
[component_container_isolated-2] [INFO] [1763479908.754121674] [zed.zed_node]:  * Camera flip: FALSE
[component_container_isolated-2] [INFO] [1763479908.754329683] [zed.zed_node]:  * Publish framerate [Hz]:  15
[component_container_isolated-2] [INFO] [1763479908.754641985] [zed.zed_node]: === VIDEO parameters ===
[component_container_isolated-2] [INFO] [1763479908.754858410] [zed.zed_node]:  * Saturation: 4 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.754995056] [zed.zed_node]:  * Sharpness: 4 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.755127574] [zed.zed_node]:  * Gamma: 8 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.755269372] [zed.zed_node]:  * Auto Exposure/Gain: TRUE [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.755553320] [zed.zed_node]:  * Exposure: 80 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.755715535] [zed.zed_node]:  * Gain: 80 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.756017948] [zed.zed_node]:  * Auto White Balance: TRUE [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.756346027] [zed.zed_node]:  * White Balance Temperature: 42 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.756486385] [zed.zed_node]:  * ZED X Exposure time: 16000 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.756605974] [zed.zed_node]:  * ZED X Auto Exp. time range min: 28 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.756723739] [zed.zed_node]:  * ZED X Auto Exp. time range max: 30000 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.756832224] [zed.zed_node]:  * ZED X Exposure comp.: 50 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.756943716] [zed.zed_node]:  * ZED X Analog Gain: 1255 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.757080170] [zed.zed_node]:  * ZED X Auto Analog Gain range min: 1000 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.757197871] [zed.zed_node]:  * ZED X Auto Analog Gain range max: 16000 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.757324501] [zed.zed_node]:  * ZED X Digital Gain: 1 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.757450746] [zed.zed_node]:  * ZED X Auto Digital Gain range min: 1 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.758026035] [zed.zed_node]:  * ZED X Auto Digital Gain range max: 256 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.758317664] [zed.zed_node]:  * ZED X Auto Digital Gain range max: 50 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.758429509] [zed.zed_node]: === DEPTH parameters ===
[component_container_isolated-2] [INFO] [1763479908.759033279] [zed.zed_node]:  * Depth mode: NEURAL LIGHT [4]
[component_container_isolated-2] [INFO] [1763479908.759380686] [zed.zed_node]:  * Min depth [m]: 1
[component_container_isolated-2] [INFO] [1763479908.759663131] [zed.zed_node]:  * Max depth [m]: 15
[component_container_isolated-2] [INFO] [1763479908.759816673] [zed.zed_node]:  * Depth Stabilization: 30
[component_container_isolated-2] [INFO] [1763479908.759867363] [zed.zed_node]:  * OpenNI mode (16bit depth): DISABLED with NITROS
[component_container_isolated-2] [INFO] [1763479908.760006313] [zed.zed_node]:  * Point cloud rate [Hz]: 10
[component_container_isolated-2] [INFO] [1763479908.760167152] [zed.zed_node]:  * Point cloud resolution: COMPACT
[component_container_isolated-2] [INFO] [1763479908.760341560] [zed.zed_node]:  * Depth Confidence: 95 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.760495583] [zed.zed_node]:  * Depth Texture Confidence: 100 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.760625636] [zed.zed_node]:  * Remove saturated areas: TRUE [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.760692711] [zed.zed_node]: === GNSS FUSION parameters ===
[component_container_isolated-2] [INFO] [1763479908.761209822] [zed.zed_node]:  * GNSS fusion enabled: FALSE
[component_container_isolated-2] [INFO] [1763479908.761445960] [zed.zed_node]: === POSITIONAL TRACKING parameters ===
[component_container_isolated-2] [INFO] [1763479908.761709843] [zed.zed_node]:  * Positional tracking enabled: TRUE
[component_container_isolated-2] [INFO] [1763479908.761955902] [zed.zed_node]:  * Positional tracking mode: GEN 2
[component_container_isolated-2] [INFO] [1763479908.762090180] [zed.zed_node]:  * Map frame id: map
[component_container_isolated-2] [INFO] [1763479908.762189896] [zed.zed_node]:  * Odometry frame id: odom
[component_container_isolated-2] [INFO] [1763479908.762314510] [zed.zed_node]:  * Broadcast Odometry TF: TRUE
[component_container_isolated-2] [INFO] [1763479908.762426930] [zed.zed_node]:  * Broadcast Pose TF: TRUE
[component_container_isolated-2] [INFO] [1763479908.762588537] [zed.zed_node]:  * Depth minimum range: 0
[component_container_isolated-2] [INFO] [1763479908.762720191] [zed.zed_node]:  * TF timestamp offset: 0 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.762886438] [zed.zed_node]:  * Path publishing rate: 2 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.763068846] [zed.zed_node]:  * Path history lenght: -1
[component_container_isolated-2] [INFO] [1763479908.763411069] [zed.zed_node]:  * Initial pose: [0,0,0,0,0,0,]
[component_container_isolated-2] [INFO] [1763479908.763625446] [zed.zed_node]:  * Area Memory: TRUE
[component_container_isolated-2] [INFO] [1763479908.763976150] [zed.zed_node]:  * Area Memory File: 
[component_container_isolated-2] [INFO] [1763479908.764231137] [zed.zed_node]:  * Save Area Memory on closing: FALSE
[component_container_isolated-2] [INFO] [1763479908.764371751] [zed.zed_node]:  * Camera is static: FALSE
[component_container_isolated-2] [INFO] [1763479908.764490572] [zed.zed_node]:  * Gravity as origin: TRUE
[component_container_isolated-2] [INFO] [1763479908.765679840] [zed.zed_node]:  * IMU Fusion: TRUE
[component_container_isolated-2] [INFO] [1763479908.765959436] [zed.zed_node]:  * Floor Alignment: FALSE
[component_container_isolated-2] [INFO] [1763479908.766161557] [zed.zed_node]:  * Reset Odometry with Loop Closure: TRUE
[component_container_isolated-2] [INFO] [1763479908.766414976] [zed.zed_node]:  * Publish 3D Landmarks: FALSE
[component_container_isolated-2] [INFO] [1763479908.766695916] [zed.zed_node]:  * Publish Landmark Skip Frame: 
[component_container_isolated-2] [INFO] [1763479908.766832050] [zed.zed_node]:  * 2D mode: FALSE
[component_container_isolated-2] [INFO] [1763479908.766946135] [zed.zed_node]:  * Reset pose with SVO loop: TRUE
[component_container_isolated-2] [INFO] [1763479908.767001209] [zed.zed_node]: === Region of Interest parameters ===
[component_container_isolated-2] [INFO] [1763479908.767115006] [zed.zed_node]:  * Automatic ROI generation: FALSE
[component_container_isolated-2] [INFO] [1763479908.767327239] [zed.zed_node]:  * Manual ROI polygon: []
[component_container_isolated-2] [INFO] [1763479908.767380586] [zed.zed_node]: === SENSORS STACK parameters ===
[component_container_isolated-2] [INFO] [1763479908.767496015] [zed.zed_node]:  * Broadcast IMU TF [not for ZED]: FALSE
[component_container_isolated-2] [INFO] [1763479908.767607635] [zed.zed_node]:  * Sensors Camera Sync: FALSE
[component_container_isolated-2] [INFO] [1763479908.767763578] [zed.zed_node]:  * Sensors publishing rate [Hz]: 100 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.767813788] [zed.zed_node]: === Spatial Mapping parameters ===
[component_container_isolated-2] [INFO] [1763479908.767974339] [zed.zed_node]:  * Spatial Mapping Enabled: FALSE
[component_container_isolated-2] [INFO] [1763479908.768153483] [zed.zed_node]:  * Spatial Mapping resolution [m]: 0.05
[component_container_isolated-2] [INFO] [1763479908.768334131] [zed.zed_node]:  * 3D Max Mapping range [m]: 5
[component_container_isolated-2] [INFO] [1763479908.768516603] [zed.zed_node]:  * Map publishing rate [Hz]: 1 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.768658497] [zed.zed_node]:  * Clicked point topic: /clicked_point
[component_container_isolated-2] [INFO] [1763479908.768940013] [zed.zed_node]:  * Plane Det. Max Dist. Thresh.: 0.15
[component_container_isolated-2] [INFO] [1763479908.769188184] [zed.zed_node]:  * Plane Det. Normals Sim. Thresh.: 15
[component_container_isolated-2] [INFO] [1763479908.769523687] [zed.zed_node]: === OBJECT DETECTION parameters ===
[component_container_isolated-2] [INFO] [1763479908.769759409] [zed.zed_node]:  * Object Det. enabled: FALSE
[component_container_isolated-2] [INFO] [1763479908.769924696] [zed.zed_node]:  * Object Det. allow reduced precision: FALSE
[component_container_isolated-2] [INFO] [1763479908.770115072] [zed.zed_node]:  * Object Det. maximum range [m]: 20
[component_container_isolated-2] [INFO] [1763479908.770298920] [zed.zed_node]:  * Object Det. prediction timeout [sec]: 2
[component_container_isolated-2] [INFO] [1763479908.770479920] [zed.zed_node]:  * Object Det. tracking: TRUE
[component_container_isolated-2] [INFO] [1763479908.770711194] [zed.zed_node]:  * Object Filtering mode: NMS3D
[component_container_isolated-2] [INFO] [1763479908.770928868] [zed.zed_node]:  * Object Det. model: MULTI CLASS BOX FAST
[component_container_isolated-2] [INFO] [1763479908.771360694] [zed.zed_node]:  * MultiClassBox people: TRUE [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.771495420] [zed.zed_node]:  * MultiClassBox vehicles: TRUE [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.771729478] [zed.zed_node]:  * MultiClassBox bags: TRUE [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.771863660] [zed.zed_node]:  * MultiClassBox animals: TRUE [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.772098102] [zed.zed_node]:  * MultiClassBox electronics: TRUE [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.772244445] [zed.zed_node]:  * MultiClassBox fruits and vegetables: TRUE [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.772481703] [zed.zed_node]:  * MultiClassBox sport-related objects: TRUE [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.772649102] [zed.zed_node]:  * MultiClassBox people confidence: 65 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.772844375] [zed.zed_node]:  * MultiClassBox vehicles confidence: 60 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.773015710] [zed.zed_node]:  * MultiClassBox bags confidence: 40 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.773136323] [zed.zed_node]:  * MultiClassBox animals confidence: 40 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.773278986] [zed.zed_node]:  * MultiClassBox electronics confidence: 45 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.774477982] [zed.zed_node]:  * MultiClassBox fruits and vegetables confidence: 50 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.774649189] [zed.zed_node]:  * MultiClassBox sport-related objects confidence: 30 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.774716840] [zed.zed_node]: === Body Track. parameters ===
[component_container_isolated-2] [INFO] [1763479908.774993012] [zed.zed_node]:  * Body Track. enabled: FALSE
[component_container_isolated-2] [INFO] [1763479908.775234142] [zed.zed_node]:  * Body Track. model: HUMAN BODY MEDIUM
[component_container_isolated-2] [INFO] [1763479908.775568909] [zed.zed_node]:  * Body Track. format: BODY 38
[component_container_isolated-2] [INFO] [1763479908.775705875] [zed.zed_node]:  * Body Track. allow reduced precision: FALSE
[component_container_isolated-2] [INFO] [1763479908.775978559] [zed.zed_node]:  * Body Track. maximum range [m]: 15
[component_container_isolated-2] [INFO] [1763479908.776240394] [zed.zed_node]:  * Body Track. KP selection: FULL
[component_container_isolated-2] [INFO] [1763479908.776491509] [zed.zed_node]:  * Body fitting: FALSE
[component_container_isolated-2] [INFO] [1763479908.776646460] [zed.zed_node]:  * Body joints tracking: TRUE
[component_container_isolated-2] [INFO] [1763479908.776886822] [zed.zed_node]:  * Body Track. prediction timeout [sec]: 0.5
[component_container_isolated-2] [INFO] [1763479908.777011692] [zed.zed_node]:  * Body Track. confidence thresh.: 50 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.777136369] [zed.zed_node]:  * Body Track. min. KP thresh.: 5 [DYNAMIC]
[component_container_isolated-2] [INFO] [1763479908.777191347] [zed.zed_node]: === STREAMING SERVER parameters ===
[component_container_isolated-2] [INFO] [1763479908.777434654] [zed.zed_node]:  * Streaming Server enabled: FALSE
[component_container_isolated-2] [INFO] [1763479908.777756396] [zed.zed_node]:  * Stream codec: H264
[component_container_isolated-2] [INFO] [1763479908.777907922] [zed.zed_node]:  * Stream port: 30000
[component_container_isolated-2] [INFO] [1763479908.778089754] [zed.zed_node]:  * Stream bitrate: 12500
[component_container_isolated-2] [INFO] [1763479908.778332773] [zed.zed_node]:  * Stream GOP size: -1
[component_container_isolated-2] [INFO] [1763479908.778831131] [zed.zed_node]:  * Stream Chunk size: 16084
[component_container_isolated-2] [INFO] [1763479908.779416788] [zed.zed_node]:  * Adaptive bitrate: FALSE
[component_container_isolated-2] [INFO] [1763479908.779624573] [zed.zed_node]:  * Target frame rate:0
[component_container_isolated-2] [INFO] [1763479908.779733026] [zed.zed_node]: === ADVANCED parameters ===
[component_container_isolated-2] [INFO] [1763479908.780183093] [zed.zed_node]:  * Thread sched. policy: SCHED_BATCH
[component_container_isolated-2] [INFO] [1763479908.781420619] [zed.zed_node]: === SERVICES ===
[component_container_isolated-2] [INFO] [1763479908.785935823] [zed.zed_node]:  * Advertised on service: '/zed/zed_node/reset_odometry'
[component_container_isolated-2] [INFO] [1763479908.787645721] [zed.zed_node]:  * Advertised on service: '/zed/zed_node/reset_pos_tracking'
[component_container_isolated-2] [INFO] [1763479908.791899922] [zed.zed_node]:  * Advertised on service: '/zed/zed_node/set_pose'
[component_container_isolated-2] [INFO] [1763479908.794029518] [zed.zed_node]:  * Advertised on service: '/zed/zed_node/save_area_memory'
[component_container_isolated-2] [INFO] [1763479908.795897855] [zed.zed_node]:  * Advertised on service: '/zed/zed_node/enable_obj_det'
[component_container_isolated-2] [INFO] [1763479908.797238810] [zed.zed_node]:  * Advertised on service: '/zed/zed_node/enable_body_trk'
[component_container_isolated-2] [INFO] [1763479908.799292755] [zed.zed_node]:  * Advertised on service: '/zed/zed_node/enable_mapping'
[component_container_isolated-2] [INFO] [1763479908.800881368] [zed.zed_node]:  * Advertised on service: '/zed/zed_node/enable_streaming'
[component_container_isolated-2] [INFO] [1763479908.802722792] [zed.zed_node]:  * Advertised on service: '/zed/zed_node/start_svo_rec'
[component_container_isolated-2] [INFO] [1763479908.803900027] [zed.zed_node]:  * Advertised on service: '/zed/zed_node/stop_svo_rec'
[component_container_isolated-2] [INFO] [1763479908.804894246] [zed.zed_node]:  * Advertised on service: '/zed/zed_node/set_roi'
[component_container_isolated-2] [INFO] [1763479908.806151324] [zed.zed_node]:  * Advertised on service: '/zed/zed_node/reset_roi'
[component_container_isolated-2] [INFO] [1763479908.806294979] [zed.zed_node]: === STARTING CAMERA ===
[component_container_isolated-2] [INFO] [1763479908.807319119] [zed.zed_node]: ZED SDK Version: 5.1.1 - Build 106899_5f817843
[component_container_isolated-2] [INFO] [1763479908.821651389] [zed.zed_node]: === CAMERA OPENING ===
[component_container_isolated-2] [2025-11-18 17:31:49 UTC][ZED][INFO] Logging level INFO
[component_container_isolated-2] [ZED-X][Warning] Failed to connect to zed_x_daemon.
[component_container_isolated-2] [2025-11-18 17:31:51 UTC][ZED][INFO] [Init]  Camera FW version: 2001
[component_container_isolated-2] [2025-11-18 17:31:51 UTC][ZED][INFO] [Init]  Video mode: SVGA@30
[component_container_isolated-2] [2025-11-18 17:31:51 UTC][ZED][INFO] [Init]  Serial Number: S/N 41165475
[component_container_isolated-2] [2025-11-18 17:31:51 UTC][ZED][INFO] [Init]  Depth mode: NEURAL LIGHT
[component_container_isolated-2] (Argus) Error Timeout:  (propagating from src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 137)
[component_container_isolated-2] (Argus) Error Timeout:  (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 92)
[component_container_isolated-2] (Argus) Error Timeout:  (propagating from src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 137)
[component_container_isolated-2] (Argus) Error Timeout:  (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 92)
[component_container_isolated-2] [2025-11-18 17:32:21 UTC][ZED][ERROR] [Init]  Corrupted frames detected. Check that your camera is connected properly.
[component_container_isolated-2] [2025-11-18 17:32:25 UTC][ZED][ERROR] FAILURE in sl::ERROR_CODE sl::Camera::open(sl::InitParameters)
[component_container_isolated-2] [WARN] [1763479945.396327428] [zed.zed_node]: Error opening camera: FAILURE
[component_container_isolated-2] [INFO] [1763479945.396459273] [zed.zed_node]: Please verify the camera connection
[component_container_isolated-2] [ERROR] [1763479945.396531852] [zed.zed_node]: Camera detection timeout

Sadly, didn’t seem to help much.
I seem to be doing something really wrong, I guess.
In the meantime, I will reassemble my entire setup and replace the ribbon cable.
Thank you for your help so far.

Please check again all the connections because it seem a connection stability issue.
Do not unplug/replug cables and camera when the device is on, always remove the power before.

Hello.
Getting back to you, I can now confirm that this is not a physical connection issue. I have checked all the connections and replaced the ribbon cable, but nothing changes - sometimes everything works fine, sometimes it doesn’t.

What else should I look into?
Thank you for your time.

I’m sorry, but this confirms a connection issue.
If the card were damaged, it would never work.

Have you tried replacing the ribbon cables with new, shorter ones?

Hello.
I finally had some time to return to this project, so I investigated.
Replacing the ribbon cable with shorter or longer ones had no noticeable effect.
Downgrading to older versions of SDK or JetPack also didn’t do much. I tried the fix offered by someone on this forum, which was to downgrade all the way to SDK 4.2.2, but on Jetson Orin Nano I ran into a lot of compatibility issues.
I also found seemingly nothing wrong with the capture card.
My team suspects the GMSL cable, because the stability of this setup seems to be affected by the cable positioning, folding, etc,
While the replacement card and the replacement cable are on the way, just in case, is there anything I should look into in the meantime?
Thank you.

This is a possible cause of the problem. Do you have electronic tools to check that the cable can correctly transmit data?

Checked in with the tech, I’m being told that we do not have the tools to check the data transfer quality for this particular case. Anything else I could do?

I recommend you replace the cable.
According to what you described, you damaged it in some way.
GMSL2 cables are not designed to be bent at very sharp angles. Is this the case?