Vivio
May 22, 2024, 8:59am
1
Hi there,
Finally I’ve bought an ZED X with capture card.
I want to pair it to SEEED reComputer J4012-Edge NVIDIA Jetson Orin™ NX 16GB module.
J4012 has a carrier board called J401.
Based on this documentation I’ve connected the capture card to the J401.
The docs regarding capture card and J401 are a little bit unclear if the capture card MUST be powered up with 12-19V or it gets power though the CSI port as stated in the specification of the Stereolabs capture card
Connects to and is powered by the CSI port of the Orin/Xavier Developer Kit.
Hi @Vivio
Welcome to the Stereolabs community.
The 12-19V power is required. The flat cables cannot provide the required current to power the capture card.
Vivio
May 22, 2024, 3:59pm
3
Thank you @Myzhar !
If I may, I want to put some follow up questions:
Is there a chance to powerup the capture card internally? I want to avoid using two power supplies.
What’s the power consumption of the Capture card? I’ve seen that the ZED box with Orin NX 16GB & capture card is shipped with 12V/5A power supply.
You could split the Jetson power cable, so you can use the same source.
1A is the recommended minimum current to be provided to the capture card.
Vivio
May 22, 2024, 4:23pm
5
I can split it, right!
Is there a more less visible solution like on the Zed Box?
The capture card has some headers. They cannot be used for power?
I guess that soldering on the pads of the barrel jack voids my warranty.
Is there a schematic of the caprure card?
Thank you for shooting the replies fast