ZED X and Zed Box mini questions

Hi, I have a couple of questions related to Zed X and Zed box mini

  1. Can I use a 16V power supply to power the Zed box mini, or does it have to be 12V?

  2. Why does the Zed X image look more grainy compared to Zed 2i in similar enviroments?

Thanks!

Hi @hey_you

As reported in the ZED Box Mini datasheet, you must use an input source in the range:
10.5V to 13.5V - 60W max

Please add pictures to compare the images and understand more. Please note that they do not have the same type of sensor.

Hi, thanks for the info, I will update the images as soon as I can.
I have a question, why does the zed box need a HDMI plug? I have a jetson orin NX dev kit and it can run ZED SDK with ZED 2i without any plug throught SSH and SSH -X works with ZED_Explorer and ros2 launch both.
Is this related to ZED BOX, ZED SDK or Nvidia?

Thanks!

Everything is explained here:

https://support.stereolabs.com/hc/en-us/articles/28103346502167-Why-can-t-I-use-the-ZED-X-camera-with-ssh-X-in-headless-mode

Even after turning off area memory, for some reason the memory is continuously growing slowly but steadily, any thoughts on that?

Thanks!

Please do not ever post off-topic questions.
This is an issue we discussed in another thread, and I’ve already said that it will be fixed in one of the next releases of the ZED SDK.