hi Zed community
Recently we got this issue while running the ROS ZED wrapper by enabling Object Detection. As we used that feature for one of the previously developed applications it became a priority for us. while testing it after some time we faced this issue. It worked for us with our previous version 3.7.6 which is not currently available.
we are using Nvidia Xavier AGX 64GB with jetpack version 4.6.1 ubuntu 20.04.
Please help us resolve this issue.
Error we got
Optimizing all AI models
Optimizing: MULTI CLASS DETECTION...
Optimized model not found, trying to download it...
Optimizing objects_performance_2.2 \ 0.3%[> ] 13min 17s est. left Stack trace (most recent call last):
#10 Object "ZED_Diagnostic", at 0x434687, in
#9 Object "/lib/aarch64-linux-gnu/libc.so.6", at 0x7fac110e0f, in __libc_start_main
#8 Object "ZED_Diagnostic", at 0x41e3a7, in
#7 Object "ZED_Diagnostic", at 0x435c87, in
#6 Object "ZED_Diagnostic", at 0x46942f, in
#5 Object "ZED_Diagnostic", at 0x468de7, in
#4 Object "/usr/local/zed/lib/libsl_ai.so", at 0x7fa11c4b97, in
#3 Object "/usr/local/zed/lib/libsl_ai.so", at 0x7fa11c73e3, in
#2 Object "/usr/local/zed/lib/libsl_ai.so", at 0x7fa11f6517, in
#1 Object "/usr/local/zed/lib/libsl_ai.so", at 0x7fa11f2d13, in
#0 Object "/usr/local/zed/lib/libsl_ai.so", at 0x7fa11eee7c, in
Segmentation fault (Address not mapped to object [0x8])
Segmentation fault (core dumped)
Regards
Venkata prasad