Zed driver problem: jetpack 6.2.2, driver 1.4.2

Version info:

Ubuntu: 22.04.5

L4T: 36.5

Jetpack: 6.2.2+b24

ZED SDK: 5.2.3

ZED driver: 1.4.2

Problem description:

Unable to start zed_x_daemon.service. Download from official release link: driver ; Install with dpkg; reboot after installation. In contrast, if extract the .deb file, and copy the files to corresponding directories, the ZED_Diagnostic will show that driver is not installed.

running sudo ZED_Diagnostic -c

The error info is in the attached json file;

Also try to activate zed_x_daemon: sudo systemctl enable zed_x_daemon driver_zed_loader IMU_Daemon

This is the result I got:

Failed to enable unit: Unit file zed_x_daemon.service does not exist.

I’d appreciate your reply.

Hi @gjd2003
please copy and paste here the content of the “dmesg.log” file generated by the command sudo ZED_Diagnostic --dmesg.

Please also provide all the details about the hardware that you are using.

ZED_Diagnostic_Results.json (35.7 KB)

Details of hardware:

Jetson AGX Orin 64GB

Zed X camera

Zedlink Duo GMSL2 capture card

All the cables are included in the box/devkit

                "[  691.661125] zedx 9-0028: zedx_probe: Serial Number : 47412493",
                "[  691.661173] zedx 9-0028: zedx_probe: success",

Your camera is correctly detected by the driver.

Have you tried to restart the daemon with the command sudo service zed_x_daemon restart?

What’s the output of the command sudo service zed_x_daemon status 20 seconds after you restarted it?

Can you open the camera with ZED_Studio and ZED_Explorer?

In case the problem persists, I recommend you uninstall and reinstall the ZED X Driver:

  • sudo dpkg -r stereolabs-zedlink-duo
  • sudo dpkg -i stereolabs-zedlink-duo_1.4.2-LI-MAX96712-L4T36.5.0_arm64.deb
  • sudo reboot