Hi,
I am facing some issues using the ZED Box Mini with ROS2 Jazzy. One of the problems is the support for installing Ubuntu 24.04 and running ROS2 Jazzy natively.
Previously, I tried to run ROS2 Jazzy through a Docker container using a devcontainer, but I encountered some library versioning issues when using the Docker image jazzy-desktop-r36.4.0-cu128-24.04.
I had problems installing all the dependencies of the ROS2 ZED Wrapper for Jazzy, as well as enabling multicast communication for ROS2 Jazzy.
Therefore, through this post, I would like to ask for a clean solution to use ROS2 Jazzy on the ZED Box Mini.
Hi @affonsoviccari-plx,
As the Ubuntu version is tied to the Jetpack version, you cannot easily upgrade to another without upgrading Jetpack.
As of today, Nvidia does not support Jetpack 7 (which comes with Ubuntu24) for the Orin module, so the easiest way of having support is to use the images for L4T36.4 as you’ve been doing here.
If you have specific log errors, we can take a look and see what may be the issue.
Hello,
I have a ZED Box Orin NX that is currently running factory installed Ubuntu 22.04.5 LTS, and I am interested in using Ubuntu 24.04 and ROS 2 Jazzy on it.
Does the above discussion imply the only way to do this is to use an Ubuntu 24.04 image?
If not, is there a documented flashing or upgrade process for moving the device from its current 22.04 setup to a 24.04-based system?
Thanks