Title: ZED 2i not detected on Ubuntu 22.04 with ZED SDK v5.0.7
Hardware:
Camera: Stereolabs ZED 2i
GPU: NVIDIA GeForce RTX 3060 Mobile (Max-Q)
USB: Direct connection to USB 3.0 port
Software / Drivers:
Steps Taken:
Installed ZED SDK v5.0.7 using .run installer.
Installed NVIDIA driver successfully; confirmed nvidia-smi works.
Verified Secure Boot is disabled in BIOS.
Checked USB detection:
lsusb | grep -i stereo
Bus 003 Device 005: ID 2b03:f881 STEREOLABS ZED-2i HID INTERFACE
Bus 003 Device 006: ID 2b03:f880 STEREOLABS ZED 2i
Checked kernel logs:
sudo dmesg | grep -i zed
Shows USB connection but no ZED kernel module loaded.
Verified permissions and added user to video and plugdev groups.
Problem:
ZED_Explorer and /usr/local/zed/tools/ZED_Diagnostic report “Camera not detected” .
lsmod | grep zed returns empty , indicating the kernel module is not loaded.
Tried reinstalling SDK, but camera still not accessible.
ZED_Diagnostic_Results.json (6.5 KB)
Myzhar
October 10, 2025, 9:38am
2
Hi @vansh_agg
Welcome to the Stereolabs community.
From the diagnostic:
"glx_info": "OpenGL vendor string: AMD\nOpenGL renderer string: RENOIR (renoir, LLVM 15.0.7, DRM 3.57, 6.8.0-85-generic)\nOpenGL core profile version string: 4.6 (Core Profile) Mesa 23.2.1-1ubuntu3.1~22.04.3
This means that the discrete GPU is not used.
Please apply the fix described in this support page: https://support.stereolabs.com/hc/en-us/articles/8422008229143-How-can-I-solve-ZED-SDK-OpenGL-issues-under-Ubuntu
ZED_Diagnostic_Results.json (6.4 KB)
i done with your suggestion this specific issue solve but something is still there which cause problem.
new diagnostic results, please check
thank you
Myzhar
October 10, 2025, 9:55am
4
Hi @vansh_agg
Please use cheese or guvcview to try to open the camera stream.
Is it visible? Can you change the resolution and grab rate?
hey , i found the issue there is a mismatch in the cuda version i have installed 12.4 and for zed sdk i have installed 12.8 .
you please give me the zed_sdk for cuda 12.4
Myzhar
October 10, 2025, 4:01pm
6
That should not be a problem. The major version is important, not the minor.
v_agg
October 13, 2025, 12:14pm
7
i am also having same kind of issue on my ubuntu machine then i try on my windows but still facing the issue please help .
Zed 2i is works in the Zed explorer but not works in diagnostic, depth viewer, and other application
also works in the windows camera and visible in the ports
why this happen?
can i share the diagnostic reports