Hi,
I setup a stereo rig, with the zed-issaac-sim plugin,
I have loaded the usd files for the fish eye cameras to the scene,
and connected it in thethe action script
following this tutorial:
im getting an error when pressing play,
AttributeError: ‘ValuesForInputs’ object has no attribute ‘transport_layer_mode’
Traceback (most recent call last):
File “…/zed-isaac-sim/exts/sl.sensor.camera/sl/sensor/camera/nodes/SlCameraOneStreamer.py”, line 62, in compute
hi,
So I tried to setup simliarly to the tutorial , but it doesnt seem to connect ,
in the action script, I set it to IPC ,
I then run ZED_Depth_viewer , and try to connect ,
the zed-isaac-sim ext seems to complain about an invalid path:
2026-05-12 13:36:20 [Error] [sl.sensor.camera.annotators] Camera prim path /Root/ZED_X/base_link/ZED_X/CameraRight/base_link/ZED_XONE_GS/Camera is not valid.
yet, the path im using in the action graph is:
/Root/ZED_X/base_link/ZED_X/CameraRight
it seems to add base_link/ZED_XONE_GS ?
perhaps it works better on Windows ? which OS is recomended ?
also, can you elaborate on how to use the ZED Calibration exporter in IsaacSim?
is it for the virtual stereo rig streams? im not sure how to enable it for my stereo rig setup, thanks
Can you make sure you chose the correct camera model ? It seems to have a missmatch here (ZED X vs ZED XONE GS).
The Calibration exporter extension can be used to generate virtual stereo cameras from 2 ZED X Ones. To be more precise it helps you generate the calibration file necessary to use this rig with the ZED SDK.
You can find a guide on how to use this extension here : GitHub - stereolabs/zed-isaac-sim: NVIDIA Isaac Sim integration for ZED SDK · GitHub.
hi, when trying to stream via ipc on the same machine,
ZED_Explorer prints the following:
[Streaming] Warning : receiving port 40000 is not available (already used)… switching to port 40002. Retrying…
[Streaming] Backward compatibility required.
pls advise how to enable reading frames from ZED_Explorer
im trying to stream ZED x one GS mono camera first , if that works, I will try 2 ZED x one GS , and a virtual stereo.
do you support fisheye camera simulation ?
how close is zed x one camera simulation to the real camera ?
can you share examples of simulating zed x one fisheye ? a recorded svo file ?
There are 3 nodes,
playback->Isaac Run One simulation frame->Zed Camera one helper → setting : IPC , SN , port and camera ,
I put the serial number of the real zed x one camera we use.
im getting similar errors on ZED_Studio:
[ZED][Streaming] Switching to SHM-boost backend input
[Streaming] Warning : receiving port 40000 is not available (already used)… switching to port 40002. Retrying…
[Streaming] Warning : receiving port 40002 is not available (already used)… switching to port 40004. Retrying…
[Streaming] Backward compatibility required.
[2026-05-20 19:51:52 UTC][ZED][WARNING] Simulated ZED One camera used. ZED XOne GS
The fisheye option is not available for now. You can only simulate the ZED X One GS and ZED X One 4k cameras.
For mono cameras, you do not need to specify a serial number, it’s only necessary for the virtual stereo camera (after you calibrated it).
Changing this might create a mismatch, I’m not sure.
For monocular cameras, you don’t need to specify a serial number, a dedicated serial number (for simulation purposes) will be assigned to the camera automatically.
To connect to isaac sim, you need to open a stream in ZED Explorer or ZED Studio (or another sample) and set the IP of the machine that runs Isaac sim. For IPC, you must use 127.0.0.1 or localhost.
The port must match in both Isaac sim and your receiving app (and be an even number).
Hi,
The ext should not depend on the ZED SDK so I don’t think that is what’s causing the crash of Isaac sim.
Does isaac sim crashes at startup ? Can you share the logs?
I do not think it comes from that, but you can still delete those file, they will re generate in case it helps.
Did you change anything else other than the ZED SDK Version ? Installing a new sdk version should not have any impact on the Isaac sim extension, that’s why I’m a bit surprised there.
no, I updated the sdk and checked isaac-sim , checking if downgrading the sdk helps,
also, should I consider installing isaac-sim from source for better debugging ?
As a workaround, you can copy the “libsl_zed.so” from the ZED SDK installation (in /usr/local/zed/lib/) into the extension folder, in bin/. It should fix it (at least temporarily).