Unable to Visualize Object Detection in RViz2: Empty and Uneditable Topic in ZedOdDisplay

Hello, I am new to the world of computer vision and am experimenting with your ‘Robotics Perception Kit - Dual’. I’m ‘playing’ with the detection provided by the ros2_ZED_wrapper.
When I launch the ROS node of the ZED X camera with the command:
ros2 launch zed_wrapper zed_camera.launch.py camera_model:=zedx serial_number:=XXXXXXXX node_name:=zed_camera_2 namespace:=ZEDX
No errors or warnings occur, and I can subscribe to the object detection topic:
ros2 topic echo /zed/zed_camera_2/obj_det/objects | tee -a ~/Documents/output.txt
However, the problem arises when I try to visualize object detection in the RViz2 app. I have previously installed the plugin as explained here:

But when I launch RViz2:
ros2 launch zed_display_rviz2 display_zed_cam.launch.py camera_model:=zedx
Everything displayed in the console seems correct except for this error message related to ‘AerialMap’:

[rviz2-1] [ERROR] [1727096225.964193503] [rviz2]: PluginlibFactory: The plugin for class ‘rviz_satellite/AerialMap’ failed to load. Error: According to the loaded plugin descriptions the class rviz_satellite/AerialMap with base class type rviz_common::Display does not exist. Declared types are grid_map_rviz_plugin/GridMap rviz_default_plugins/AccelStamped rviz_default_plugins/Axes rviz_default_plugins/Camera rviz_default_plugins/DepthCloud rviz_default_plugins/Effort rviz_default_plugins/FluidPressure rviz_default_plugins/Grid rviz_default_plugins/GridCells rviz_default_plugins/Illuminance rviz_default_plugins/Image rviz_default_plugins/InteractiveMarkers rviz_default_plugins/LaserScan rviz_default_plugins/Map rviz_default_plugins/Marker rviz_default_plugins/MarkerArray rviz_default_plugins/Odometry rviz_default_plugins/Path rviz_default_plugins/PointCloud rviz_default_plugins/PointCloud2 rviz_default_plugins/PointStamped rviz_default_plugins/Polygon rviz_default_plugins/Pose rviz_default_plugins/PoseArray rviz_default_plugins/PoseWithCovariance rviz_default_plugins/Range rviz_default_plugins/RelativeHumidity rviz_default_plugins/RobotModel rviz_default_plugins/TF rviz_default_plugins/Temperature rviz_default_plugins/TwistStamped rviz_default_plugins/Wrench rviz_plugin_zed_od/ZedOdDisplay
*


*
’
However, when I add the ‘ZedOdDisplay’, it gives an error because the topic is empty, and I cannot manually enter the topic address.


How can I solve this?
Thank you

Hi @franmartin
welcome to the Stereolabs community.

Did you follow the Object Detection online documentation to learn how to enable the module?

You can find it here.

Hello Myzhar! Thank you for your help. Yes, I have followed the tutorial and I believe I did it correctly. In fact, the detection works properly. I can verify it by subscribing to the object detection topic, viewing it in the console, and saving it to a file, as I explained earlier. I have tried changing the different detections by configuring the common.yaml file. The problem is that I want to visualize it in RViz2, and it’s not possible. I have followed the steps to install the ZedOdDisplay plugin, but I have the error that I described to you earlier. Thanks and best regards.

image

You miss the OD topic here: /zed/zed_node/obj_det/objects

image

As I mentioned in the first post, I know the topic field is empty, but the problem is that it won’t let me edit it. I can edit the topic of all the displays: the topic for RGB_Image, the topic for RobotModel, etc., but just not that one. I’ll try cleaning everything and recompiling again. Thanks

What’s the output of the command ros2 topic hz /zed/zed_node/obj_det/objects?