When I was installing zed sdk, cuda 12.1 was required. But I am using ubuntu 20.04 and NVIDIA RTX 4090, and the lowest cuda version seems to be cuda 12.2.
I tried to remove default cuda and let the zed sdk automatically install cuda. However, when I did this, I could not log in ubuntu gui. So I have to remove cuda and reinstalled default cuda and nvidia driver so that I could use my PC again.
So the question here is how to install zed sdk on ubuntu 20 with NVIDIA rtx 4090.
Yeah, I successfully installed sdk with cuda12.2. But I have another issue same as this Object Detection sample code Error Message
I followed the solution, doing ‘sudo prime-select nvidia’, but I could no longer login to my PC. I am concerned that ZED and its apis can’t well support RTX4090.
[quote=“weizhu, post:6, topic:7335”]
the monitor should be connected to the NVIDIA HDMI ports instead of other HDMI ports.[/quote]
I apologize to not have asked to check this. I thought it was obvious.