Hello everyone,
I am trying to use the ZED m model with ROS on Jetson Nano but I get an error regarding the ZED connection.
, I’ve run the SDK installation file (ZED_SDK_Tegra_L4T32.7_v3.8.2.zstd.run) until completion and then I built the catkin workspace, then I sourced the workspace and launched the zed.m file.
I’ve found a similar issue but deleting the build and devel folders did not help me.
Steps to Reproduce
- I’ve run the SDK installation file (ZED_SDK_Tegra_L4T32.7_v3.8.2.zstd.run) until completion
- Cloned the repository on my workspace
- catkin_make
- roslaunch zed_wrapper zedm.launch
Expected Result
I expected the node to start up smoothly and publish the desired topics.
Actual Result
The node started but the output I get is the following:
[ INFO] [1669890207.084863231]: *** Opening ZED-M...
[ INFO] [1669890207.268928840]: ZED connection -> NVIDIA DRIVER OUT OF DATE
CUDA error at Camera.cpp:121 code=35(cudaErrorInsufficientDriver) "void sl::Camera::close()"
CUDA error at Camera.cpp:149 code=35(cudaErrorInsufficientDriver) "void sl::Camera::close()"
CUDA error at Camera.cpp:174 code=35(cudaErrorInsufficientDriver) "void sl::Camera::close()"
CUDA error at Camera.cpp:214 code=35(cudaErrorInsufficientDriver) "void sl::Camera::close()"
CUDA error at Camera.cpp:219 code=35(cudaErrorInsufficientDriver) "void sl::Camera::close()"
CUDA error at CameraUtils.hpp:773 code=35(cudaErrorInsufficientDriver) "void sl::ObjectsDetectorHandler::clear()"
CUDA error at CameraUtils.hpp:789 code=35(cudaErrorInsufficientDriver) "void sl::ObjectsDetectorHandler::clear()"
CUDA error at CameraUtils.hpp:795 code=35(cudaErrorInsufficientDriver) "void sl::ObjectsDetectorHandler::clear()"
CUDA error at CameraUtils.hpp:798 code=35(cudaErrorInsufficientDriver) "void sl::ObjectsDetectorHandler::clear()"
CUDA error at CameraUtils.hpp:800 code=35(cudaErrorInsufficientDriver) "void sl::ObjectsDetectorHandler::clear()"
CUDA error at CameraUtils.hpp:809 code=35(cudaErrorInsufficientDriver) "void sl::ObjectsDetectorHandler::clear()"
CUDA error at Camera.cpp:234 code=35(cudaErrorInsufficientDriver) "void sl::Camera::close()"
[ INFO] [1669890209.269835503]: ZED connection -> NVIDIA DRIVER OUT OF DATE
ZED Camera model
ZED Mini
Environment
OS: 4.9.140-tegra CPU: ARMv8 Processor rev 1 (v8l) × 4
GPU: NVIDIA Tegra X1 (nvgpu)/integrated (Nvidia Jetson Nano)
ZED SDK version: 3.8.2
CUDA version: CUDA 10.2
Any ideas?