I’m trying working with ZED 2i cameras for body tracking and object detection. I want to use them with Python. But when I start the python program for ZED, it stops showing the message “MOTION SENSORS REQUIRED”. Did someone encounter the same problem? And if yes, did you resolve it?
I am following tutorials provided by Stereolabs, first ones go perfectly, so the camera is recognized. But when I try the Body Tracking tutorial, terminal, after recognizing the ZED camera, stops with the message “MOTION SENSORS REQUIRED”. The fact is this problem occurs only in some devices; in another device, the python code works. So it’s not an HW problem.