Running into performance issues when running ZED X Mini on the Jetson Orin. Using SDK version 4.0.1, what are configurations that I could set (perhaps in the common.yaml) that could lower CPU usage and GPU usage. For example, how can we turn off all depth computation that ZED X Mini may be running on the Orin?
Hi @karmenlu
can you please provide more information (number and benchmarking methods) regarding this?
Hi @Myzhar,
Thanks for getting back to us!
Our perception stack uses images published by the ZED X Mini to find targets. The performance of the ZED has been measured against the same perception stack running with a different camera. The key indicator that ZED-related performance issues are present include that the ZED/Orin/perception setup crashes/disconnected while the other camera/Orin/perception setup connects properly and runs without disconnecting. Crashing / freezing led us to look into ZED performance. We have been measuring with jtop, the Jetson Stats tool. By default, ZED X Mini has been running with the Depth Quality setting of Ultra. (Ideally, we would want to set Depth Quality to 0/None. Running into issues discussed here). In the logs before, key columns to compare include the temperature, power, and GPU. We believe that minimizing power and compute usage by the ZED would prevent the overheat/crashing of our ZED testbench setup.
ZED X Mini Running w/ Depth Quality Ultra:
| time | uptime | CPU1 | CPU2 | CPU3 | CPU4 | CPU5 | CPU6 | CPU7 | CPU8 | CPU9 | CPU10 | CPU11 | CPU12 | RAM | SWAP | EMC | GPU | APE | DLA0_CORE | DLA0_FALCON | DLA1_CORE | DLA1_FALCON | NVDEC | NVENC | NVJPG | NVJPG1 | PVA0_CPU_AXI | PVA0_VPS | SE | VIC | Fan pwmfan0 | Temp CPU | Temp CV0 | Temp CV1 | Temp CV2 | Temp GPU | Temp SOC0 | Temp SOC1 | Temp SOC2 | Temp Tboard | Temp Tdiode | Temp tj | Power tj | Power TOT | jetson_clocks | nvp model | ||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| 2023-08-02 19:24:38 | 0:06:09 | 26 | 25 | 24 | 24 | 25 | 24 | 26 | 24 | 23 | 24 | 24 | 23 | 0.2774543256 | 0 | 0 | 98.9 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 61.17647059 | 76.187 | -256 | -256 | -256 | 72.375 | 71.468 | 71.187 | 70.968 | 61 | 64.5 | 76.187 | 9359 | 41406 | OFF | MAXN | ||
| 2023-08-02 19:24:38 | 0:06:09 | 26 | 25 | 24 | 24 | 25 | 24 | 26 | 24 | 23 | 24 | 24 | 23 | 0.2774543256 | 0 | 0 | 98.9 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 61.17647059 | 76.187 | -256 | -256 | -256 | 72.375 | 71.468 | 71.187 | 70.968 | 61 | 64.5 | 76.187 | 9359 | 41406 | OFF | MAXN | ||
| 2023-08-02 19:24:39 | 0:06:10 | 27 | 29 | 24 | 39 | 23 | 36 | 37 | 68 | 50 | 32 | 36 | 37 | 0.2782506435 | 0 | 0 | 98.7 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 61.17647059 | 75.937 | -256 | -256 | -256 | 72.906 | 71.531 | 71.187 | 70.937 | 61 | 64.75 | 75.937 | 9359 | 41082 | OFF | MAXN | ||
| 2023-08-02 19:24:40 | 0:06:11 | 39 | 29 | 27 | 26 | 21 | 34 | 25 | 72 | 27 | 30 | 39 | 29 | 0.2782028005 | 0 | 0 | 95.3 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 61.17647059 | 75.718 | -256 | -256 | -256 | 72.562 | 71.5 | 71.156 | 70.937 | 61 | 64.5 | 75.718 | 9359 | 41103 | OFF | MAXN | ||
| 2023-08-02 19:24:41 | 0:06:12 | 33 | 32 | 30 | 28 | 38 | 31 | 30 | 37 | 73 | 20 | 34 | 24 | 0.2781731225 | 0 | 0 | 99.1 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 61.17647059 | 76.218 | -256 | -256 | -256 | 72.781 | 71.5 | 71.125 | 71.125 | 61 | 64.5 | 75.812 | 9359 | 41324 | OFF | MAXN | ||
| 2023-08-02 19:24:42 | 0:06:13 | 34 | 29 | 32 | 28 | 29 | 17 | 22 | 31 | 77 | 35 | 26 | 33 | 0.2782475734 | 0 | 0 | 96.3 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 61.17647059 | 76.218 | -256 | -256 | -256 | 72.531 | 71.531 | 71.187 | 71.062 | 61 | 64.5 | 76.218 | 9258 | 40804 | OFF | MAXN | ||
| 2023-08-02 19:24:43 | 0:06:14 | 34 | 29 | 32 | 30 | 35 | 31 | 37 | 35 | 41 | 20 | 71 | 32 | 0.278165703 | 0 | 0 | 83.4 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 61.17647059 | 75.968 | -256 | -256 | -256 | 72.656 | 71.406 | 71.156 | 70.968 | 62 | 64.25 | 75.968 | 9158 | 40195 | OFF | MAXN | ||
| 2023-08-02 19:24:44 | 0:06:15 | 33 | 29 | 30 | 31 | 31 | 31 | 32 | 34 | 29 | 16 | 48 | 59 | 0.278215209 | 0 | 0 | 99.1 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 61.17647059 | 75.687 | -256 | -256 | -256 | 72.906 | 71.406 | 71.406 | 71.156 | 62 | 64.5 | 76 | 9258 | 40565 | OFF | MAXN | ||
| 2023-08-02 19:24:45 | 0:06:16 | 34 | 31 | 29 | 29 | 30 | 33 | 46 | 30 | 27 | 84 | 18 | 24 | 0.2783069295 | 0 | 0 | 98.8 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 61.17647059 | 75.906 | -256 | -256 | -256 | 72.593 | 71.562 | 71.343 | 71.093 | 62 | 64.5 | 75.906 | 9258 | 41022 | OFF | MAXN |
Other Camera:
| time | uptime | CPU1 | CPU2 | CPU3 | CPU4 | CPU5 | CPU6 | CPU7 | CPU8 | CPU9 | CPU10 | CPU11 | CPU12 | RAM | SWAP | EMC | GPU | APE | DLA0_CORE | DLA0_FALCON | DLA1_CORE | DLA1_FALCON | NVDEC | NVENC | NVJPG | NVJPG1 | PVA0_CPU_AXI | PVA0_VPS | SE | VIC | Fan pwmfan0 | Temp CPU | Temp CV0 | Temp CV1 | Temp CV2 | Temp GPU | Temp SOC0 | Temp SOC1 | Temp SOC2 | Temp Tboard | Temp Tdiode | Temp tj | Power tj | Power TOT | jetson_clocks | nvp model | ||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| 2023-08-02 21:24:50 | 0:12:49 | 16 | 14 | 13 | 14 | 13 | 13 | 13 | 14 | 13 | 14 | 13 | 14 | 0.3111295092 | 0 | 0 | 42.7 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | OFF | 30.19607843 | 56.156 | -256 | -256 | -256 | 52.187 | 51.968 | 51.031 | 52.218 | 42 | 45.25 | 56.156 | 8291 | 34789 | OFF | MAXN | ||
| 2023-08-02 21:24:50 | 0:12:49 | 16 | 14 | 13 | 14 | 13 | 13 | 13 | 14 | 13 | 14 | 13 | 14 | 0.3111295092 | 0 | 0 | 42.7 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | OFF | 30.19607843 | 56.156 | -256 | -256 | -256 | 52.187 | 51.968 | 51.031 | 52.218 | 42 | 45.25 | 56.156 | 8291 | 34789 | OFF | MAXN | ||
| 2023-08-02 21:24:51 | 0:12:50 | 41 | 52 | 45 | 53 | 28 | 51 | 36 | 71 | 33 | 40 | 40 | 32 | 0.3107495791 | 0 | 0 | 99 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | OFF | 30.19607843 | 55.968 | -256 | -256 | -256 | 54.468 | 52.156 | 50.968 | 52.75 | 42 | 45 | 55.968 | 8696 | 37348 | OFF | MAXN | ||
| 2023-08-02 21:24:52 | 0:12:51 | 29 | 33 | 29 | 47 | 25 | 98 | 18 | 22 | 45 | 27 | 42 | 57 | 0.311450467 | 0 | 0 | 53.3 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | OFF | 30.19607843 | 56.031 | -256 | -256 | -256 | 52.531 | 52.031 | 51.093 | 52.281 | 42 | 45.25 | 56.031 | 8291 | 35278 | OFF | MAXN | ||
| 2023-08-02 21:24:53 | 0:12:52 | 35 | 46 | 43 | 31 | 32 | 73 | 59 | 33 | 44 | 20 | 61 | 41 | 0.3117581209 | 0 | 0 | 99.4 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | OFF | 30.19607843 | 56.031 | -256 | -256 | -256 | 55.125 | 52.25 | 51.062 | 52.531 | 42 | 45 | 56.031 | 8595 | 36853 | OFF | MAXN | ||
| 2023-08-02 21:24:54 | 0:12:53 | 31 | 37 | 44 | 37 | 32 | 32 | 56 | 76 | 48 | 26 | 21 | 52 | 0.3123647298 | 0 | 0 | 60.9 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | OFF | 30.19607843 | 56.656 | -256 | -256 | -256 | 52.656 | 52.031 | 51.062 | 52.531 | 42 | 45 | 56.656 | 8291 | 35579 | OFF | MAXN | ||
| 2023-08-02 21:24:55 | 0:12:54 | 56 | 60 | 40 | 37 | 48 | 63 | 39 | 96 | 34 | 32 | 37 | 37 | 0.3138743444 | 0 | 0 | 99.4 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | OFF | 30.19607843 | 57.718 | -256 | -256 | -256 | 54.031 | 52.562 | 51.187 | 52.75 | 42 | 45.25 | 57.625 | 8595 | 38140 | OFF | MAXN | ||
| 2023-08-02 21:24:56 | 0:12:55 | 50 | 51 | 56 | 43 | 97 | 44 | 28 | 39 | 39 | 43 | 38 | 38 | 0.3127868744 | 0 | 0 | 73.4 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | OFF | 30.19607843 | 56.437 | -256 | -256 | -256 | 53.218 | 52.5 | 51.281 | 52.625 | 42 | 45 | 56.437 | 8392 | 35774 | OFF | MAXN | ||
| 2023-08-02 21:24:57 | 0:12:56 | 77 | 34 | 38 | 45 | 33 | 44 | 26 | 31 | 39 | 37 | 41 | 87 | 0.3128693845 | 0 | 0 | 99.2 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | OFF | 30.19607843 | 56.25 | -256 | -256 | -256 | 54.343 | 52.843 | 51.5 | 53.062 | 42 | 45.75 | 56.25 | 8696 | 37844 | OFF | MAXN |
Hi, what is your other camera ? Does it run depth computing ?
Also, could you publish the code you run so I can check what can be using your CPU ?
Other camera: Realsense. Runs depth computation too.
Our code runs deep learning algorithms on top of ZED data. Stepping aside from our code, the ZED X Mini is an edge device and shouldn’t be consuming too much of the Orin’s compute anyway.
Below are jtop logs with ZED running on the Orin without our code at different depth qualities. The difference between GPU usage on 0 and GPU usage on 3 looks great! Any configuration suggestions for lowering CPU, Temperature, and Power that would be compatible with either/both depth quality settings?
0/None:
| time | uptime | CPU1 | CPU2 | CPU3 | CPU4 | CPU5 | CPU6 | CPU7 | CPU8 | CPU9 | CPU10 | CPU11 | CPU12 | RAM | SWAP | EMC | GPU | APE | DLA0_CORE | DLA0_FALCON | DLA1_CORE | DLA1_FALCON | NVDEC | NVENC | NVJPG | NVJPG1 | PVA0_CPU_AXI | PVA0_VPS | SE | VIC | Fan pwmfan0 | Temp CPU | Temp CV0 | Temp CV1 | Temp CV2 | Temp GPU | Temp SOC0 | Temp SOC1 | Temp SOC2 | Temp Tboard | Temp Tdiode | Temp tj | Power tj | Power TOT | jetson_clocks | nvp model |
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| 2023-08-07 11:01:39 | 0:19:11 | 19 | 16 | 17 | 14 | 16 | 16 | 16 | 16 | 18 | 16 | 16 | 17 | 0.1063119817 | 0 | 0 | 13.6 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 53.562 | -256 | -256 | -256 | 48.031 | 49.375 | 49.781 | 48.531 | 41 | 42 | 53.25 | 5846 | 13548 | OFF | MAXN |
| 2023-08-07 11:01:39 | 0:19:11 | 19 | 16 | 17 | 14 | 16 | 16 | 16 | 16 | 18 | 16 | 16 | 17 | 0.1063119817 | 0 | 0 | 13.6 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 53.562 | -256 | -256 | -256 | 48.031 | 49.375 | 49.781 | 48.531 | 41 | 42 | 53.25 | 5846 | 13548 | OFF | MAXN |
| 2023-08-07 11:01:40 | 0:19:12 | 30 | 23 | 21 | 25 | 32 | 14 | 15 | 14 | 30 | 28 | 30 | 27 | 0.1067281139 | 0 | 0 | 0 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 52.843 | -256 | -256 | -256 | 48.031 | 49.375 | 49.781 | 48.5 | 41 | 42 | 52.843 | 5846 | 13319 | OFF | MAXN |
| 2023-08-07 11:01:41 | 0:19:13 | 29 | 20 | 19 | 19 | 18 | 18 | 13 | 17 | 26 | 25 | 25 | 25 | 0.10676099 | 0 | 0 | 0 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 52.531 | -256 | -256 | -256 | 48.125 | 49.406 | 49.812 | 48.468 | 41 | 42 | 52.531 | 5745 | 12755 | OFF | MAXN |
| 2023-08-07 11:01:42 | 0:19:14 | 25 | 25 | 24 | 24 | 23 | 23 | 23 | 25 | 21 | 23 | 20 | 24 | 0.1067448717 | 0 | 0 | 0 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 52.625 | -256 | -256 | -256 | 48.062 | 49.593 | 50 | 48.5 | 41 | 42 | 52.718 | 5745 | 12754 | OFF | MAXN |
| 2023-08-07 11:01:43 | 0:19:15 | 34 | 20 | 20 | 26 | 23 | 22 | 25 | 24 | 29 | 26 | 23 | 23 | 0.1067584315 | 0 | 0 | 0 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 52.656 | -256 | -256 | -256 | 47.906 | 49.343 | 50.093 | 48.468 | 41 | 42 | 52.656 | 5745 | 12989 | OFF | MAXN |
| 2023-08-07 11:01:44 | 0:19:16 | 29 | 21 | 20 | 16 | 29 | 25 | 26 | 26 | 25 | 21 | 24 | 23 | 0.1068635839 | 0 | 0 | 0 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 52.687 | -256 | -256 | -256 | 48.125 | 49.593 | 49.906 | 48.562 | 41 | 42 | 52.812 | 5745 | 13679 | OFF | MAXN |
| 2023-08-07 11:01:45 | 0:19:17 | 29 | 27 | 26 | 22 | 17 | 23 | 23 | 22 | 20 | 25 | 21 | 26 | 0.1068840515 | 0 | 0 | 0 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 52.687 | -256 | -256 | -256 | 48.031 | 49.406 | 49.906 | 48.531 | 41 | 42 | 52.687 | 5745 | 12757 | OFF | MAXN |
| 2023-08-07 11:01:46 | 0:19:18 | 28 | 26 | 24 | 23 | 23 | 19 | 24 | 23 | 20 | 23 | 28 | 22 | 0.1068493845 | 0 | 0 | 0 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 52.781 | -256 | -256 | -256 | 48.125 | 49.312 | 50.125 | 48.5 | 41 | 42 | 52.781 | 5745 | 12755 | OFF | MAXN |
| 2023-08-07 11:01:47 | 0:19:19 | 31 | 23 | 24 | 25 | 24 | 22 | 22 | 22 | 19 | 19 | 20 | 22 | 0.1068990184 | 0 | 0 | 0 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 52.625 | -256 | -256 | -256 | 47.968 | 49.343 | 50.031 | 48.468 | 41 | 42 | 53.031 | 5745 | 12755 | OFF | MAXN |
| 2023-08-07 11:01:48 | 0:19:20 | 31 | 27 | 19 | 20 | 21 | 24 | 23 | 26 | 21 | 20 | 21 | 23 | 0.1069284406 | 0 | 0 | 0 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 52.562 | -256 | -256 | -256 | 47.906 | 49.468 | 49.968 | 48.593 | 41 | 42 | 52.562 | 5745 | 12755 | OFF | MAXN |
| 2023-08-07 11:01:49 | 0:19:21 | 24 | 23 | 22 | 21 | 21 | 20 | 25 | 25 | 29 | 27 | 25 | 27 | 0.1068797021 | 0 | 0 | 0 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 52.656 | -256 | -256 | -256 | 47.968 | 49.656 | 50.062 | 48.5 | 41 | 42 | 52.656 | 5745 | 12754 | OFF | MAXN |
| 2023-08-07 11:01:50 | 0:19:22 | 27 | 22 | 19 | 25 | 21 | 19 | 20 | 19 | 24 | 22 | 25 | 27 | 0.1068857145 | 0 | 0 | 0 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 52.593 | -256 | -256 | -256 | 47.875 | 49.5 | 50.062 | 48.531 | 41 | 42.25 | 52.906 | 5745 | 12755 | OFF | MAXN |
3/Ultra:
| time | uptime | CPU1 | CPU2 | CPU3 | CPU4 | CPU5 | CPU6 | CPU7 | CPU8 | CPU9 | CPU10 | CPU11 | CPU12 | RAM | SWAP | EMC | GPU | APE | DLA0_CORE | DLA0_FALCON | DLA1_CORE | DLA1_FALCON | NVDEC | NVENC | NVJPG | NVJPG1 | PVA0_CPU_AXI | PVA0_VPS | SE | VIC | Fan pwmfan0 | Temp CPU | Temp CV0 | Temp CV1 | Temp CV2 | Temp GPU | Temp SOC0 | Temp SOC1 | Temp SOC2 | Temp Tboard | Temp Tdiode | Temp tj | Power tj | Power TOT | jetson_clocks | nvp model |
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| 2023-08-07 11:03:59 | 0:21:09 | 34 | 28 | 27 | 25 | 19 | 18 | 21 | 23 | 23 | 24 | 24 | 27 | 0.1289226821 | 0 | 0 | 43.2 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 54.312 | -256 | -256 | -256 | 49.218 | 50.343 | 50.718 | 49.406 | 42 | 43 | 53.875 | 5745 | 13913 | OFF | MAXN |
| 2023-08-07 11:03:59 | 0:21:09 | 34 | 28 | 27 | 25 | 19 | 18 | 21 | 23 | 23 | 24 | 24 | 27 | 0.1289226821 | 0 | 0 | 43.2 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 54.312 | -256 | -256 | -256 | 49.218 | 50.343 | 50.718 | 49.406 | 42 | 43 | 53.875 | 5745 | 13913 | OFF | MAXN |
| 2023-08-07 11:03:59 | 0:21:32 | 20 | 17 | 17 | 15 | 17 | 16 | 16 | 16 | 18 | 17 | 16 | 17 | 0.1319689025 | 0 | 0 | 43.9 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 54.406 | -256 | -256 | -256 | 49.093 | 50.312 | 50.625 | 49.468 | 42 | 43 | 54.125 | 6652 | 16458 | OFF | MAXN |
| 2023-08-07 11:04:00 | 0:21:33 | 37 | 32 | 27 | 22 | 21 | 25 | 25 | 19 | 31 | 25 | 28 | 29 | 0.132158228 | 0 | 0 | 21.3 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 53.843 | -256 | -256 | -256 | 49.093 | 50.468 | 50.843 | 49.468 | 42 | 43 | 54 | 6552 | 15346 | OFF | MAXN |
| 2023-08-07 11:04:01 | 0:21:34 | 33 | 26 | 25 | 24 | 29 | 24 | 31 | 27 | 27 | 26 | 28 | 24 | 0.1321716598 | 0 | 0 | 21.3 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 53.812 | -256 | -256 | -256 | 49.281 | 50.281 | 50.718 | 49.406 | 42 | 43 | 53.812 | 6552 | 15349 | OFF | MAXN |
| 2023-08-07 11:04:02 | 0:21:35 | 29 | 25 | 24 | 19 | 26 | 30 | 27 | 23 | 27 | 26 | 25 | 23 | 0.132125096 | 0 | 0 | 21.8 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 53.687 | -256 | -256 | -256 | 49.062 | 50.437 | 50.843 | 49.437 | 42 | 43 | 53.718 | 6552 | 15117 | OFF | MAXN |
| 2023-08-07 11:04:03 | 0:21:36 | 31 | 27 | 27 | 22 | 26 | 27 | 26 | 32 | 29 | 28 | 25 | 27 | 0.1322114437 | 0 | 0 | 32.9 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 53.781 | -256 | -256 | -256 | 49.125 | 50.531 | 50.968 | 49.343 | 42 | 43 | 53.937 | 6552 | 15116 | OFF | MAXN |
| 2023-08-07 11:04:04 | 0:21:37 | 31 | 23 | 24 | 20 | 27 | 29 | 26 | 34 | 22 | 26 | 24 | 28 | 0.1321344344 | 0 | 0 | 42.8 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 54 | -256 | -256 | -256 | 49.062 | 50.375 | 50.625 | 49.437 | 42 | 43 | 53.906 | 6451 | 15015 | OFF | MAXN |
| 2023-08-07 11:04:05 | 0:21:38 | 30 | 27 | 26 | 19 | 31 | 27 | 30 | 28 | 23 | 22 | 27 | 24 | 0.1322214217 | 0 | 0 | 21.3 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 53.781 | -256 | -256 | -256 | 49.218 | 50.343 | 50.75 | 49.375 | 42 | 43 | 54.187 | 6552 | 15349 | OFF | MAXN |
| 2023-08-07 11:04:06 | 0:21:39 | 30 | 24 | 23 | 28 | 29 | 28 | 34 | 29 | 27 | 28 | 26 | 26 | 0.132277196 | 0 | 0 | 21.3 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 53.843 | -256 | -256 | -256 | 49.25 | 50.5 | 50.968 | 49.437 | 42 | 43 | 54.125 | 6552 | 15447 | OFF | MAXN |
| 2023-08-07 11:04:07 | 0:21:40 | 27 | 21 | 22 | 19 | 29 | 30 | 30 | 30 | 28 | 25 | 26 | 28 | 0.132262229 | 0 | 0 | 29.9 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 53.843 | -256 | -256 | -256 | 49.25 | 50.5 | 50.812 | 49.593 | 42 | 43 | 53.843 | 6552 | 15349 | OFF | MAXN |
| 2023-08-07 11:04:08 | 0:21:41 | 24 | 23 | 16 | 17 | 29 | 31 | 29 | 28 | 32 | 27 | 33 | 30 | 0.1322617173 | 0 | 0 | 32.7 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 54.312 | -256 | -256 | -256 | 49.437 | 50.406 | 50.968 | 49.531 | 42 | 43 | 54.437 | 6552 | 15447 | OFF | MAXN |
| 2023-08-07 11:04:09 | 0:21:42 | 24 | 21 | 17 | 18 | 29 | 31 | 25 | 29 | 28 | 31 | 30 | 27 | 0.1322816732 | 0 | 0 | 24.1 | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | OFF | 473600 | 115200 | 27.45098039 | 54.187 | -256 | -256 | -256 | 49.343 | 50.531 | 50.781 | 49.406 | 42 | 43 | 54.031 | 6552 | 15217 | OFF | MAXN |
Hi,
Intel Realsense works quite differently than a purely passive camera. One of the advantage are indeed a lower compute, it’s normal that the ZED takes more compute since it does not run “simple” disparity algorithm but neural networks too.
However, ULTRA should be quite light for an AGX. In our benchmarks, an AGX can run 4 cameras at 15 FPS or 2 cameras at 15. We work on improving that, we want the AGX to run 4 cameras with more power available.
Can you share the code you use for your benchmark ? What module do you use apart Depth ?
Also, be aware that you can cap the FPS of the SDK so that it does not take up all the power available. Otherwise, it will try to reach the target framerate.
Hi,
Is it possible to turn the neural networks running on the ZED off? We are very interested in simplifying whatever is running on the ZED. The benchmark code is simply jtop exported to csv. We used jtop_logger.py here.
We have been using the common.yaml pulled from the Stereolabs GitHub. Only changing Depth Quality between 0, 1, and 3. Unable to get 0 to work without ASYNC/RGB warnings.
If you set the depth mode NONE, you should run at full speed. I’ve seen you get a few issues, that are related to ROS – I suggest you don’t use ROS for a benchmark, it’s more accurate to use directly the C++.
Okay, great. I can try running with a lower fps and the max speed. Is the lower speed that I have been running with the probable cause for the ASYNC/RGB warning?
I don’t know what errors you encountered. Can you share these warnings ?