Hi,
I am facing a Low bandwidth error when I try to launch a zed2i camera on my computer. I am using the original zed usb cable and is plugged into a USB3.1Gen2 (10G) port. The cable length is 5m. I tried opening the camera in the zed explorer and it opened without any LOW BANDWIDTH ERROR. The error only comes when using the ros2 launch.
I have been operating the camera at HD720@30fps and I still see the Consider trying a lower resolution and/or FPS. I wonder what the issue is
\[component_container_isolated-1\] \[2025-08-06 18:27:08 UTC\]\[ZED\]\[INFO\] Logging level INFO
\[component_container_isolated-1\] \[2025-08-06 18:27:09 UTC\]\[ZED\]\[INFO\] \[Init\] Depth mode: NEURAL
\[component_container_isolated-1\] \[2025-08-06 18:27:10 UTC\]\[ZED\]\[ERROR\] \[Init\] Unable to capture images. Consider trying a lower resolution and/or FPS
\[component_container_isolated-1\] \[2025-08-06 18:27:10 UTC\]\[ZED\]\[INFO\] \[Init\] Failed to open camera. Trying to re-open for 5 seconds.
\[component_container_isolated-1\] \[2025-08-06 18:27:10 UTC\]\[ZED\]\[INFO\] \[Init\] Random wait interval before consecutive openings: \[250\], \[1500\] msec.
\[component_container_isolated-1\] \[2025-08-06 18:27:10 UTC\]\[ZED\]\[INFO\] \[Init\] Waiting 917 msec before next opening attempt.
\[component_container_isolated-1\] \[2025-08-06 18:27:11 UTC\]\[ZED\]\[INFO\] \[Init\] Timeout in 3531msec
\[component_container_isolated-1\] \[2025-08-06 18:27:11 UTC\]\[ZED\]\[INFO\] \[Init\] Opening Camera. Attempt #2
\[component_container_isolated-1\] \[2025-08-06 18:27:11 UTC\]\[ZED\]\[ERROR\] \[Init\] Unable to capture images. Consider trying a lower resolution and/or FPS
\[component_container_isolated-1\] \[2025-08-06 18:27:13 UTC\]\[ZED\]\[INFO\] \[Init\] Waiting 797 msec before next opening attempt.
\[component_container_isolated-1\] \[2025-08-06 18:27:14 UTC\]\[ZED\]\[INFO\] \[Init\] Trying to force a device reboot to recover the video module.
\[component_container_isolated-1\] \[WARN\] \[1754504836.810659463\] \[zed_camera.camera1\]: Error opening camera: LOW USB BANDWIDTH
\[component_container_isolated-1\] \[INFO\] \[1754504836.810708243\] \[zed_camera.camera1\]: Please verify the camera connection
\[component_container_isolated-1\] \[2025-08-06 18:27:16 UTC\]\[ZED\]\[INFO\] \[Init\] Camera opening timeout reached.
\[component_container_isolated-1\] \[2025-08-06 18:27:16 UTC\]\[ZED\]\[WARNING\] LOW USB BANDWIDTH in sl::ERROR_CODE sl::Camera::open(sl::InitParameters)
\[component_container_isolated-1\] \[2025-08-06 18:27:22 UTC\]\[ZED\]\[INFO\] Logging level INFO
\[component_container_isolated-1\] \[2025-08-06 18:27:22 UTC\]\[ZED\]\[INFO\] \[Init\] Depth mode: NEURAL
\[component_container_isolated-1\] \[2025-08-06 18:27:23 UTC\]\[ZED\]\[ERROR\] \[Init\] Unable to capture images. Consider trying a lower resolution and/or FPS
\[component_container_isolated-1\] \[2025-08-06 18:27:23 UTC\]\[ZED\]\[INFO\] \[Init\] Failed to open camera. Trying to re-open for 5 seconds.
\[component_container_isolated-1\] \[2025-08-06 18:27:23 UTC\]\[ZED\]\[INFO\] \[Init\] Random wait interval before consecutive openings: \[250\], \[1500\] msec.
\[component_container_isolated-1\] \[2025-08-06 18:27:24 UTC\]\[ZED\]\[INFO\] \[Init\] Waiting 1267 msec before next opening attempt.
\[component_container_isolated-1\] \[2025-08-06 18:27:26 UTC\]\[ZED\]\[INFO\] \[Init\] Trying to force a device reboot to recover the video module.
\[component_container_isolated-1\] \[WARN\] \[1754504848.622145288\] \[zed_camera.camera1\]: Error opening camera: LOW USB BANDWIDTH
\[component_container_isolated-1\] \[2025-08-06 18:27:28 UTC\]\[ZED\]\[INFO\] \[Init\] Camera opening timeout reached.
\[component_container_isolated-1\] \[2025-08-06 18:27:28 UTC\]\[ZED\]\[WARNING\] LOW USB BANDWIDTH in sl::ERROR_CODE sl::Camera::open(sl::InitParameters)
\[component_container_isolated-1\] \[INFO\] \[1754504848.622209848\] \[zed_camera.camera1\]: Please verify the camera connection
\[component_container_isolated-1\] \[2025-08-06 18:27:34 UTC\]\[ZED\]\[INFO\] Logging level INFO
\[component_container_isolated-1\] \[2025-08-06 18:27:34 UTC\]\[ZED\]\[INFO\] \[Init\] Depth mode: NEURAL
\[component_container_isolated-1\] \[2025-08-06 18:27:35 UTC\]\[ZED\]\[ERROR\] \[Init\] Unable to capture images. Consider trying a lower resolution and/or FPS
\[component_container_isolated-1\] \[2025-08-06 18:27:35 UTC\]\[ZED\]\[INFO\] \[Init\] Failed to open camera. Trying to re-open for 5 seconds.
\[component_container_isolated-1\] \[2025-08-06 18:27:35 UTC\]\[ZED\]\[INFO\] \[Init\] Random wait interval before consecutive openings: \[250\], \[1500\] msec.
\[component_container_isolated-1\] \[2025-08-06 18:27:36 UTC\]\[ZED\]\[INFO\] \[Init\] Waiting 1118 msec before next opening attempt.
\[component_container_isolated-1\] \[2025-08-06 18:27:37 UTC\]\[ZED\]\[INFO\] \[Init\] Trying to force a device reboot to recover the video module.
\[component_container_isolated-1\] \[2025-08-06 18:27:40 UTC\]\[ZED\]\[INFO\] \[Init\] Camera opening timeout reached.
\[component_container_isolated-1\] \[2025-08-06 18:27:40 UTC\]\[ZED\]\[WARNING\] LOW USB BANDWIDTH in sl::ERROR_CODE sl::Camera::open(sl::InitParameters)
\[component_container_isolated-1\] \[WARN\] \[1754504860.287362328\] \[zed_camera.camera1\]: Error opening camera: LOW USB BANDWIDTH
\[component_container_isolated-1\] \[INFO\] \[1754504860.287432658\] \[zed_camera.camera1\]: Please verify the camera connection
\[component_container_isolated-1\] \[ERROR\] \[1754504860.287445168\] \[zed_camera.camera1\]: Camera detection timeout