Launching multiple cameras does not work

Getting the following error when launching multiple cameras:

[component_container_isolated-2] [2025-01-28 23:36:40 UTC][ZED][INFO] Logging level INFO
[component_container_isolated-2] [2025-01-28 23:36:40 UTC][ZED][ERROR] [ZED] sl::Camera::Open has not been called, no Camera instance running.
[component_container_isolated-2] [2025-01-28 23:36:40 UTC][ZED][ERROR] [ZED] sl::Camera::Open has not been called, no Camera instance running.
[component_container_isolated-2] [WARN] [1738107400.041873084] [camera_front.zed_node_0]: Error opening camera: CAMERA NOT DETECTED
[component_container_isolated-2] [INFO] [1738107400.041958971] [camera_front.zed_node_0]: Please verify the camera connection
[component_container_isolated-2] [2025-01-28 23:36:40 UTC][ZED][WARNING] CAMERA NOT DETECTED in sl::ERROR_CODE sl::Camera::open(sl::InitParameters)
[component_container_isolated-2] [2025-01-28 23:36:45 UTC][ZED][INFO] Logging level INFO
[component_container_isolated-2] [2025-01-28 23:36:45 UTC][ZED][ERROR] [ZED] sl::Camera::Open has not been called, no Camera instance running.
[component_container_isolated-2] [2025-01-28 23:36:45 UTC][ZED][ERROR] [ZED] sl::Camera::Open has not been called, no Camera instance running.
[component_container_isolated-2] [WARN] [1738107405.542829394] [camera_front.zed_node_0]: Error opening camera: CAMERA NOT DETECTED
[component_container_isolated-2] [INFO] [1738107405.542923921] [camera_front.zed_node_0]: Please verify the camera connection
[component_container_isolated-2] [2025-01-28 23:36:45 UTC][ZED][WARNING] CAMERA NOT DETECTED in sl::ERROR_CODE sl::Camera::open(sl::InitParameters)
[component_container_isolated-2] [2025-01-28 23:36:51 UTC][ZED][INFO] Logging level INFO
[component_container_isolated-2] [2025-01-28 23:36:51 UTC][ZED][ERROR] [ZED] sl::Camera::Open has not been called, no Camera instance running.
[component_container_isolated-2] [2025-01-28 23:36:51 UTC][ZED][ERROR] [ZED] sl::Camera::Open has not been called, no Camera instance running.
[component_container_isolated-2] [WARN] [1738107411.043618478] [camera_front.zed_node_0]: Error opening camera: CAMERA NOT DETECTED
[component_container_isolated-2] [INFO] [1738107411.043717741] [camera_front.zed_node_0]: Please verify the camera connection
[component_container_isolated-2] [2025-01-28 23:36:51 UTC][ZED][WARNING] CAMERA NOT DETECTED in sl::ERROR_CODE sl::Camera::open(sl::InitParameters)
[component_container_isolated-2] [2025-01-28 23:36:56 UTC][ZED][INFO] Logging level INFO
[component_container_isolated-2] [2025-01-28 23:36:56 UTC][ZED][ERROR] [ZED] sl::Camera::Open has not been called, no Camera instance running.
[component_container_isolated-2] [2025-01-28 23:36:56 UTC][ZED][ERROR] [ZED] sl::Camera::Open has not been called, no Camera instance running.
[component_container_isolated-2] [2025-01-28 23:36:56 UTC][ZED][WARNING] CAMERA NOT DETECTED in sl::ERROR_CODE sl::Camera::open(sl::InitParameters)
[component_container_isolated-2] [WARN] [1738107416.544449005] [camera_front.zed_node_0]: Error opening camera: CAMERA NOT DETECTED
[component_container_isolated-2] [INFO] [1738107416.544607211] [camera_front.zed_node_0]: Please verify the camera connection

Context:

  • Running the multi-camera launch from here: zed-ros2-examples/tutorials/zed_multi_camera at master · stereolabs/zed-ros2-examples · GitHub
  • Launching zed_wrapper separately for each camera works
  • Launching individual zed_wrapper for all cameras in multiple terminal sessions in parallel works also, though the second camera launch starts logging the following warning: [component_container_isolated-2] [ZED-X][Warning] Failed to connect to zed_x_daemon.
  • Restarting zed_daemon doesn’t change this
  • Setup uses 3 cameras (one ZED X + two monocular)
  • ZED SDK 4.2, Jetpack 6.0 / L4T 36.3.0, latest Quad link drivers
  • ROS2 Humble
  • ZED_Explorer also detects and runs all cameras
  • Already did the Middleware + Network tuning

EDIT 1:
It seems there must be some race condition → small edits to the launch file to add a 1s delay for each additional launch (using TimerAction) works. It’s not an actual fix, rather a workaround.

Hi @Myzhar , any suggestions on this, please?

Hi @dh662
can you post the command that you are using and the full log?

Ran the zed_multi_camera launch file from the zed-ros2-examples repo: zed-ros2-examples/tutorials/zed_multi_camera/launch/zed_multi_camera.launch.py at master · stereolabs/zed-ros2-examples · GitHub

You can comment out the Robot State Publisher for simplicity like this:
zed_multi_camera.launch.py (5.7 KB)

Running:

ros2 launch zed_multi_camera zed_multi_camera.launch.py cam_names:="[camera_front,camera_left,camera_right]" cam_models:="[zedx,zedxonegs,zedxonegs]" cam_serials:="[<sn1>, <sn2>, <sn3>]"

Output:
logs.txt (116.9 KB)

In this case camera_left failed to start with:

[component_container_isolated-4] [WARN] [1738363130.919734046] [camera_left.zed_node_1]: Error opening camera: CAMERA NOT DETECTED                                                                                                                        
[component_container_isolated-4] [INFO] [1738363130.919881079] [camera_left.zed_node_1]: Please verify the camera connection                                                                                                                              
[component_container_isolated-4] [2025-01-31 22:38:50 UTC][ZED][WARNING] CAMERA NOT DETECTED in sl::ERROR_CODE sl::CameraOneImpl::open(const sl::InitParametersOne&) 

ros2 node list only shows camera_front and camera_right.

Other times, it might be the front one or the right one that fails. Sometimes 2 out of 3 fail with this error. Again, running each camera individually works, all cameras show up in ZED_Explorer and restarting zed_x_daemon has no impact. All cameras work if you add incremental sleep before each subsequent launch to simulate sequential launch.

Hi @dh662
the multicamera example is not made to work with hybrid configurations.
It was designed to work only with multiple stereo cameras.

The README file does not mention anything about stereo camera only, in fact it states: “system equipped with multiple different models of ZED cameras”.

Point being, it would be nice if this was documented so you don’t send people down a rabbit hole. Also, mentioned our setup uses one ZED X + two monocular cameras in my initial post, unclear why you asked for command + logs :grinning:

It doesn’t strike me as an issue related to the mix of plugins between ZedCamera and ZedCameraOne. For what it’s worth, the same error occurs when trying to launch just the two monocular cameras.

Anyway, we found a work around when launching sequentially. Consider this user feedback.

That’s because the tutorial was created before the release of the ZED X One model.
We will update the README accordingly.

Normally customers using two monocular cameras create virtual stereo rigs.
I wrongly assumed you were doing the same.

What version of the ZED SDK are you using?

That’s because the tutorial was created before the release of the ZED X One model.
We will update the README accordingly.

Sounds good, thank you.

What version of the ZED SDK are you using?

ZED SDK 4.2.3 ZED_SDK_Tegra_L4T36.3_v4.2.3.zstd.run
Quad link 1.2.1 stereolabs-zedlink-quad_1.2.1-SL-MAX96712-all-L4T36.3.0_arm64.deb

I will try a similar setup to exclude eventual problems.

We identified a potential issue when opening GMSL2 cameras by using the serial number to select which camera to open.

The team is working on a fix

Hi @Myzhar
I am using 2 ZedX + 2ZedX mini cameras using the multi-robot launch.

System = Jetson Orin AGX 64gb dev kit (Duo capture card), Ubuntu 22
ZED Sdk 5.0 , 1.3.0 driver version

I am getting this same error (cameras use GMSL2) and maybe related to the error you just mentioned (here)

Is that issue fixed already in the configuration I am using?

Thank you !

Hi @KavitShah1998
Welcome to the StereoLabs community.

The problem is supposed to be fixed with the latest ZED SDK v5.0.2.
If that’s not the case, please report it.

Hi @Myzhar and @KavitShah1998,

I have a similar issue. We are using a jetson orin AGX and four ZEDX stereo cameras. Sometimes we get the issue described here (Connection issues ZED_Multi ROS2 node - #3 by robinvetsch).

But when starting the ZED_multi node we also have sometimes the issue, that the cameras are not been detected. We are using SDK 5.0.2 but the issue still presists…

Do you also have the issue when using 5.0.2?

Are you using the Serial Numbers or the Camera IDs to identify the cameras?
If you are using the Serial Numbers, please try to use the Camera IDs instead.

We’ve noted your reports and opened a bug for the ZED SDK team.

I also have the same issue. Launching the ros wrapper fails with 2 cameras on a camera not detected issue, but it works with only 1 camera.

How can I force it to use only the camera IDs and not the serial numbers? I think I have to supply both to the zed_components package. It looks like in zed_camera_component.cpp there is

if (mCamSerialNumber > 0) {
      mInitParams.input.setFromSerialNumber(mCamSerialNumber);
    } else if (mCamId >= 0) {
      mInitParams.input.setFromCameraID(mCamId);
    }

Is changing above to prioritize camid sufficient?

Dear support team,

I too have the same issue. My setup looks like the following:

  1. Jetson AGX Orin 64GB
  2. Zed Link Capture Card Quad
  3. Driver Version: stereolabs-zedlink-quad_1.3.0-SL-MAX96712-all-L4T36.4.0_arm64.deb
  4. SDK Version: ZED_SDK_Tegra_L4T36.4_v5.0.1.zstd.run
  5. Cameras: 1x ZED X & 3x ZED X Mini
  6. zed-ros2-wrapper

The zed link capture card quad was setup using the guide: ZED Link Quad on AGX Orin - Stereolabs and was powered externally with a 19V 4.4 A power supply.

Problem Description:

When I tried to launch all four cameras using their respective serial numbers, camera models, camera name, only two of them were successfully initialized (the first two cameras that I launched). The remaining two cameras failed to launch. However, when I open ZED Explorer, I am able to view the feed from each camera individually, confirming that all four devices are detected and functional.

Could you please assist in identifying the root cause or suggest any configuration or troubleshooting steps to enable the usage of all four cameras through ROS 2?

This is how I launch the cameras in my launch script (The values to the parameters were fetched from a yaml file before passing to the launch command) :

ros2 launch zed_wrapper zed_camera.launch.py \
camera_model:=$MODEL \
namespace:=$NS \
camera_name:=$NAME \
serial_number:=$SERIAL \
common_config_path:=$COMMON_CONFIG_FILE \
camera_config_path:=$CAM_CONFIG \
publish_tf:=false \
publish_map_tf:=false

Hoping to hear from you soon and thank you in advance for the support.

Hi @Shine
Welcome to the StereoLabs community.
Have you tried to install the latest ZED X Driver v1.3.1?

Hi @Myzhar ,

I have encountered the same issue described above regarding the multiple camera launch.

Therefore, I have tried to update the zed link driver to v1.3.1 (for zed link quad), with SDK v5.0.3 on Nvidia Jetson AGX Orin with Jetpack 6.2.1.

However, when I run ZED_Explorer --all on a terminal, I obtain the following logs:
(Argus) Error Timeout: (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function openSocketConnection(), line 220)
(Argus) Error Timeout: Cannot create camera provider (in src/rpc/socket/client/SocketClientDispatch.cpp, function createCameraProvider(), line 107)
No ZED detected

Note that I’m executing this with a screen connected to the display port of the jetson.

Here is the json file generated when executing ZED_Diagnostic tool.
ZED_Diagnostic_Results.json (24.7 KB)

Hi @Myzhar,

I have also tried to update the zed link driver to v1.3.1 (for zed link quad), with SDK v5.0.3 on Nvidia Jetson AGX Orin with Jetpack 6.0.

The result is that the “camera rebooting” and “connection issue detected” logs when launching multiple cameras still persist, so the problem seems to be unsolved.

Thank you.