Hi,
I was following this https://www.stereolabs.com/blog/getting-started-with-ros2-on-jetson-agx-orin/ to setup my AGX Orin with ROS2. I followed all the codes as described on the page until running the colcon build command
colcon build --symlink-install --cmake-args=-DCMAKE_BUILD_TYPE=Release
results this:
Starting >>> zed_interfaces
Finished <<< zed_interfaces [12.0s]
Starting >>> zed_components
[Processing: zed_components]
[Processing: zed_components]
[Processing: zed_components]
— stderr: zed_components
In file included from /home/nayan/ros2_ws/src/zed-ros2-wrapper/zed_components/src/zed_camera/include/zed_camera_component.hpp:19,
from /home/nayan/ros2_ws/src/zed-ros2-wrapper/zed_components/src/zed_camera/src/zed_camera_component.cpp:20:
/usr/local/zed/include/sl/Fusion.hpp:68:64: note: #pragma message: ~ FUSION SDK is distributed in Early Access ~
68 | #pragma message(“~ FUSION SDK is distributed in Early Access ~”)
| ^
Finished <<< zed_components [1min 41s]
Starting >>> zed_wrapper
— stderr: zed_wrapper
In file included from /home/nayan/ros2_ws/install/zed_components/include/zed_components/zed_camera_component.hpp:19,
from /home/nayan/ros2_ws/src/zed-ros2-wrapper/zed_wrapper/src/zed_wrapper.cpp:17:
/usr/local/zed/include/sl/Fusion.hpp:68:64: note: #pragma message: ~ FUSION SDK is distributed in Early Access ~
68 | #pragma message(“~ FUSION SDK is distributed in Early Access ~”)
| ^
Finished <<< zed_wrapper [12.9s]
Starting >>> zed_ros2
Finished <<< zed_ros2 [1.01s]
Summary: 4 packages finished [2min 7s]
2 packages had stderr output: zed_components zed_wrapper
I am using the latest jetpack and ZED SDK. Kindly let me know how to overcome the build error. Thank you.