I need to install autoware and zed at the same cuda so I can use with it

I need to use it on host computer at 20.04 with foxy installed but autoware requires humble verison and cuda versions from ./setup-dev-env.sh
ok: [localhost] => {
“msg”: [
{
“rosdistro”: “humble”
},
{
“rmw_implementation”: “rmw_cyclonedds_cpp”
},
{
“cuda_version”: “12.4”
},
{
“cudnn_version”: “8.9.7.29-1+cuda12.2”
},
{
“tensorrt_version”: “10.8.0.43-1+cuda12.8”
}
]
}
how can I use both on docker ? which cuda version won’t affect the perception module of the autoware
‘Source installation - Autoware Documentation’

Hi @Hensbag
Welcome to the stereolabs community.

What type of host is it? Desktop, laptop, Jetson?

host computer looks like have some kind of ADAS computer probably can be considered as desktop , here is the documentation:https://cdn.teknofest.org/media/upload/userFormUpload/2025_Robotaksi_Hazir_Arac_Mimari_Tanimlama_Dokumani_tkBlS.pdf

Hi btw , thank you :sweat_smile:

You can use the instructions from the Docker folder of the ZED ROS2 Wrapper repository to create a Docker container with ROS2 Humble on Ubuntu 20.04:

You must simply adapt the build command to your requirements:
./desktop_build_dockerfile_from_sdk_ubuntu_and_cuda_version.sh <Ubuntu version> <CUDA version> <ZED SDK version>

İf I build it on 22.04 will there be any issue ? Because I don’t have the vehicle all the time.

What do you refer to?

Referring to ubuntu version 22.04 docker build on humble , thanks a lot btw.

Humble runs natively on Ubuntu 22.04, so you can install the binaries with the APT command both in a Docker container or on the host.

Okay, Thanks a lot. much appreciated. :pray:. Where can I reach you for further questions about using zed2 camera on autoware ?

We are not officially supporting Autoware. I recommend you reach out to their support team because it’s possible that they have more information.