Help with Neural Network Optimization Issue

Hi, I’m having an issue with optimizing my neural network. It doesn’t proceed at all, whether I try from the diagnostic application or directly from the command line, even after cleaning the models. When trying to optimize from the command line after downloading the model, it starts optimizing at 0.1% as shown in the image, but then it stops. I’ve tried using the latest SDK 4.25 and 4.1 with CUDA 12 and 11.8, and I’ve fully uninstalled and restarted everything.
ZED_Diagnostic_Results.json (20.7 KB)


I have 5080 and Ultra 9 285K

Hi @MechatronicMan
with RTX GPU cards we recommend using CUDA 12.
Please uninstall CUDA 11.8, verify that you installed the latest version of the GPU driver, and then install CUDA 12.6.
Then uninstall the ZED SDK and reboot.
Finally, install the ZED SDK v4.2.5 and verify with ZED Depth Viewer that you can correctly optimize the NEURAL Depth model.

sorry but still the same


all done with full reboot after each step.

Hi @MechatronicMan
we are investigating a possible compatibility issue with the RTX GPU models of the series 5000.

Meanwhile, to exclude an eventual bad configuration, can you test if you can build and run one of the CUDA samples?

Hi, I have problems with visual studio (camke generate files correct) but not specialist in and have problems with other librarys also… But i have other test on the same machine with win10 zed sdk 4.25 and cuda 12.6 also the same error
ZED_Diagnostic_Results-win10 (8.5 KB)

maybe it will help, it’s look that zed appear in GPU mem from cuda point of view


success compile cuda example

Hi,
Thanks. We may have found the problem. Would you be interested in testing an installer which could fix the issue? Unfortunately, I can’t test it on real hardware. Here’s the link for Windows CUDA 12: https://stereolabs.sfo2.cdn.digitaloceanspaces.com/zedsdk/4.2/ZED_SDK_Windows_cuda12.1_v4.2.6.exe
Let us know if this solves it.

start testing will let You know :slight_smile:

So test on 12.1, 12.6, 12.8 with full cycle of restart and still error in diagnostic tool, in command line still error but get 0.5% of progress :stuck_out_tongue:

After investigating and for future readers, the ZED SDK 4.2 doesn’t support Blackwell GPUs. We’re working on supporting it in a new release (it will require TRT 10 and CUDA 12.8)

I have the same problem with a RTX 5080 and can’t get the neural depth mode working (ZED SDK 4.2, CUDA 12.6). Are there any updates on the SDK to resolve this problem? Thanks

Yes, the support of RTX 50X0 GPUs has been added to the upcoming ZED SDK 5.0. An early access will be released soon

@szollmann The new early access version can be downloaded at ZED SDK 5.0 - Download | Stereolabs

Fantastic, it now works on my side. I tested the neural mode and neural plus. Models are downloading fine and depth estimation works well.

So the depth viewer and neural mode works well, but I just tried to use the python API and I have some problems with numpy incompatiblities. Is there a specific version required (I tried the version that was recommended for the old SDK and I tried numpy2.24).
" import pyzed.sl
Traceback (most recent call last):
File “”, line 1, in
File “pyzed\sl.pyx”, line 1, in init pyzed.sl
ValueError: numpy.dtype size changed, may indicate binary incompatibility. Expected 96 from C header, got 88 from PyObject"
Thank you

Touch designer and Unity integration also fail in this point

@szollmann Awesome! For your Python issue, you should use numpy 2. This is unexpected. You can try compiling the wrapper from src, I pushed the update: zed-python-api/src at master · stereolabs/zed-python-api · GitHub

@MechatronicMan Unity integration will be released very soon. For TouchDesigner it’s maintained by the editor itself so it may take some time

is 4.x ever going to support 5000-series GPUs? We have a very big project with a very big client built in Unity with a HEAVILY edited 4.2 Unity SDK; “simply” migrating to 5.x is not going to be feasible if we ever need to replace a machine in the field and can’t find a 3000 or 4000 series card due to market conditions. The latest 4.2.5 in the archive still fails on model optimization

I understand.
That’s not currently planned as it requires significant code changes and backporting a good chunk from 5 and newer dependencies like CUDA 12.8 and TensorRT 10.

On the C++ API side, the move from 4 to 5 requires very minimal, if not no code changes. I’m not super familiar with the C/unity wrapper but it may be an acceptable compromise to port it.