Hi @TanguyHardelin
Thanks again for your guidance
As you suggested i have set my mode to NEURAL but while ingesting GNSS to zed i am getting INVALID TIMESTAMP issue apart from any Non performance depth mode iam getting INVALID TIMESTAMP but As u informed in the difference is expected to be less than 4 seconds i have verified difference betweeb GNSS Time and sl.getCurrentTimeStamp() it is less than a second still iam getting INVALID TIMESTAMP.
Observations:
- The GNSS timestamp and the
sl.getCurrentTimeStamp()are less than 1 second apart, which is well within the <4s threshold mentioned in the docs. - The issue disappears when switching to a performance depth mode (e.g.,
PERFORMANCE). - The error only occurs in NEURAL and other non-performance depth modes, which are necessary for our use case due to the scene’s complexity and speed.
CODE
LOGS
Additional Notes:
- As you suggested earlier, we are actively working on increasing the GNSS covariance to assist with fusion stability.
- The INVALID_TIMESTAMP issue appears tightly linked to NEURAL mode — possibly due to an internal delay or different sync behavior compared to PERFORMANCE mode.
Questions:
- Could NEURAL depth mode introduce a delay that causes GNSS timestamps to be misaligned internally?
- Is there a known workaround or recommended approach to ensure reliable GNSS fusion when using NEURAL mode?
In the meantime, if there’s any solution or workaround available for the INVALID_TIMESTAMP issue specifically, it would be extremely helpful to keep our pipeline moving forward.
Thanks in advance for your support!