Framerate issue when using the Fusion Network Workflow

Hello,

We are currently experiencing issues calibrating a multi-camera ZED 2i setup using the Fusion Network workflow.

We are experimenting with a two-camera configuration, each camera connected to a Jetson Orin Nano 8GB running ZED SDK 5.0.7.

We have built a simple sender client based on the sample code provided here: https://www.stereolabs.com/docs/fusion/overview

So far, this part works well: the client runs at a stable 30 FPS. We have also tested single-camera skeleton detection independently and found the results to be of adequate quality.

Each Jetson is connected via a private network to a third machine (Intel i9 + RTX 4090, running Windows and ZED SDK 5.0.7).

We then start ZED360 and configure it using the Jetsons’ IP addresses and the ZED camera serial numbers. However, to our surprise, the incoming streams fluctuate between 10 and 15 FPS.

We observe similar results when running ZED360 on a third Jetson.

We ran an additional test by writing custom code that receives both camera streams via the Fusion API. Once again, the observed FPS is significantly lower than expected and fluctuates between 15 and 25 FPS, making the setup unusable.

Based on these tests, we believe that the Fusion SDK is receiving the skeleton streams at a lower frame rate than the 30 FPS at which they are being sent.

We would appreciate your assistance in identifying the failure point and understanding why the streams are not being received at the expected frame rate, especially since we do not have access to the Fusion SDK internals.

Please let us know if you need additional details or access to the specific code we are using.

Thanks in advance,

Shadi

Hi @shadi
Welcome to the Stereolabs community.

Please verify that the system time of all the components of the rig is synchronized.

You could use PTP (or any other method) to guarantee it.

Thanks for getting back to me, @Myzhar.

All the components of the rig are indded synchronised by PTP. The slave is reporting an offset in the tens of thousands of nanoseconds, which I’m assmuming is sufficient.

[122.322] master offset -11530 s2 freq -22665 path delay 93340
[123.322] master offset -12272 s2 freq -22751 path delay 94017
[124.322] master offset -19051 s2 freq -23448 path delay 97486
[125.322] master offset -13736 s2 freq -22930 path delay 94313
[126.322] master offset -6967 s2 freq -22260 path delay 93917
[127.322] master offset -7275 s2 freq -22298 path delay 93917
[128.323] master offset 8293 s2 freq -20733 path delay 93917
[129.323] master offset -7109 s2 freq -22281 path delay 95601
[130.323] master offset -30849 s2 freq -24685 path delay 95601
[131.323] master offset -8630 s2 freq -22472 path delay 94618

Before proceeding further, I recommend you upgrade the ZED SDK on all the machines to the latest v5.1.2: https://www.stereolabs.com/developers/release

Hi @Myzhar . I have upgraded to 5.1.2, but but now ZED360 has stopped working and is returning an error: ERROR: WRONG BODY FORMAT. No sekeleton are showing in ZED360. I have tried all 3 formats on the sender end (18, 34, 38), same error. What format is ZED360 expecting?

Here’s my sender code:

// ZED includes
#include <sl/Camera.hpp>


// Using std and sl namespaces
using namespace std;
using namespace sl;

void print(string msg_prefix, ERROR_CODE err_code = ERROR_CODE::SUCCESS, string msg_suffix = "");
void parseArgs(int argc, char **argv, InitParameters& param);

int main(int argc, char **argv) {

    // Create ZED Bodies
    Camera zed;
    InitParameters init_parameters;
    init_parameters.camera_resolution = RESOLUTION::AUTO;
    init_parameters.depth_mode = DEPTH_MODE::NEURAL_LIGHT;
    init_parameters.coordinate_system = COORDINATE_SYSTEM::RIGHT_HANDED_Y_UP;

    // Open the camera
    auto returned_state = zed.open(init_parameters);
    if (returned_state != ERROR_CODE::SUCCESS) {
        zed.close();
        return EXIT_FAILURE;
    }

    // Enable Positional tracking (mandatory for object detection)
    PositionalTrackingParameters positional_tracking_parameters;
    //If the camera is static, uncomment the following line to have better performances
    positional_tracking_parameters.set_as_static = true;

    returned_state = zed.enablePositionalTracking(positional_tracking_parameters);
    if (returned_state != ERROR_CODE::SUCCESS) {
        zed.close();
        return EXIT_FAILURE;
    }

    // Enable the Body tracking module
    BodyTrackingParameters body_tracker_params;
    body_tracker_params.enable_tracking = false; // track people across images flow
    body_tracker_params.enable_body_fitting = false; // smooth skeletons moves
    body_tracker_params.body_format = sl::BODY_FORMAT::BODY_18;
    body_tracker_params.detection_model = BODY_TRACKING_MODEL::HUMAN_BODY_FAST;
    //body_tracker_params.allow_reduced_precision_inference = true;

    returned_state = zed.enableBodyTracking(body_tracker_params);
    if (returned_state != ERROR_CODE::SUCCESS) {
        zed.close();
        return EXIT_FAILURE;
    }

    // Configure object detection runtime parameters
    BodyTrackingRuntimeParameters body_tracker_parameters_rt;
    body_tracker_parameters_rt.detection_confidence_threshold = 40;
    body_tracker_parameters_rt.skeleton_smoothing = 0.7;
    
    CommunicationParameters configuration;
    configuration.setForLocalNetwork(30000);
    zed.startPublishing(configuration);

    // Create ZED Bodies filled in the main loop
    Bodies bodies;
    while (true) {
        // Grab images
        auto err = zed.grab();
        if (err == ERROR_CODE::SUCCESS) {
            // Retrieve Detected Human Bodies
            zed.retrieveBodies(bodies, body_tracker_parameters_rt);
        } 
    }

    // Release Bodies
    bodies.body_list.clear();

    // Disable modules
    zed.disableBodyTracking();
    zed.disablePositionalTracking();
    zed.close();

    return EXIT_SUCCESS;
}

Hi, this means the fusion module is receiving data from different formats coming from each camera.
Can you double-check each sender is using the same SDK version and the same body format as well?

Thanks for get back to me @BenjaminV.

I double checked and both senders and receiver are using the same SDK version (5.1.2) and the sender code I posted above (so sl::BODY_FORMAT::BODY_18).

Some additional context:

  • The error happens consistently and no skeletons appear. However once in a while (1 out 10, or 1 out of 20). There’s no error, the skeletons are displayed, and everything works impeccably. I was not able to isolate the factor that causes it to work, seems to be random.
  • This error started appearing when I upgraded from 5.0.7 to 5.1.2, it wasn’t present before. I upgraded because 5.0.7 had another issue (low framerate, which is now solved).
  • Both ZED Live Link and my custom receiver work consistly fine. It’s only ZED360 which is causing issues. Therefore, I have no way of debugging this, as the calibration functions are not exposed in the API afaik.

It’s quite frustrating because this look like the last hurdle before having a functional system, everything else seems to be working fine. Your help would be much appreciated. Please let me know if there’s any useful tests I can run or if you have any sender code that’s proven to work with this SDK version.

@BenjaminV, here’s a another experiment I ran to validate the senders are working individually:

I aksed ZED360 to load the same camera twice (using a config file). Both nodes work well when tested individually and there’s no error.

However if I try to load the two cameras at the same time (the normal setup) then it fails.

Hope that helps.

Hi,

You can find an example of the sender code here:

It looks very similar to what you’re using, so I don’t think the issue is coming from the sender side.

Are the Jetsons connected over Wi-Fi? If so, this could explain the inconsistent behavior. For this type of Fusion network workflow, we strongly recommend using a wired Ethernet connection to ensure stable bandwidth.

Thanks for getting back to me @BenjaminV.

My sender code is based on the example you shared, so it is indeed very similar.

The entire system is on Ethernet, not Wifi.

This error started appearing when I upgraded from 5.0.7 to 5.1.2, so it looks like something has changed between these two versions.

Hi @BenjaminV,

I’m Elsa, Senior Producer working with Shadi at FIELD.IO. This matter is now halting our production timeline, with a big Korean automotive client waiting and pause on further large-scale purchases from StereoLab.

Can we please escalate this into a phone-call or a meeting, either today or by Monday morning latest?

Elsa
+45 3033 5899 / elsa@field.io

Hi @Elsa
Welcome to the Stereolabs community.

We understand the urgency of your situation. Our team is actively investigating the possible causes of the issue described by your colleagues.

At the moment, we don’t yet have a definitive update to share, which is why your tickets haven’t been updated. Please be assured that the lack of visible replies does not mean the issue is being ignored.

Customer satisfaction remains a top priority for us, and we are doing our best to support you and all our customers as quickly and thoroughly as possible.

Hi Myzhar,

Thank you for your reply, it’s highly appreciated.

We will need to make a decision by Monday whether or not to move forward with StereoLab or another company for this project and therefore time is of the essence.

Could we please set up a meeting to resolve this together? I believe this would be the most efficient use of time for everyone involved. This way we can easier get to the bottom of the issue and have faster communication between our developers and yours.

Please let me know your availability for this as soon as possible.

Best regards,
Elsa

Hi again Myzhar,

We still haven’t received an update on the issue in your ZED360 calibration software.

As mentioned last week, we need to make a decision now on whether or not to go forward with StereoLabs on this project. Could you please share with us the resolve status of this issue? Are we correct in thinking this is a bug on your end, in which case, when can it be fixed?

I can push the decision-making of which system/company to go with until end of this week latest—but in that case, we need to have some reassurance that this can be resolved.

Please consider giving me a call to discuss this, especially given your top priority on customer satisfaction,

Elsa
+45 3033 5899 / elsa@field.io

@Elsa The Fusion network is broken since one year starting with 5.x. We have the same issue since then Fusion in 5.0.2 very slow - #9 by Tunkali

I really like the zed2i cameras. But the fusion network workflow isn’t reliable for customer projects and software support is catastrophic (i guess too many construction sites). We also had a big costumer project, which we could only rescue buying old 40xx graphics cards and using 4.x sdk. But this isn’t a workaround for future projects. So we are also looking for a different solution for future projects.

I’m sure the developers and support team is doing there best… but it don’t work out. But Stereolabs should focus on core features and not doing false promises…

Same issue over here. Stock Jetson ZEDbox running iirc 5.0.7. Two individual camera grabbers using the provided sample code completely saturate the box’s wattage in MAXN mode, but with tuned settings, we can get both reporting ballpark 30fps grab. Any Fusion receiver build we connect to that dual IP data stream does not run more than ballpark 15fps. We have been given the runaround about using PTP to sync the sender and receivers, but not only is this very nontrivial when the receiver is Windows, it is mooted by the fact that a Fusion receiver running on the same box gets identical 15fps performance to a Fusion receiver running remotely, without meaningfully impacting the sender grab rate.

Right now, we are experimenting with running the full Fusion stack on the Jetson, which gets us ~24fps, but we still have an independent issue of bodies changing IDs when they cross from camera to camera, and the additional issue that the Fusion project provided as a sample does not seem to expose its data port (20001) to external machines, and the whole network stack underlying Fusion looks to be API-obscured. About the best bodge we can make at present is to run not only the full camera-to-Fusion stack on the Jetson, but also an additional layer of bespoke middleware to consume the raw UDP 20001 unicast data and relay it on a more flexible TCP socket for external use.

(Completely independently, we are also in the position of needing to maintain long-term 4.x projects which are no longer compatible with available (read: RTX 5xxx) GPUs, but that deserves another thread entirely)

As an update, with the same hardware (ZEDBOX MINI), running the same full-stack 2x GMSL2 ZED X MINI Fusion end-to-end locally with NEURAL_LIGHT depth mode and HUMAN_BODY_FAST detection HD1080 30fps requested,

  • SDK 4.2.5 flat out cannot find the cameras, even with latest drivers, and a support email response indicates this is expected. (but a full Windows 4.x stack on a RTX 4080 does not have any issues with framerate or body ID)
  • SDK 5.0.7 clocks 24fps fused, dropping to 20-22 with a user in-scene, but can’t maintain body ID across cameras. When using individual grabbers sending over IP, this drops to 15fps fused whether the receiver is local or remote.
  • SDK 5.1.2 clocks 15fps fused, weirdly rising to 18fps with a user being tracked, but still can’t maintain body ID.

A support email response indicates `There are no slowing down verified issues with Fusion and Body Tracking. The SDK team was not able to replicate them.`

Please add more details useful to replicate your problems.
If the team cannot replicate a problem, it’s not possible to fix it.

A list of useful information:

  • Communication scheme
  • Code snippets
  • SVO recording
  • List of parameters used with the ZED SDK
  • Configuration (CPU, GPU, RAM, disc, network, etc) of all the involved systems
  • Anything else that you can consider useful to understand the setup

As already indicated, we are using a NVIDIA Jetson ZEDBOX MINI, I believe the 16GB Orin NX given tegrastats reports 15655MB RAM (I was not part of the purchase process, but our CTO spent significant time in discussion with StereoLabs over our use-case requirements) and 2 ZED X MINI cameras on GMSL2. We have tried the above-listed SDKs, and recently updated from 1.3.1 to 1.3.2 drivers with no change in performance. The problem manifests on the StereoLabs sample sender from Fusion - Stereolabs with the sample receiver zed-unity-livelink/zed-unity-livelink-fusion at main · stereolabs/zed-unity-livelink · GitHub . We have made negligible adjustments e.g. removing sleep waits, adding a simple ctime-based framecounter for comparative metrics and experimenting with different depth and tracking values in all codebases, but have standardized on HD1080@30 NEURAL_LIGHT HUMAN_BODY_ACCURATE BODY_38 as the most performant without sacrificing needed quality (e.g. BODY_18 on the sample sender does not materially improve grab framerate, but creates issues in a downstream pipeline built on the assurance of at least BODY_34 data).

When running from the standalone senders to an external receiver, we are seeing the same ballpark 15fps performance receiving to the fusion sample on Windows 11 Home 25H2, Intel Core Ultra 9 285K CPU (3.7GHz), 32GB RTX 5090 GPU, 64GB RAM with approximately 1 second of system-time skew from the Jetson (again, compatible Windows PTP solutions are prohibitive without a PTP-expert IT team on hand and/or investing in a corporate-tier paid/managed PTP management platform, and 1 second skew is the minimum we’ve been able to dial in by controlling both box’s choices of NTP server). We were not seeing the same framedrop and body ID loss when running in a pure-Windows ecosystem on SDK 4, but that configuration is increasingly inaccessible given hardware availability and camera compatibility.

We are moving on to experiments with a single-camera setup, but as of yesterday, the sample unity-livelink-mono project (with similar adjustments to format) could only manage 15-18fps grab on SDK 5.1.2. I plan on re-testing on 5.0.7 today, since 5.0.7 could at least manage 24fps running the full Fusion stack locally at the same settings.

—

Update: The unity-livelink-mono project running standalone at the above settings manages 15-18fps in both 5.1.2 and 5.0.7. However, the unity-livelink-fusion project running with a config file manually edited down to a single camera, and the same settings, runs 30fps and finally gives us a usable data stream for our end application. Which all leaves me somewhat mystified where exactly the framedrop is happening… adding more depth to the stack should not double performance.

Update 2: Still on 1 camera, reworking to a standalone sender on the Jetson (with or without body_tracker_params.enable_tracking = true;) and receiving to the fusion demo in the Windows machine, we are getting 30fps performance but seeing body ID change when the user crosses the lateral (canonically X) midpoint of the scene. This means that (a) framerate drop really is somewhere in the fusion stack, but more weirdly (b) ID instability may be something more fundamentally wrong than just moving from one camera to another. We’ll take another pass at making sure everything is on the same and ideally latest SDK build (some parts of our stack may be 3rdparty-capped as far back as 5.0.4), but that is unlikely to happen before Monday.

Hi @NNSkelly
All the details have been forwarded to the ZED SDK team.
They will analyze the problem and try to reproduce and fix it with one of the next releases.