Using sudo dmesg | grep zedx I can see that both of my two ZED X Ones have been recognised by the dual capture card, since I can see both of their serial numbers in that output. However when I open the ZEDXOne Media Server tool, it only ever detects and streams one camera. I can’t get to the point where I see both camera streams in that Media Server like in the setup guide here. sudo ZED_Diagnostic --dmesg log attached here. dmesg.log (23.6 KB)
Setup:
Seeed J4012 Orin NX 16GB
Jetpack 6.1 from Nvidia (not the modified build from Seeed)
Latest ZED SDK (4.2.2) and X driver (1.2.1)
ZED Link Duo capture card, short CSI cables (5cm), no long/extended GMSL2 cables.
How can I debug this to get both ZED X One cameras working at the same time so I can go ahead with calibration?
Noting here that I have found a workaround for now by using the ZED X driver that is meant for the ZED Box Orin NX 16 GB, since the ZED Link Duo did not work.
Current mostly-working setup which has let me complete stereo calibration is:
Seeed J4012 Orin NX 16GB
Jetpack 6.0 from Nvidia (not the modified build from Seeed)
Latest ZED SDK (4.2.2)
Latest X driver (1.2.1) using the version meant for ZED Box Orin NX 16 GB since the ZED Link Duo did not work
ZED Link Duo capture card, short CSI cables (5cm), no long/extended GMSL2 cables.
Now facing a new issue detailed here:
But still eager to know why the ZED X driver for ZED Link Duo did not work.
Hi @Blake-James
Unfortunately, we cannot provide support for Seeed Studio devices, as they are not officially supported by our drivers and we have never tested them with these devices.