Cannot initialize second camera

Possibly related to ZED X Camera Cannot initialize Error opening Camera: Camera Failed to setup

I have two ZED X camera attached to a ZED dual link card with an Nvidia Jetson Orin dev kit. When I try to open and stream both cameras using ZED_Explorer I can see the first one but not the second one.

Using JP5.1.2 and the following installers for the camera drivers and ZED SDK
stereolabs-zedlink-duo_1.2.1-LI-MAX96712-ALL-L4T35.4.1_arm64.deb
ZED_SDK_Tegra_L4T35.4_v4.2.2.zstd.run

Output of sudo ZED_Diagnostic --dmseg I can send separately (cannot upload if new user?

When running ZED_Explorer and switching to my second camera (first streams ok) I get the following error with ZED_Explorer crashing

(Argus) Error EndOfFile: Unexpected error in reading socket (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadCore(), line 277)
(Argus) Error EndOfFile: Receiving thread terminated with error (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadWrapper(), line 379)
(Argus) Error InvalidState: Receive thread is not running cannot send. (in src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 96)
(Argus) Error InvalidState:  (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 91)
Stack trace (most recent call last) in thread 7961:
#10   Object "[0xffffffffffffffff]", at 0xffffffffffffffff, in
#9    Object "/usr/lib/aarch64-linux-gnu/libc.so.6", at 0xffffab94462b, in
#8    Object "/usr/lib/aarch64-linux-gnu/libpthread.so.0", at 0xffffac8da623, in
#7    Object "/usr/lib/aarch64-linux-gnu/libQt5Core.so.5", at 0xffffabd3d50f, in
#6    Object "ZED_Explorer", at 0x454637, in
#5    Object "ZED_Explorer", at 0x575683, in
#4    Object "ZED_Explorer", at 0x5ac05b, in
#3    Object "ZED_Explorer", at 0x5ab64b, in
#2    Object "ZED_Explorer", at 0x59a8bb, in
#1    Object "ZED_Explorer", at 0x5a3b8f, in
#0    Object "/usr/lib/aarch64-linux-gnu/tegra/libnvargus_socketclient.so", at 0xffffadc08368, in
Segmentation fault (Address not mapped to object [(nil)])
Segmentation fault (core dumped)

(base) brianlerner@beachbot-1:~$ ZED_Explorer -a
## Cam  0  ##
 Model :  "ZED-X"
 S/N :  43740003
 State :  "Camera Available"
 Path :  /dev/i2c-30
 ID :  0
 Type :  "GMSL2"
********************
## Cam  1  ##
 Model :  "ZED-X"
 S/N :  45235829
 State :  "Camera Available"
 Path :  /dev/i2c-30
 ID :  1
 Type :  "GMSL2"
********************

I also tried opening with the ZED_SENSOR_Viewer and get the following error. No sensor readings are showing for the second camera.

(base) brianlerner@beachbot-1:~$ ZED_Sensor_Viewer
[2024-12-06 18:20:11 UTC][ZED][INFO] Logging level INFO
[2024-12-06 18:20:11 UTC][ZED][INFO] Logging level INFO
[2024-12-06 18:20:11 UTC][ZED][INFO] [Init]  Depth mode: NONE
[ZED-X][Warning] Failed to connect to zed_x_daemon.
[2024-12-06 18:20:14 UTC][ZED][INFO] [Init]  Camera FW version: 2001
[2024-12-06 18:20:14 UTC][ZED][INFO] [Init]  Video mode: HD1200@30
[2024-12-06 18:20:14 UTC][ZED][INFO] [Init]  Serial Number: S/N 43740003
[2024-12-06 18:20:16 UTC][ZED][WARNING] [Init]  Self-calibration failed. Point the camera towards a more textured and brighter area. Avoid objects closer than 1 meter (Error code: 0x01)
[2024-12-06 18:20:21 UTC][ZED][INFO] Logging level INFO
[2024-12-06 18:20:21 UTC][ZED][INFO] Logging level INFO
[2024-12-06 18:20:21 UTC][ZED][INFO] [Init]  Depth mode: NONE
(Argus) Error EndOfFile: Unexpected error in reading socket (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadCore(), line 277)
(Argus) Error EndOfFile: Receiving thread terminated with error (in src/rpc/socket/client/ClientSocketManager.cpp, function recvThreadWrapper(), line 379)
[2024-12-06 18:20:41 UTC][ZED][ERROR] [ZED] Cannot initialize the camera.
(Argus) Error InvalidState: Receive thread is not running cannot send. (in src/rpc/socket/client/ClientSocketManager.cpp, function send(), line 96)
(Argus) Error InvalidState:  (propagating from src/rpc/socket/client/SocketClientDispatch.cpp, function dispatch(), line 91)
Segmentation fault (core dumped)

Please write an email to support@stereolabs.com and send the diagnostic report as an attachment.