I’m having trouble getting two Stereolabs ZED XOne GS cameras working on a Jetson.
System:
Jetson Orin
JetPack 6.2.1
L4T 36.4.4
Linux kernel 5.15.148
CUDA 12.6
TensorRT 10.3.0
cuDNN 9.3.0.75
Cameras / ZED:
2 × ZED XOne GS
GMSL via MAX96712
ZED SDK 5.5.0
ZEDLink Duo 1.4.3-LI-MAX96712-L4T36.4.0
The cameras are correctly detected by ZED Explorer, GMSL/I2C communication works, the kernel detects both sensors, and /dev/video0 and /dev/video1 are created.
However, the cameras cannot actually stream any frames. Even using v4l2-ctl directly on the host, no frames are received.
The ZED SDK then fails with:
CAMERA FAILED TO SETUP
and the process exits with code -11.
Im trying to launch them with ros2 wrapper in docker and it returns with a log:
I understand that it may not be directly supported, although it was working on 5.2.2 before. Perfectly fine with 1 camera, problems with stability occured after adding 2nd camera and then upgrading to 5.5 results in errors above. Therefore i am quite certain that correct setup is possible on this hardware configuration.
Could you at least point me in the right direction with component_container_isolated-1] [2026-10-06 18:33:24 UTC][ZED][ERROR] [ZED-Argus][Critical] Cannot create iQueue (produceSingleV5) error?
Also, i have just tested that camera is streaming with ZED_Explorer when the graphical interface is active.