Hello @Myzhar, any updates on this?
I forgot to attach the config files, please have a look on them, most of it should be without modifications:
common.yaml
# params/common.yaml
# Common parameters to Stereolabs ZED and ZED mini cameras
---
# Dynamic parameters cannot have a namespace
brightness: 4 # Dynamic
contrast: 4 # Dynamic
hue: 0 # Dynamic
saturation: 4 # Dynamic
sharpness: 4 # Dynamic
gamma: 8 # Dynamic - Requires SDK >=v3.1
auto_exposure_gain: true # Dynamic
gain: 100 # Dynamic - works only if `auto_exposure_gain` is false
exposure: 100 # Dynamic - works only if `auto_exposure_gain` is false
auto_whitebalance: true # Dynamic
whitebalance_temperature: 42 # Dynamic - works only if `auto_whitebalance` is false
depth_confidence: 50 # Dynamic
depth_texture_conf: 100 # Dynamic
point_cloud_freq: 10.0 # Dynamic - frequency of the pointcloud publishing (equal or less to `grab_frame_rate` value)
general:
camera_name: zed # A name for the camera (can be different from camera model and node name and can be overwritten by the launch file)
zed_id: 0
serial_number: 0
gpu_id: -1
base_frame: 'base_link' # must be equal to the frame_id used in the URDF file
sdk_verbose: 1 # Set verbose level of the ZED SDK
svo_compression: 2 # `0`: LOSSLESS, `1`: AVCHD, `2`: HEVC
self_calib: true # enable/disable self calibration at starting
camera_flip: 'AUTO' # camera flip mode: 'OFF', 'ON', 'AUTO'
pub_resolution: 'CUSTOM' # The resolution used for output. 'NATIVE' to use the same `general.grab_resolution` - `CUSTOM` to apply the `general.pub_downscale_factor` downscale factory to reduce bandwidth in transmission
pub_downscale_factor: 2.0 # rescale factor used to rescale image before publishing when 'pub_resolution' is 'CUSTOM'
pub_frame_rate: 15.0 # frequency of publishing of video and depth data (see SDK API "InitParameters::grab_compute_capping_fps")
svo_realtime: true # if true the input SVO will be played trying to respect the original framerate eventually skipping frames, otherwise every frame will be processed respecting the `pub_frame_rate` setting
region_of_interest: '[]' # A polygon defining the ROI where the ZED SDK perform the processing ignoring the rest. Coordinates must be normalized to '1.0' to be resolution independent.
#region_of_interest: '[[0.25,0.33],[0.75,0.33],[0.75,0.5],[0.5,0.75],[0.25,0.5]]' # A polygon defining the ROI where the ZED SDK perform the processing ignoring the rest. Coordinates must be normalized to '1.0' to be resolution independent.
#region_of_interest: '[[0.25,0.25],[0.75,0.25],[0.75,0.75],[0.25,0.75]]' # A polygon defining the ROI where the ZED SDK perform the processing ignoring the rest. Coordinates must be normalized to '1.0' to be resolution independent.
#region_of_interest: '[[0.5,0.25],[0.75,0.5],[0.5,0.75],[0.25,0.5]]' # A polygon defining the ROI where the ZED SDK perform the processing ignoring the rest. Coordinates must be normalized to '1.0' to be resolution independent.
#video:
depth:
depth_mode: 'ULTRA' # 'NONE', 'PERFORMANCE', 'QUALITY', 'ULTRA', 'NEURAL'
depth_stabilization: 1 # [0-100] - 0: Disabled
openni_depth_mode: false # 'false': 32bit float meter units, 'true': 16bit uchar millimeter units
pos_tracking:
pos_tracking_enabled: true # True to enable positional tracking from start
pos_tracking_mode: 'STANDARD' # Matches the ZED SDK setting: 'QUALITY', 'STANDARD' -> Use 'QUALITY' with 'ULTRA' depth mode for improved outdoors performance
set_gravity_as_origin: true # If 'true' align the positional tracking world to imu gravity measurement. Keep the yaw from the user initial pose.
imu_fusion: true # enable/disable IMU fusion. When set to false, only the optical odometry will be used.
publish_tf: true # publish `odom -> base_link` TF
publish_map_tf: true # publish `map -> odom` TF
map_frame: 'map' # main frame
odometry_frame: 'odom' # odometry frame
area_memory_db_path: '' # file loaded when the node starts to restore the "known visual features" map.
save_area_memory_db_on_exit: false # save the "known visual features" map when the node is correctly closed to the path indicated by `area_memory_db_path`
area_memory: true # Enable to detect loop closure
floor_alignment: false # Enable to automatically calculate camera/floor offset
initial_base_pose: [0.0,0.0,0.0, 0.0,0.0,0.0] # Initial position of the `base_frame` -> [X, Y, Z, R, P, Y]
init_odom_with_first_valid_pose: true # Enable to initialize the odometry with the first valid pose
path_pub_rate: 2.0 # Camera trajectory publishing frequency
path_max_count: -1 # use '-1' for unlimited path size
two_d_mode: false # Force navigation on a plane. If true the Z value will be fixed to "fixed_z_value", roll and pitch to zero
fixed_z_value: 0.00 # Value to be used for Z coordinate if `two_d_mode` is true
depth_min_range: 0.0 # Set this value for removing fixed zones of the robot in the FoV of the camerafrom the visual odometry evaluation
set_as_static: false # If 'true' the camera will be static and not move in the environment
mapping:
mapping_enabled: false # True to enable mapping and fused point cloud publication
resolution: 0.05 # maps resolution in meters [0.01f, 0.2f]
max_mapping_range: -1 # maximum depth range while mapping in meters (-1 for automatic calculation) [2.0, 20.0]
fused_pointcloud_freq: 1.0 # frequency of the publishing of the fused colored point cloud
clicked_point_topic: '/clicked_point' # Topic published by Rviz when a point of the cloud is clicked. Used for plane detection
sensors:
sensors_timestamp_sync: false # Synchronize Sensors messages timestamp with latest received frame
max_pub_rate: 400. # max frequency of publishing of sensors data. MAX: 400. - MIN: grab rate
publish_imu_tf: true # publish `IMU -> <cam_name>_left_camera_frame` TF
object_detection:
od_enabled: false # True to enable Object Detection [not available for ZED]
model: 'MULTI_CLASS_BOX_ACCURATE' # 'MULTI_CLASS_BOX_FAST', 'MULTI_CLASS_BOX_MEDIUM', 'MULTI_CLASS_BOX_ACCURATE', 'PERSON_HEAD_BOX_FAST', 'PERSON_HEAD_BOX_ACCURATE'
max_range: 15. # Maximum detection range
allow_reduced_precision_inference: true # Allow inference to run at a lower precision to improve runtime and memory usage
prediction_timeout: 0.5 # During this time [sec], the object will have OK state even if it is not detected. Set this parameter to 0 to disable SDK predictions
object_tracking_enabled: true # Enable/disable the tracking of the detected objects
mc_people: true # Enable/disable the detection of persons for 'MULTI_CLASS_BOX_X' models
mc_vehicle: true # Enable/disable the detection of vehicles for 'MULTI_CLASS_BOX_X' models
mc_bag: true # Enable/disable the detection of bags for 'MULTI_CLASS_BOX_X' models
mc_animal: true # Enable/disable the detection of animals for 'MULTI_CLASS_BOX_X' models
mc_electronics: true # Enable/disable the detection of electronic devices for 'MULTI_CLASS_BOX_X' models
mc_fruit_vegetable: true # Enable/disable the detection of fruits and vegetables for 'MULTI_CLASS_BOX_X' models
mc_sport: true # Enable/disable the detection of sport-related objects for 'MULTI_CLASS_BOX_X' models
Zed2i.yaml
# params/zed2i.yaml
# Parameters for Stereolabs ZED 2i camera
---
general:
camera_model: 'zed2i'
grab_resolution: 'HD720' # 'HD2K', 'HD1080', 'HD720', 'VGA', 'AUTO'
grab_frame_rate: 30 # Frequency of frame grabbing for internal SDK operations
depth:
min_depth: 0.3 # Min: 0.3, Max: 3.0 - Default 0.7 - Note: reducing this value wil require more computational power and GPU memory
max_depth: 15.0 # Max: 40.0