@Myzhar, could you please clarify my last post? We are working on time-syncing ZEDX with other cameras and modalities, and knowing both - the end of each camera’s exposure and the delay between a trigger/drop and the corresponding frame/drop is pivotal, since we use frame triggering/dropping across cameras to align them temporally. Thank you.
Also, I have a theory - Please tell me if this is correct or not
The image capture lags the trigger by 1 pulse. As you said before, the trigger pulse rising edge syncs with the end of exposure for the image capture. Let’s say we set the camera to receive a pulse at 30 Hz. For the first pulse we send, it cannot estimate when to start the exposure such that the end is synced. This means that the camera/SDK, based on the first pulse, estimates when the next pulse will arrive and then starts the exposure so that the end of the exposure syncs with the second pulse.
Let’s say we send a pulse of 1111010010011, then the camera images are _111101001001 → basically delayed by 1 frame relative to the trigger. Is this correct ? If yes, then this explains why I was seeing a frame delay between the trigger and the corresponding image/drop, which means the delay is not coming from a wrong timestamp (i.e., ZEDX images contain the correct end-of-exposure time and not the timestamp post-frame buffering due to the ISP stack on the Jetson host)