Understanding Slave mode on the Quad capture card

Just to be clear, when you say the end of the capture is synchronized with the rising edge you are referring to the slave right ?

This would also mean that in case the trigger is generated usign a master Zed camera, then end of exposure of both the slave and master is synced with the rising edge of the trigger.

Are both these statements correct ?