Zedx Mono on Orin NX + Seedstudio A603

Hello,

I have been trying, unsuccessfully, to connect to the ZEDx mini over the Zen Link Mono card using on the Jetson Orin NX featuring a seedstudio a603 carrier board.

I have followed the instructions as for the Orin dev kit, enabled CSI using the jetson_io.py utility for the ZEDx camera, successfully installed the driver and made sure that the daemon is correctly running.

I do not see anything on dmesg and the diagnostic tool also does not detect any issue. I am concerned that this carrier board is not supported or that it would need a different driver to work.

I have also made sure that the connections are correct (between the card and the carrier board) and I am correctly powering the mono card. The only difference in setup is the cable as I had to use an adapter cable going from a narrow 22 to a larger 22 CSI connector on the board side.

Do you have experiences about this carrier board?

Thanks for the support,
Giuseppe

Hi @grizzi
Welcome to the StereoLabs community.

The Seedstudio A603 carrier board requires a custom ZED X Driver to be used with our capture cards.
The custom driver is not available because we do not officially support SeeedStudio carrier boards, as they do not provide software development support.