I using Duo card and orin nano with ZED x, I do think my connection and power supply is correct, but I cannnot get my streaming in this condition.
Sure!You can download it here because I am new user in community. https://drive.google.com/file/d/1F5J08W9s9OBMz6qGrAbNpFYH59XCJvKK/view?usp=drive_link
My jetson is already work, the power supply is used in capture card is 12v/2a, I confirm that I have used correct FPC 22pin-15pin line
Does ZED Explorer or any ZED SDK sample produce any error logs?
Dmesg log suggest camera is detected, if you can send any logs that would be helpful.
Thanks for ur reply, when I try to use ros2 launch zed_wrapper zed_camera.launch.py camera_model:=zedx
I get some error in log, you can figure out it here https://drive.google.com/file/d/1o2WVVcfMhZUTJUhiClTUIo1zOt4Abm6K/view?usp=drive_link
Hi @Que121,
Thanks for the log information. Can you confirm that you have been using this guide to connect the capture card: ZED Link Duo on Orin Nano - Stereolabs ?
The mipi cables seem a bit long, which can impact the signal quality. Recommended length goes up to 12cm, above this the signal can get corrupted or noisy.
Can you try with shorter mipi cables?
I will try to use a shorter cable for making a test
Hi! I have changed the shorter cable, but it still doesn’t work, could you help me next step? I will upload the log file for you
Does the LED on the ZED Link Duo turn on when the board is on? If not, this is either a power supply issue or a hardware one itself.