The ZedX page (ZED X Stereo Camera | Stereolabs) is unclear about what cables are included.
I expected the “Secure GMSL2 connection (1.5m cable included)” that comes with the ZedX to be the same cable that ships with the perception kit (Robotics Perception Kit - Dual | Stereolabs). However, the ZedX ships with a female-female cable, while the perception kit ships with female-male extender. The only image on the ZedX page that shows the cable only shows one end
I find it odd the ZedX ships with the female-female cable since the recommended jetson capture card setup would need the female-male GSML2 extension cable. Regardless, please update the ZedX description to make this clear