Hi, Is Occulus Quest 2 supported for AR pass through Application ?
Hi,
I only tested the ZED-mini with the Oculus Quest 1 and it’s working as expected. It should be the same with the Quest2.
However, the ZED-mini needs to be tethered to a computer. Your setup Quest2 + ZED-mini cannot be wireless.
Best regards,
Benjamin Vallon
Hi , Can I try wireless setup with ZED 2 ? Lets say i broadcast a Zed 2 stream over ip !!
Hi,
First I do not recommend using a ZED2 for AR passthrough. The distance between the left and right cameras are not suited for AR.
Then, I guess you can stream the ZED images to the Oculus Quest (If the camera is not attached to the headset but plugged to a computer). However it will generate latency which is not acceptable for AP purposes.
Best regards,
Benjamin Vallon
Please, do not reply to an old post with an unrelated issue.
You can either create a new post on the community forum or write a mail at support@stereolabs.com
Thanks.
Stereolabs Support