ZedBox Mini + fan accesory: fan speed always max.

Hello,

I have problem with fan accessory on my zed box mini, fan always sound like at 100% and fan speed controls are not working.

jtop reports that fan speed is being controlled going from 30-70% when under load, but actual fan speed doesn’t change.

jtop reports fan speed at 0RPM

Hi @Janis8008
Welcome to the StereoLabs community.

This is the correct behavior. The fan speed is not controlled by the carrier board.