We have 3 cameras (1 ZED X + 2 ZED One). Running ZED360 fails with the following error message:
Only ONE opened camera
ZED360 is able to open one camera. The calibration process requires at least two cameras.
Our setup:
- Quad link card with two 4-to-1 GMSL
- We have 1 ZED X camera connected to first 4-to-1 GSML (based on the S/N logged, we know this one gets detected by
ZED360) - We have 2 ZED One cameras connected to second 4-to-1 GSML
- ZED SDK 4.2.3, Jetpack 6.0 (L4T 36.3.0), latest Quad link drivers (1.2.1-SL-MAX96712)
ZED_Explorer finds all three cameras.
Running ZED_Diagnostic also only detects the ZED X Camera:
"Camera Test": {
"InternalDevicesCount": 0,
"ZEDCount": 1,
"camera": {
"Device ID": 0,
"Firmware": 2001,
"Init Output": "OK",
"Model": "ZED-X",
"Serial Number": <redacted>,
"valid": [
"<b>Camera: </b>ZED-X",
"<b>Firmware: </b>2001"
]
}