Zed2i Camera control without SDK or CUDA capable device.

We just bought the Zed 2i Camera and we are eager to start playing with it!

The problem we are now facing is that the camera needs to be connected directly to a device with CUDA support. We have a server with CUDA support, but connecting the camera to it is not possible as it is in another building.

The developer was going to develop the app through the server, but apparently thats not possible now.

What we need to do using the camera is to mount it somewhere and have it capture some images based on a time interval. We will then grab the images and do some processing on them.

So in the end, the camera will not run any ML application, and this is why we were wondering if we can do some basic controls with a device that does not have CUDA.

Thank you in advance,

Marios.

Hi @mariosconsta
Welcome to the Stereolabs community.

You could consider these two open source solutions not using the ZED SDK: