Rolling the chessboard clockwise (from my perspective) throws an error “!!! Do not rotate the checkerboard more than 45 deg around Z !!!”. So I have to rotate it counter-clockwise from 0 to 45 degrees.
Built the application again and the Z-axis went to a 100 percent. I am sharing the results of Zed Depth Viewer, can you please tell me that the image distortion is expected or I have to re-calibrate the cameras?
After calibrating it multiple times (with 9x6 chessboard), every time the calibration file was corrupted as the baseline was coming out to be negative. Just inverting the baseline with its positive value solved the issue. Now the images are not distorting and the point clouds are forming as expected.
The left and right cameras are set accurately in the streamer application and I think it was showing correctly in the calibration application too. Should I try inverting the cameras in the streamer application itself?
Got it. Will try recalibrating it and get accurate results.