ZED X One S + ZED Link Duo — correct GMSL2 cabling for 10m distance?

Hi,
I purchased 3× ZED X One S (Narrow) with a ZED Link Capture Card Duo on a Jetson Orin Nano.

What I have:

  • 3× ZED X One S (Narrow)

  • 3× GMSL2 Fakra F–F, 10m

  • ZED Link Capture Card Duo (came with GMSL2 1-to-4 M–F cable, 0.5m)

Target setup:
Each camera positioned up to 10m from the capture card (3 cameras total).

I’ve realized my current cables are not suitable for this setup. I noticed you offer a GMSL2 Fakra Extension Cable M–F.
Is this the correct cable I should use instead of the 3× GMSL2 Fakra F–F (10m)?

If so:

  • Will this ensure low-latency, stable, and high-quality transmission?

  • Is it possible to replace or exchange the cables I purchased with the correct ones?

Thanks in advance for your help.

Yes, that’s the correct cable to be used with the 4-wire Fakra adapter.
You can find details in this support page:
https://support.stereolabs.com/hc/en-us/articles/27132108097687-What-type-of-GMSL2-cable-should-I-use-with-my-ZED-X-camera

Yes, the cables that we send are optimized to be used with our products.

Unfortunately, this is not possible. We don’t have any exchange policy, so no exchange/replacement with other cables is possible.