ZED X One GS not detected

Hi Stereolabs,

We are still debugging the ZEDBox Mini / ZED X camera detection issue on our Jetson Orin NX system.

Background:
We previously saw that the system was booting with the Super Mode DTB:

The active Stereolabs boot entry used:

FDT /boot/dtb/kernel_tegra234-p3768-0000+p3767-0001-nv-super.dtb

and:

OVERLAYS /boot/tegra234-p3768-camera-zedbox-mini-sl-overlay.dtbo

Based on your previous advice that Super Mode may cause issues with the Mini Carrier / ZEDBox Mini setup, we tested a normal DTB.

We added a separate boot entry without modifying the existing one:

LABEL Stereolabs-normal-test

using the same kernel, initrd, APPEND line and ZEDBox Mini overlay, but with:

FDT /boot/tegra234-p3768-0000+p3767-0001-nv.dtb

The normal DTB exists locally and its compatible strings are:

Current result on the normal DTB is that no zed device are detected.

The Stereolabs-related kernel modules are loaded:

$ lsmod | grep -Ei "sl_|zed|max929"
sl_zedxone_uhd         40960  0
sl_zedx                28672  0
sl_zedxhdr             24576  0
sl_max9295             16384  3 sl_zedxhdr,sl_zedxone_uhd,sl_zedx
sl_max9296             36864  4 sl_zedxhdr,sl_zedxone_uhd,sl_max9295,sl_zedx
tegra_camera          217088  6 nvhost_isp5,nvhost_nvcsi_t194,sl_zedxhdr,sl_zedxone_uhd,nvhost_vi5,sl_zedx
videodev              249856  7 v4l2_async,sl_zedxhdr,videobuf2_v4l2,tegra_camera,sl_zedxone_uhd,videobuf2_common,sl_zedx

But with dmesg it still shows the same I2C / MAX9296 failure:

i2c i2c-2: of_i2c: modalias failure on /bus@0/i2c@3180000/zedxone_uhd_ser@44
i2c i2c-2: Failed to create I2C device for /bus@0/i2c@3180000/zedxone_uhd_ser@44
i2c i2c-2: of_i2c: modalias failure on /bus@0/i2c@3180000/zedxone_uhd@1a
i2c i2c-2: Failed to create I2C device for /bus@0/i2c@3180000/zedxone_uhd@1a

sl_max9296 2-0048: Driver Version : v1.4.2
sl_max9296 2-0048: write_reg_Dser: addr = 0x10, val = 0x80
sl_max9296 2-0048: write_reg_Dser: addr = 0x10, val = 0x21
sl_max9296: probe of 2-0048 failed with error -1

bmi088: probe of 2-004b failed with error -5
bmi088: probe of 2-003b failed with error -5

And ZED Explorer still detects nothing:

$ /usr/local/zed/tools/ZED_Explorer --all
No ZED detected

System details:

L4T: R36.4.7
Kernel: 5.15.148-tegra
Ubuntu: 22.04.5
ZED SDK: 5.1.2
Stereolabs package: stereolabs-zedbox-mini 1.4.2-SL-MAX9296-ZEDBOX-MINI-L4T36.4.0

Important observation:
Earlier we inspected the live device tree and the ZEDBox Mini overlay. It looks like the overlay creates both complete suffixed nodes and incomplete/non-suffixed nodes, for example:

Complete-looking nodes:

zedxone_uhd_0@1a
zedxone_uhd_ser_0@44

but also suspicious incomplete nodes:

zedxone_uhd@1a
zedxone_uhd_ser@44

The kernel errors specifically reference the non-suffixed nodes:

zedxone_uhd@1a
zedxone_uhd_ser@44

These appear to be missing required properties such as compatible and/or reg, which matches the of_i2c: modalias failure messages.

So after testing the normal DTB, the conclusion is:

  1. The camera stack still fails in the exact same way with normal-mode

  2. The failure appears to be related to the ZEDBox Mini overlay / device-tree nodes and/or the MAX9296 probe.

Dp you have any suggestions?

Specifically:

  • Is stereolabs-zedbox-mini 1.4.2-SL-MAX9296-ZEDBOX-MINI-L4T36.4.0 expected to work on L4T R36.4.7 / kernel 5.15.148-tegra?

  • Are the non-suffixed nodes zedxone_uhd@1a and zedxone_uhd_ser@44 expected to exist in the live device tree?

  • If they are dummy/placeholder nodes, should they be disabled or removed from the active I2C bus?

  • Is the sl_max9296: probe of 2-0048 failed with error -1 caused by the invalid/dummy serializer/sensor phandles?

  • Is there a newer ZEDBox Mini overlay/driver package for this exact L4T version?

  • Should we patch the DTBO, downgrade/upgrade the Stereolabs package, or do a full normal-mode reflash with a specific JetPack/L4T version?

Hi @hatfalk
Welcome to the StereoLabs community.

Are you using a ZED X One GS or a ZED X One 4K? They are different models that have different multi-camera setup requirements.

Are the cameras detected when they are connected singularly?

Yes, it is.

Why are you modifying the device tree if you are using a StereoLabs device? This is not normally required.

Hey, thank you for quick reply. We are using ZED X One GS. They are not detected when connected singularly.
Just saw it complaining about probe failures and thought had something do with the DTBO iguess. linked to the dmesg log.

I recommend you uninstall the current driver:
sudo dpkg --purge stereolabs-zedbox-mini
Then reboot, and download and install the latest ZED X Driver v.1.4.2 for L4T 36.4.x (JetPack 6.1 & 6.2.1).

Finally, download and install the latest ZED SDK v5.3.1.

After a reboot, you should be able to open the cameras with ZED_Studio, ZED_Explorer, and ZED_Depth_Viewer.

If problems persist, I recommend you reflash the device and reinstall all the software from scratch: