Zed X one 4K Depth of field and custom lenses

Hi,

I couldn’t find the depth of field of zed X one 4K.

Furthermore, I need very specific DOF (from 0.3m to 2m) so I probably need specific lenses. Can you please provide me some suggestion or even just lens provider? If I buy my own lenses will the product still be waterproof?

Hi @Mowgli
Welcome to the Stereolabs community.

This information is not provided. The ZED X One cameras are calibrated to provide focus to infinity

Yes, in this case I recommend you get the camera with no optics and install the lenses that fulfill your requirements.

You can use the S-Mount optics that you prefer.

The ZED X One 4K is not waterproof. It has no certified IP rating.

Thanks for your kind answer Myzhar.

What about the minimum focus distance?

I can provide full details from our Optics team:
Close range = 0.58m
Far range = 70.89m
→ DoF = 70.31m