ZED X on TwoWin TW-T808P-G — V4L2 capture timeout due to incomplete 4-lane CSI init in sl_max96712 v1.4.0

Hi everyone,

I’m trying to use a ZED X camera on a Jetson Orin NX 16GB mounted on a TwoWin TW-T808P-G carrier board via GMSL2.

Setup:

  • Jetson Orin NX 16GB, JetPack 6.2.1 (L4T R36.4.3)
  • TwoWin TW-T808P-G carrier board
  • MAX96712 deserializer connected to Jetson CSI port-index 0 (serial_a), 4-lane CSI
  • Built Stereolabs BSP drivers from zedx-driver-bsp (L4T 36.x branch), all v1.4.0
  • Custom device tree overlay adapted for TwoWin’s hardware

What’s working:

  • All three kernel modules load and probe successfully
  • GMSL2 link is active, camera detected on correct port
  • Camera serial number confirmed, “camera pipeline operational”
  • /dev/video0 and /dev/video1 created
  • ZED SDK detects the camera as “AVAILABLE”

What’s NOT working:

  • V4L2 capture always times out: “uncorr_err: request timed out after 2500 ms”
  • No video data flows from deserializer to Jetson VI
  • ZED SDK fails with “CAMERA FAILED TO SETUP”

Details:
TwoWin’s carrier board uses 4-lane CSI (bus-width=4, opt-csi-port=“a”). The driver reports “Setup Deser as 4 lanes output” which is correct. However, it seems like the 4-lane CSI output mode may not be fully initializing the deserializer’s output — the 2-lane mode works on Stereolabs’ own carrier boards but 4-lane mode on a third-party board does not.

I’ve confirmed the correct CSI wiring with TwoWin (port-index, lane count, lane polarity) so the device tree overlay is correct.

Questions:

  1. Is 4-lane CSI mode (2x4) fully supported in the current BSP driver (v1.4.0)?
  2. Is there a newer driver version with improved support for 4-lane CSI configurations?
  3. Has anyone successfully used ZED X on a third-party carrier board that uses 4-lane CSI?
  4. Are there any additional device tree properties or driver configurations needed for 4-lane mode on non-Stereolabs boards?

Happy to share dmesg logs or device tree overlay privately if it helps debug.

Thanks!

Hello,

Can you contact support@stereolabs.com with your issue so we can better assist you ?

Thanks !

Stereolabs Support

Hi Rodolphe,

I already sent a detailed email to support@stereolabs.com on March 17th, followed up on the 18th, and then again on the 20th regarding this exact issue.

I detailed the root cause found in the driver initialization tables for 4-lane mode.

Can you check the thread or let me know who I should contact directly?

Thanks!

Hi Pushpendra,

Thanks for following up — and also for the detailed investigation you shared earlier. I hadn’t seen the original support email you had sent. Sorry about this.

I see that someone from our team has already replied on that support thread over the last few days. We’re currently reviewing internally the latest information you’ve shared this morning, and we’ll get back to you as soon as possible on the existing support thread.

Thanks again for your patience.

Best,

Stereolabs Support

No worries, thanks for the update!

Hi Stereolabs,

Just a quick follow-up — if you need any specific technical details about the TwoWin TW-T808P-G board to help adapt the driver, please let us know exactly what information you require. We can request it directly from the board supplier.

Thank you!

No worries, thanks for the update!

Did you ever resolve this? I’m considering buying one of these but I need support for 4x Zed One GS